Member's Forum What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 71 replies
  • Subscribers 593 subscribers
  • Views 11741 views
  • Users 0 members are here
  • element14 community
  • win
  • element14 members
  • aske14
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What’s the most time-saving habit you’ve picked up? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 1 month ago

A new month means a new AskE14!

Engineers, makers, and problem‑solvers are always finding smarter ways to work. From optimising workflows to automating repetitive tasks, small habits can add up to serious time savings.

This month, AskE14 is all about sharing the habits that help you work more efficiently, whether you’re designing, prototyping, debugging, documenting, or managing projects.

Time for the question:

What’s the most time-saving habit you’ve picked up? 

Time is a valuable resource in engineering. A simple habit — like better version control, smarter test setups, or clearer documentation. This can save hours down the line.

imageimage

Competition Details

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:


1. You need to make sure you are  Register  or Login
2. Then answer the following question by adding a reply or commenting!

What’s the most time-saving habit you’ve picked up? 

This month, we are giving away:

The Community team will then select the best 3 answers to win the UNO R4 Minima! 

image

Closing date: 1st March 

Winners announced: 10th March 

UNO R4 Minima  

Terms and Conditions 

imagePDF

The winners! 

dang74 

wolfgangfriedrich 

skruglewicz 

E14Alice will be reaching out to you soon to confirm contact details

  • Cancel

Top Replies

  • dang74
    dang74 1 month ago +5
    For hobby projects I've been pasting code into ChatGPT so that it can fulfill the role of a peer review. It has caught many dumb mistakes that would have otherwise gone unnoticed until the debug stage…
  • Arnovsharma
    Arnovsharma 1 month ago +5
    The habit that has been most valuable to me is to document my work as I do it, rather than later. This includes: Maintaining a simple project log (even in a notebook or text file). Recording why…
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago +5
    Simulate critical parts of the design. If the simulation works, chances are that you saved one iteration of design and the likelihood of the 1st prototype working increased by a lot. If the simulation…
  • Arnovsharma
    Arnovsharma 1 month ago in reply to Aniket_kumar_raj

    I'm also Ai Wink

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • bradfordmiller
    bradfordmiller 1 month ago

    When writing code I generally work bottom up and, I also write the test cases for that code (based on the spec), which can be commented out (or in a separate file not normally loaded). Then I can test each module separately which saves a lot of time during integration (higher level testing) as the lower level parts are known to meet their specification. Additionally some of these tests (e.g., type validation of arguments) can be added directly into the code but suppressed for higher optimization levels (i.e. for delivery).

    Design by contract languages may help with this as well, though I'm not currently using one. I suppose this would be the moral equivalent of using SystemVerilog for testbenches, but something that can be carried around in code that is actually being executed on the target rather than only in simulation.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • dang74
    dang74 1 month ago in reply to Aniket_kumar_raj

    Perphaps... but what I see is that many people discuss using AI for code generation... but not so much for verification... so I posted this to benefit those that are not doing this... there is still a caveat though in terms of privacy and one should be mindful of their company's IP policies before pasting code into something like ChatGPT.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich 1 month ago in reply to Aniket_kumar_raj

    LTspice for discrete circuits and ModelSim for VHDL design. 
    And then there is QSpice which claims to be able to simulate digital (C, VHDL) and discrete components in the same design, but I did not have time to try it out properly.

    And for simple stuff there is always a handheld calculator and Brain1.0

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • battlecoder
    battlecoder 1 month ago in reply to wolfgangfriedrich

    I've been doing some simulations in LTSpice lately, and it's made so much easier and faster to test stuff out. They also help me figure out if something works or not before even hitting the breadboard so I agree!

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
  • michaelkellett
    michaelkellett 1 month ago in reply to wolfgangfriedrich

    LT Spice is one of very few things which is both good and free. It does rather push you towards the Analog Devices part for any given job (assuming they make one) because it only includes ready to use models for their chips (although you can use spice models from other manufacturers with a little bit of effort (although they don't always work)).

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • dougw
    dougw 1 month ago

    I use many methods to save time such as organizing tools and components during a build so that I can access everything from where I sit without standing up, but the one that saves the most time is structuring my workflow so that I can order long lead components as early in the project as possible.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • robogary
    robogary 1 month ago

    Keeping tbe workshop, parts, and tools organized.

    There was a previous E14 discussion post on this topic. I continue to refine the workshop and workbench areas,  in fact, I have just ordered an "Pack Over Door Organizer with 5 Large Pockets 10 Mesh Side Pockets, 44 lbs Weight Capacity Hanging Storage Organizer with Clear Window Kids Toys, Shoes, Diapers, Dark Grey, 5 Layers" People often use these for baby supplies or bathroom supplies.

    Im going to use this organizer to put DVMs, handheld scopes, usb scopes, bags of sorted usb cables,  crimpers and strippers,  markers, pencils and pens - stuff that gets buried on my workbench , that needs to be quickly accessed and kept nearby. Im also running out of floor space for shelves and drawers. 

    I waste too much time looking for parts and meters when getting into the heat of battle.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
  • BigG
    BigG 1 month ago in reply to wolfgangfriedrich

    I certainly need to do this more often. I've had a case where hardware did fail and on close inspection of the design had identified an issue, but could not quite explain the why. Other engineers had other ideas. It was most satisfying when the LTspice simulation was completed, and it was able to not only mimic the failure but was also able to show why the attempted fixes did not work. It then proved the hunch.

    These days you can simulate directly via KiCAD. So no excuses.

    • Cancel
    • Vote Up +1 Vote Down
    • Cancel
  • veluv01
    veluv01 1 month ago

    I'd say adding proper comments (block wise instead of just at the top of the file) throughout my code. It kinda sounds basic, but saves my time for the future me trying to understand the stuff I wrote a few weeks ago and also my coworkers don't have to haunt me with the questions about it.

    • Cancel
    • Vote Up 0 Vote Down
    • Cancel
<>