Member's Forum What’s the worst mistake/problem you’ve made during a project, and what did you learn from it? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 59 replies
  • Subscribers 593 subscribers
  • Views 1793 views
  • Users 0 members are here
  • rasberrypi
  • win
  • aske14
Related

What’s the worst mistake/problem you’ve made during a project, and what did you learn from it? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 19 days ago

Hello Everyone!

Hope you are all doing well. I’m excited to announce that this month's AskE14 question is: What is the worst mistake or problem you've encountered during a project, and what did you learn from it?

Sharing your experiences can help others identify similar challenges and understand how to overcome them. I hope this discussion will be beneficial for those who are just starting out on a project or feeling stuck with a problem.

Here's the question:

What’s the worst mistake/problem you’ve made during a project, and what did you learn from it? 

imageimage

Competition Details

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:

1. You need to make sure you are Register  or Login
2. Then answer the following question by adding a reply or commenting!

What’s the worst mistake/problem you’ve made during a project, and what did you learn from it?  

The Community team will then select the best 3 answers to win a Raspberry Pi 400!

This month, we are giving away:

image

Learn more

Terms and Conditions 

imagePDF

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw 19 days ago +8
    My first rude awakening on the job was building a linear regulator to output 4A at 5V with a car battery as the input. I used a 2N3055 (TO3) as the pass transistor because it could handle 15 Amps and 115…
  • gordonmx
    gordonmx 19 days ago +6
    Many years ago, I worked for a company that made portable computers. A large service company wanted an add-on module base with more battery power to boost the operating life. The original computer had…
  • chloro
    chloro 19 days ago +5
    My worst project mistake? I guess I would say trusting a breadboard connection that “looked fine.” I spent hours debugging firmware, rewriting code, and questioning my life choices… only to find one…
Parents
  • fyaocn
    fyaocn 18 days ago

    Project Mistake & Lessons Learned  by flashing FRDM-RW612 Platform During the development of an AI-powered smart speaker project.

    The smart speaker is centered on the FRDM‑RW612 development board, with audio capture using an ICS‑43434 I²S digital microphone.

    image

    Then detect the voice when command phrase appears, as up-down-on-off etc. I create one time series studio project for FRDM-RW612

    image

    Then upload voice track for training

    image

    It turns out to output AI model 

    image

    Everything works fine, and I want to make sure the RW612 is good for this tinyML project, I find one ready-to-go demo project in another official board from NXP RD-RW612-BGA

    image

    I presume that both share same RW612 chip and it shall work fine.  Then  I made one of the worst and most costly mistakes:

    Flashed firmware built for the RD‑RW612‑BGA module onto the FRDM‑RW612 development board, even though they use the same chip.
    This wrong flash immediately locked the board, and it became extremely difficult to unlock, even by following the official NXP unlock guide:community.nxp.com/.../2015561
    Even with AI model training and high-level application logic, this low-level hardware/firmware mismatch fully bricked the device. It seems that I am not alone in doing so. But the FRDM-RW612 still bricks and my project paused now. 

    Key Lessons Learned

    1. Always verify hardware platform before flashing
      Even with the same core chip, different boards (module vs. evaluation board) have different memory layouts, boot configurations, clock sources, and pin mappings. Using the wrong firmware will cause lockup or permanent damage.
    2. Understand fundamental logic before taking action
      High-level AI features mean nothing if you don’t master the boot process, flash security, ISP mode, and low-level hardware configuration.
    3. Double-check build target and firmware configuration
      Never assume “same chip = same firmware”. Always confirm the target:
      • rdrw612bga
      • frdmrw612
    4. Have a recovery plan before mass flashing
      Know how to enter bootloader/ISP mode, backup original firmware, and use official unlock tools before programming.
    This was the most critical mistake in the entire project. It taught me that embedded system stability starts with understanding the basics, not just high-level AI functions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fyaocn
    fyaocn 18 days ago

    Project Mistake & Lessons Learned  by flashing FRDM-RW612 Platform During the development of an AI-powered smart speaker project.

    The smart speaker is centered on the FRDM‑RW612 development board, with audio capture using an ICS‑43434 I²S digital microphone.

    image

    Then detect the voice when command phrase appears, as up-down-on-off etc. I create one time series studio project for FRDM-RW612

    image

    Then upload voice track for training

    image

    It turns out to output AI model 

    image

    Everything works fine, and I want to make sure the RW612 is good for this tinyML project, I find one ready-to-go demo project in another official board from NXP RD-RW612-BGA

    image

    I presume that both share same RW612 chip and it shall work fine.  Then  I made one of the worst and most costly mistakes:

    Flashed firmware built for the RD‑RW612‑BGA module onto the FRDM‑RW612 development board, even though they use the same chip.
    This wrong flash immediately locked the board, and it became extremely difficult to unlock, even by following the official NXP unlock guide:community.nxp.com/.../2015561
    Even with AI model training and high-level application logic, this low-level hardware/firmware mismatch fully bricked the device. It seems that I am not alone in doing so. But the FRDM-RW612 still bricks and my project paused now. 

    Key Lessons Learned

    1. Always verify hardware platform before flashing
      Even with the same core chip, different boards (module vs. evaluation board) have different memory layouts, boot configurations, clock sources, and pin mappings. Using the wrong firmware will cause lockup or permanent damage.
    2. Understand fundamental logic before taking action
      High-level AI features mean nothing if you don’t master the boot process, flash security, ISP mode, and low-level hardware configuration.
    3. Double-check build target and firmware configuration
      Never assume “same chip = same firmware”. Always confirm the target:
      • rdrw612bga
      • frdmrw612
    4. Have a recovery plan before mass flashing
      Know how to enter bootloader/ISP mode, backup original firmware, and use official unlock tools before programming.
    This was the most critical mistake in the entire project. It taught me that embedded system stability starts with understanding the basics, not just high-level AI functions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Aniket_kumar_raj
    Aniket_kumar_raj 18 days ago in reply to fyaocn

    As the saying goes, simplicity is the ultimate sophistication. You were chasing 10,000 AI parameters when you should have been chasing one hardware jumper. This proves that in embedded systems, the 'basics' aren't just the beginning—they are the entire game. You tried to build a skyscraper on a swamp of 'assumed' compatibility, and the board gave you the ultimate reality check