Member's Forum What’s the most dramatic failure of a low‑quality component you’ve seen, and how did you diagnose the root cause, evaluate the impact, and prevent it from happening again? We are asking e14 in our Join, Share & Win Competition
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Locked Locked
  • Replies 23 replies
  • Subscribers 628 subscribers
  • Views 5904 views
  • Users 0 members are here
  • element14 community
  • win
  • element14 members
  • aske14
Related
This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

What’s the most dramatic failure of a low‑quality component you’ve seen, and how did you diagnose the root cause, evaluate the impact, and prevent it from happening again? We are asking e14 in our Join, Share & Win Competition

E14Alice
E14Alice 5 months ago

Hello Everyone,

I hope you are doing well!

This month’s question was inspired by one that JWx sent over, so a big thank you to JWx for the suggestion!

If anyone else has questions or ideas they’d like to see featured in AskE14, please send them my way, and I’ll line them up for the coming months.

Now to the question: 

What’s the most dramatic failure of a low‑quality component you’ve seen, and how did you diagnose the root cause, evaluate the impact, and prevent it from happening again?

imageimage

Competition Details 

You'll have to be a member of the element14 Community to join in and take part in this “Join, Share & Win” challenge. It's simple, all you have to do is:

1. You need to make sure you are Register or Login
2. Then answer the following question by adding a reply or commenting!

What’s the most dramatic failure of a low‑quality component you’ve seen, and how did you diagnose the root cause, evaluate the impact, and prevent it from happening again?

3. The Community team will then select the best 3 answers to win a UNO R4 Minima! 

image

Closing Date: 30th April 

Winners announced: 1st May

UNO R4 Minima

Terms and Conditions 

imagePDF

This month's winners

 acdc90 

 gpolder 

 strb 

E14Alice will be reaching out to you soon to confirm contact details

  • Cancel
Parents
  • kmikemoo
    kmikemoo 5 months ago

    Ope!  Another story.  Circa 2007.  One of our controller suppliers - based out of British Columbia - had a quality issue with one of the chips on their main board.  When the temperature dropped to around freezing - the systems would reset.  You would think a company based in BC would be able to design something that worked in the cold - because it gets cold in BC.  Right?
    Unfortunately, this meant that the system also went into Emergency Stop - which required a manual reset.  This is not a good condition for an emergency backup generator.  Of course, they initially denied it.  So I took a dozen of the controllers and placed them in the refrigerator freezer at work and took them out one by one for testing.  At least 1 in 4 failed - so I threatened to ship 100% of our stock back and replace them with a different supplier.  We never did figure out which chip was the root cause of failure.

    Story 2:  Home standby generators would not make voltage when the temperature dipped to 20F or so.  That's not all that unusual a temperature for Wisconsin or any of the Northern states.  It happens from time to time in the Southern states.  The generators would fail.  We would replace the voltage regulator.  They would fail again.  We would bring them to the shop.  They would not fail.  Any of them.  It took us weeks to figure out that the component supplier had changed potting material - that shrank when it got cold - and was pulling the connections on the PCB open.  They would reconnect once the potting material expanded when it got warmer.
    Laughing  While the system manufacturer blamed a supplier, we all knew that these regulators were made in house.  Joy

    Story 3:  Sort of the same thing as above - except this time it was an internal connection on a Silicon Controlled Rectifier.  Once the temperature got to below freezing, the Gate would open.  This was even harder to track down because there are 6 SCRs in a 3-phase full-wave bridge rectifier and, depending upon the load (or lack thereof - aka testing), two functional SCRs can mask the problem for a long time.  We did learn that the manufacturer changed suppliers - and wrote a better specification for the rectifier assembly.

    • Cancel
    • Vote Up +2 Vote Down
    • Cancel
Reply
  • kmikemoo
    kmikemoo 5 months ago

    Ope!  Another story.  Circa 2007.  One of our controller suppliers - based out of British Columbia - had a quality issue with one of the chips on their main board.  When the temperature dropped to around freezing - the systems would reset.  You would think a company based in BC would be able to design something that worked in the cold - because it gets cold in BC.  Right?
    Unfortunately, this meant that the system also went into Emergency Stop - which required a manual reset.  This is not a good condition for an emergency backup generator.  Of course, they initially denied it.  So I took a dozen of the controllers and placed them in the refrigerator freezer at work and took them out one by one for testing.  At least 1 in 4 failed - so I threatened to ship 100% of our stock back and replace them with a different supplier.  We never did figure out which chip was the root cause of failure.

    Story 2:  Home standby generators would not make voltage when the temperature dipped to 20F or so.  That's not all that unusual a temperature for Wisconsin or any of the Northern states.  It happens from time to time in the Southern states.  The generators would fail.  We would replace the voltage regulator.  They would fail again.  We would bring them to the shop.  They would not fail.  Any of them.  It took us weeks to figure out that the component supplier had changed potting material - that shrank when it got cold - and was pulling the connections on the PCB open.  They would reconnect once the potting material expanded when it got warmer.
    Laughing  While the system manufacturer blamed a supplier, we all knew that these regulators were made in house.  Joy

    Story 3:  Sort of the same thing as above - except this time it was an internal connection on a Silicon Controlled Rectifier.  Once the temperature got to below freezing, the Gate would open.  This was even harder to track down because there are 6 SCRs in a 3-phase full-wave bridge rectifier and, depending upon the load (or lack thereof - aka testing), two functional SCRs can mask the problem for a long time.  We did learn that the manufacturer changed suppliers - and wrote a better specification for the rectifier assembly.