I picked up something like this about three years ago. No regrets.
Though I can't help but feel like I'm also adding to the climate problem.
I picked up something like this about three years ago. No regrets.
Though I can't help but feel like I'm also adding to the climate problem.
From 2026
Pictures show scale of drought across England as rivers dry up
I did a quick test with the 6" duct fan at the weekend to see what sort of air flow / noise it generated. It's certainly very good at clearing the paperwork off one's desk at quite a distance.
I now need to work out the best arrangement and positioning. By flying the fan from the ceiling I can keep the duct as straight as possible to the window vent to maximize airflow but whether to draw cool air in or vent hot air out and whether to push or pull air through the duct.
I did another quick test and by simply exhausting the air out the door at around 40-50% fan speed I could feel cooler air being drawn into the room and the temperature on the thermometer started dropping at a rate of around 0.1C every 5 minutes.
I get the feeling I'm going to need an anemometer soon.
Although, I suspect that the solid walls / roof space act as a storage heaters to some extent.
Yes, walking around with a thermal camera shows that despite 'heat rising' there's some amount of 'infrared radiation' or otherwise radiates out from the ceiling/walls and that also takes time to cool down, even having aircon.
I'm sure having aircon is more about keeping the walls cool than the air within it.
The hard bit is our walls are solid with no space for ducting of any kind
I'm planning on ducting through an existing window vent (or two)
Have just acquired a 6" duct fan that can move up to 402cfm, so hoping I can tap into some of the cooler evening air to help with night time sleeping, without going to full-on aircon at this stage.
Although, I suspect that the solid walls / roof space act as a storage heaters to some extent.
The UK is consistently Grey and overcast as a general rule. Except 5-8 weeks in the summer where our insulated miserable weather houses struggle with 30C and we all think about getting aircon. The hard bit is our walls are solid with no space for ducting of any kind, so if you have the money some people end up with free standing units. Still rare.
I feel like we could have bought and air conditioner with the amount we've spent on reflective film
These will sort of fit UK style casement windows
Almost there but not quite right.
These will sort of fit UK style casement windows:

Had been thinking of doing something similar but with a better fixing arrangement.