Member's Forum I need help on designing a handheld storage based on micro SD Card + QSPI interface + Wi-Fi data transfer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Subscribers 628 subscribers
  • Views 733 views
  • Users 0 members are here
  • qspi
  • SD card
Related

I need help on designing a handheld storage based on micro SD Card + QSPI interface + Wi-Fi data transfer

HKPhysicist
HKPhysicist 1 month ago

Hello Fellow Engineers and Experts,

I want to design a device to replace the super expensive iCloud or Gcloud digital monopoly.  So you can download your beloved digital contents from your phone any time through Wi-Fi.  Then, stack them up one by one infinitely under your desk.

It is my basic components:

  1. micro SD Card
  2. SQPI interface and controller
  3. a MCU with SQPI peripheral, with SoC Wi-Fi
  4. a built-in Li+ battery
  5. Li+ charger chip
  6. any more
  7. There are already many USB storages for this purpose.  So this method will not be my goal.

Please share your opinions.  Perhaps, we can work together.  Wink

  • Sign in to reply
  • Cancel
  • Ravil
    0 Ravil 30 days ago

    I am not fit to validate this idea, but what comes in my mind first is to test out of this actually is suitable enough and construct a complete PoC (including software) for the same.

    I can suggest you set of MCU which has SD card slot by default (usually good speed). ESP32-P4 varient. You could write the firmware to make it the AP and the device (or devices) could connect to the STA using PSK2/3 and upload videos/photos for the same (software part will be critical and has to be optimised). Once this is success you could add up HSM (Hardware Security Module) for increasing access security of the SD card. 

    (If this becomes a product, it makes more sense if you never inform the user its a SD card. Just give a device which they have for 1TB packed in a casing. They could access it as a SSD or wireless device and ESP32 P4 with 32 Mb of flash and Ram can easily do all of this)

    Keep your journey posted, will be interested to learn more.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • abtAmit
    0 abtAmit 1 month ago in reply to HKPhysicist

    You can use esp32S3 it support SD_MMC. SD Cards does not support QSPI but they do support SD_MMC interface.
    ESP have well documented here esp-idf/examples/storage/sd_card/sdmmc at master · espressif/esp-idf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • beacon_dave
    0 beacon_dave 1 month ago in reply to cstanton
    cstanton said:
    I'm partly reminded of the old Eye-fi cards.

    Reminds me more of the Kingston MobileLite Wireless Wi-Fi enabled SD card reader.

    https://www.kingston.com/datasheets/MLW221_en.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • HKPhysicist
    0 HKPhysicist 1 month ago in reply to balajivan1995

    That add a magnet on top of a SSD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • HKPhysicist
    0 HKPhysicist 1 month ago in reply to shabaz

    Cloud storage is insecure.  They scan your contents.  If Google or apple find something that they do not like, they will lock your account for as long as they want.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz 1 month ago in reply to BigG

    A couple of interesting USB drives (on top of portable CDROM drive that doesn't work with mobile devices : (

    The foreground one is "EX400U Survivor", which would be overkill if connected to an iPhone, but is very useful with a laptop, because it is speedy.. it's possible to run software directly from it (40 Gbit/sec connection!). 

    The blue one might have made more sense pre-cloud era.. supposedly ultra secure. However Cloud has the advantage of not being so easy to lose, and still ultra-secure. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz 1 month ago in reply to HKPhysicist

    iPhone users are a more complex demographic I reckon. I think more than anything, a big subset of them prefer simplicity, hence cloud is probably attractive, because it is one less thing to manage, carry, keep safe, upgrade, charge, and so on. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dang74
    0 dang74 1 month ago in reply to HKPhysicist
    HKPhysicist said:
    In the icloud digital monopoly scenario, if one does not pay a single month fee, all his digital creation will be locked.  If the subscriber bankrupts, Apple won't care about him.  It is a total loss from the icloud subscriber's viewpoint.

    Thanks for that.  I am an Android guy so I even took for granted that you were specifically talking about the Apple ecosystem when mentioned iCloud.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • BigG
    0 BigG 1 month ago in reply to HKPhysicist

    An AI comparison... basically a cut n paste from Google. I can vouch about the thermal dissipation issue. I updated an old laptop with Linux using a USB 3 memory stick. It got rather hot!

    So essentially USB Drives are faster. Maybe worth looking at USB host drivers combined with wireless.

    ---

    The performance gap between USB flash drives and microSD cards comes down to physical space, which dictates the complexity of their internal architecture. While a standard microSD card maxes out around 10–12 MB/s if it uses older Class 10 protocols, premium microSD cards can go faster. However, high-speed USB sticks sustain blistering speeds much more easily due to several structural advantages. [1, 2, 3, 4, 5]
    1. Multi-Channel Flash Controllers
    • USB Drives: The larger housing allows for complex, multi-channel memory controllers. Similar to a solid-state drive (SSD), these controllers can write data across multiple flash memory chips simultaneously (striping data), multiplying the write speed. [1, 2, 3]
    • microSD Cards: A microSD card contains a single, microscopic controller die squeezed next to the flash storage. It generally operates on a single channel, meaning it must process data sequentially rather than in parallel. [1, 2]
    2. High-Speed Bus Interfaces
    • USB Protocol: Modern flash drives use the USB 3.0 (or newer) standard, providing a massive interface bandwidth bottleneck of 5 Gbps (~500 MB/s) to 10 Gbps. [1, 2, 3, 4, 5]
    • SD Bus Protocol: Standard microSD cards rely on the UHS-I bus interface, which tops out theoretically at 104 MB/s. The cheaper, basic cards max out much lower (around 12.5 MB/s to 25 MB/s) because of hardware limitations. [1, 2, 3]
    3. Thermal Dissipation
    • USB Drives: Writing data at 130 MB/s generates substantial heat. The larger plastic or metal body of a USB drive acts as a heatsink to dissipate thermal energy, preventing the drive from thermal throttling. [1, 2]
    • microSD Cards: Squeezing heavy data transfers into a tiny fingernail-sized plastic form factor traps heat. Slower speeds prevent the card from melting or corrupting your data. [1, 2, 3, 4]
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • HKPhysicist
    0 HKPhysicist 1 month ago in reply to colporteur

    Yes, I am considering Microchip's WiFi SoC as they carries Microchip's secure chip ATECC608C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>