• Products and Partners
    Products and Partners
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
Member's Forum Audio amplifier
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 632 subscribers
  • Views 693 views
  • Users 0 members are here
Related

Audio amplifier

e14 Contributor
e14 Contributor over 10 years ago

I'm going to build a small amplifier to fit in a 1/12 scale model car to run three 1 inch 4ohm speakers. Are there any pcbs out there without making my own? I don't have the capabilities to making them.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 10 years ago

    Hi Joshua,

     

    The 'go-to' part is possibly an LM386, it is through-hole and standard spacing so a small piece of stripboard or perfboard can be used, no need for a custom PCB. You could wire all three speakers in series for it and use a single LM386 circuit.

    Or perhaps google can provide an off-the-shelf pre-soldered amplifier but as I understand you wish to build it, so using an LM386 is not a bad option.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 10 years ago

    Hi Joshua,

     

    The 'go-to' part is possibly an LM386, it is through-hole and standard spacing so a small piece of stripboard or perfboard can be used, no need for a custom PCB. You could wire all three speakers in series for it and use a single LM386 circuit.

    Or perhaps google can provide an off-the-shelf pre-soldered amplifier but as I understand you wish to build it, so using an LM386 is not a bad option.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz

    Great thank you, the reason for the pcb is the cleanliness I don't like the pref-board as it looks DIY. No One will see it when I finish unless I build its own case and different location and that's a possibility. It needed to be relatively small.