• Products and Partners
    Products and Partners
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
Member's Forum NZ Earthquake
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 632 subscribers
  • Views 2902 views
  • Users 0 members are here
Related

NZ Earthquake

mcb1
mcb1 over 9 years ago

Guys/Gals

Just a quick update on the major Earthquake that struck NZ north of Christchurch just after midnight.

 

They have decided that there was two quakes and they are still deciding if it was along the Hope faultline which runs SW to NE and forms the hills that are between the Southern Alps and the east coast.

It would seem that this triggered many others right up the North Island so the effects were felt widespread.

 

 

I'm in Chch and was up at the time. It went on for 2-3 mins which is much longer than the previous ones.

The closest place is Kaikoura and it has caused some damage to houses, but has currently cut the road link that goes up the east coast (State Highway 1), and damaged other roads that could form an alternative route.

 

There was a Tsuanami warning issued, but got downgraded to a coastal warning.

Unfortunately these warnings end up much less than predicted, so if we actually get a real one, then I'm afraid many will ignore it.

 

 

For those that haven't experienced Earthquakes, they can be very disturbing to some people.

There is often little/no warning and while it might be a little bit of shaking at first, you have no idea how long it will last, or if it will get worse.

 

 

NZ sits on the junction of two plates and one is going under the other. The movement is constant, but various bits get stuck and then suddenly release as the stress overcomes the friction.

This release often results in extra loading on another part and triggers an aftershock which can be almost as large.

So far there have been 50 or more aftershocks in and around the area, so you get no rest from them.

GeoNet - Quakes

As you can imagine you lose power, your house gets trashed and you get no rest, so it's quite stressful in the affected are.

 

 

The christchurch event in 2010 had around 14,000 aftershocks varying down to only just detectable without instruments.

So this will last for some days and it may trigger more events.

 

 

 

If you have friends and relatives in NZ, do try to make contact but appreciate that cellphone systems get overloaded and texts are the best way to contact them.

 

 

Cheers

Mark

  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    COMPACT over 9 years ago

    Hi Mark,

     

    It's good to know that you are safe.

     

    In recent times it seems that different parts of the faults are shifting causing havoc.

     

    I used to live in Wellington and was used to the frequent small tremors (Yes - I'm part Kiwi) and many may not know that NZ is very geologically young and frequently subject to these seismic events.

    Most of the houses in Wellington are made from timber to accommodate this movement.

    Christchurch on the other hand had many buildings made from masonry that can't withstand such movement and the area was subject to liquefaction.

     

    According to current theories NZ has been very active for the past 1.8 million years. Even today the plate boundaries move about 2-3 metres every century.

    NZ has quite a few Super volcanoes with the most obvious one being Lake Taupo in the centre of the North Island which apparently last erupted only 1,800 years ago and there is scientific speculation that it may erupt or its activity will cause a massive earthquake soon so much so that emergency protocols are being formulated.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 9 years ago

    Hi Mark,

     

    It's good to know that you are safe.

     

    In recent times it seems that different parts of the faults are shifting causing havoc.

     

    I used to live in Wellington and was used to the frequent small tremors (Yes - I'm part Kiwi) and many may not know that NZ is very geologically young and frequently subject to these seismic events.

    Most of the houses in Wellington are made from timber to accommodate this movement.

    Christchurch on the other hand had many buildings made from masonry that can't withstand such movement and the area was subject to liquefaction.

     

    According to current theories NZ has been very active for the past 1.8 million years. Even today the plate boundaries move about 2-3 metres every century.

    NZ has quite a few Super volcanoes with the most obvious one being Lake Taupo in the centre of the North Island which apparently last erupted only 1,800 years ago and there is scientific speculation that it may erupt or its activity will cause a massive earthquake soon so much so that emergency protocols are being formulated.