• Products and Partners
    Products and Partners
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
Member's Forum NZ Earthquake
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 632 subscribers
  • Views 2892 views
  • Users 0 members are here
Related

NZ Earthquake

mcb1
mcb1 over 9 years ago

Guys/Gals

Just a quick update on the major Earthquake that struck NZ north of Christchurch just after midnight.

 

They have decided that there was two quakes and they are still deciding if it was along the Hope faultline which runs SW to NE and forms the hills that are between the Southern Alps and the east coast.

It would seem that this triggered many others right up the North Island so the effects were felt widespread.

 

 

I'm in Chch and was up at the time. It went on for 2-3 mins which is much longer than the previous ones.

The closest place is Kaikoura and it has caused some damage to houses, but has currently cut the road link that goes up the east coast (State Highway 1), and damaged other roads that could form an alternative route.

 

There was a Tsuanami warning issued, but got downgraded to a coastal warning.

Unfortunately these warnings end up much less than predicted, so if we actually get a real one, then I'm afraid many will ignore it.

 

 

For those that haven't experienced Earthquakes, they can be very disturbing to some people.

There is often little/no warning and while it might be a little bit of shaking at first, you have no idea how long it will last, or if it will get worse.

 

 

NZ sits on the junction of two plates and one is going under the other. The movement is constant, but various bits get stuck and then suddenly release as the stress overcomes the friction.

This release often results in extra loading on another part and triggers an aftershock which can be almost as large.

So far there have been 50 or more aftershocks in and around the area, so you get no rest from them.

GeoNet - Quakes

As you can imagine you lose power, your house gets trashed and you get no rest, so it's quite stressful in the affected are.

 

 

The christchurch event in 2010 had around 14,000 aftershocks varying down to only just detectable without instruments.

So this will last for some days and it may trigger more events.

 

 

 

If you have friends and relatives in NZ, do try to make contact but appreciate that cellphone systems get overloaded and texts are the best way to contact them.

 

 

Cheers

Mark

  • Sign in to reply
  • Cancel
Parents
  • COMPACT
    COMPACT over 9 years ago

    That Paua photo is amazing!

     

    Paua is indigenous black abalone and is sold in NZ "Fush & Chup" shops as deep fried fritters. (Yum! I should pop on over to have some along with some Terakihi.)

    The inside lining of the shells are made into colourful jewellery commonly for Tikis and other souvenirs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • COMPACT
    COMPACT over 9 years ago

    That Paua photo is amazing!

     

    Paua is indigenous black abalone and is sold in NZ "Fush & Chup" shops as deep fried fritters. (Yum! I should pop on over to have some along with some Terakihi.)

    The inside lining of the shells are made into colourful jewellery commonly for Tikis and other souvenirs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to COMPACT

    Correct.

    You win the prize of as many Paua as you can legally collect.

     

    Paua and Crayfish (think Rock Lobster) are a staple fishery source in Kaikoura, and it attracts people from up and down the east coast to pop into the water to collect a feed. Without breeding stck the fishery will die.

    Thankfully the local fisherman have been actively removing them and placing them back on the rocks that are covered at low tide.

     

    This is a delicate operation as they are basically a very large muscle and any nick will kill them.

    They slither along the rocks so dropping them into the water and landing shell side down is also a death sentence.

     

    Along with paua they have also been rescuing fish stuck in pools and the odd crayfish which aren't used to being up on 'land'.

    image

     

    I also found these images taken further up the coast.

    image

       Look closely at the horizontal and vertical displacement where the driveway used to go past the house.!

     

      image image

    You can see that from this point (about 30km north of kaikoura) back toward kaikoura, the land and seabed has risen 2m.

     

      image

    That isn't Helicopter window distortion, it the same piece of displacement.

     

    Credit goes to the photographers and NBR list them on their post.

    https://www.facebook.com/NBROnline/?hc_ref=NEWSFEED

     

    and these guys

    https://www.facebook.com/NelsonMarlboroughRescueHelicopter/

     

     

    Cheers

    Mark