Member's Forum Trailer Lights Logic
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 632 subscribers
  • Views 1866 views
  • Users 0 members are here
  • logic
  • signal
  • light
  • brake
  • towing
  • trailer
Related

Trailer Lights Logic

ntewinkel
ntewinkel over 9 years ago

Hi all,

 

Remember this discussion (https://www.element14.com/community/message/201594/l/re-using-12v-at-base-of-transistor) a while back?

 

That's when I started a project involving a little travel trailer and trying to use a basic 4-wire wiring connection to properly light up separate brake and signal lights.

 

To sum up: the 4 wire connection from the car consists of: Ground, Marker lights (for night use), Left, and Right.

What that really means is that the brake and signal lights are combined in the 2 wires for left and right. Usually trailers just have a red light on the left and a red light on the right, and they do their thing.

 

But I bought fancy LED lights that separate out the brakes and the signal lights. Which left me trying to figure out if it was possible to do some logic to properly handle the brake and signal lights to their full potential... without rewiring the harness on the car!

 

I think I've found a way to do this using logic chips. And from what I can tell, the 4000 series chips will handle up to 18 volts, which is plenty to handle whatever the tow vehicle will throw my way.

 

I played around with it on this website I found (Simulator.io), and it seems to work like I want it to.

http://simulator.io/board/qQCIfvpreQ/3

1. If either the left or right wire is on, that orange indicator will go on, giving properly blinking

2. if both wires are on, the red brake lights go on, giving proper brake light function

3. if the brakes go on, the brake lights will remain on as long as there is power to the system (ie, at least one of the left or right wires has power)

4. if the brakes are on and one of the left or right wire goes off, then that indicator light goes one - essentially, the one side that's blinking will end up blinking but in reverse to how the car is blinking.

 

image

 

If you follow that URL above, you can play with the circuit - clicking on the "0" box beside the "Left" and "Right" inputs simulate the wire coming from the car.

 

I was going to test this using the 7400 series chips I have (using 5 volts and LEDs), but sadly I don't have any OR chips! (I'll have to fix that soon!). And making them from NAND chips looks to be very painful.

 

Here is my logic (edit: I had the wrong picture here earlier)

image

Special thanks goes to Michael Kellett michaelkellett for the idea of latching the brake lights ON and keeping it on until both wires are off.

And another special thanks goes to Douglas Wong dougw for the idea of putting together a logic truth table - that helped me get things straight in my mind, and gave me the idea to try using logic chips.

 

Anyway, what do you all think? Am I overlooking any potential problems?

 

ps, I think I also figured out a way to achieve this using just relays, but I figured solid state would be smaller and easier.

 

Thanks,

-Nico

 

edit: Note mostly to self: I have updated the trailer lights logic to now also reset when both blinker lights are off: https://simulator.io/board/qQCIfvpreQ/4

This allows the circuit to retain power and still function properly. The previous logic required power to be shut down in order to reset. The new logic allows battery or super-cap backup to keep it on.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 9 years ago

    Hello Nico,

     

    Generally when designing electronics for automotive use you should go for the following rough electrical spec:

     

    "12V" supply, 5 - 28V continuous, -12V continuous, system should work correctly 10V - 16V or more. 80V for 500mS

     

    Any input or port should stand spikes of perhaps 250V for 1us and static discharge, human body model, of at least 8kv.

     

    All this means is that your CMOS logic should be protected by a series resistor and shunt capacitor//zener diode on its power supply and that each logic input should be connected to a series R and a pair of diodes (one to ground and one to protected supply).

     

    You may need to filter the inputs to stop noise spikes form causing problems - which would mean adding shunt capacitors to the inputs (on the circuit side of the series R).

     

    I don't really like using feedback around gates but it may work OK - you'll need to test it. 4000 series logic is fine if you protect it - nice and slow.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • michaelkellett
    michaelkellett over 9 years ago

    Hello Nico,

     

    Generally when designing electronics for automotive use you should go for the following rough electrical spec:

     

    "12V" supply, 5 - 28V continuous, -12V continuous, system should work correctly 10V - 16V or more. 80V for 500mS

     

    Any input or port should stand spikes of perhaps 250V for 1us and static discharge, human body model, of at least 8kv.

     

    All this means is that your CMOS logic should be protected by a series resistor and shunt capacitor//zener diode on its power supply and that each logic input should be connected to a series R and a pair of diodes (one to ground and one to protected supply).

     

    You may need to filter the inputs to stop noise spikes form causing problems - which would mean adding shunt capacitors to the inputs (on the circuit side of the series R).

     

    I don't really like using feedback around gates but it may work OK - you'll need to test it. 4000 series logic is fine if you protect it - nice and slow.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 9 years ago in reply to michaelkellett

    "12V" supply, 5 - 28V continuous, -12V continuous, system should work correctly 10V - 16V or more. 80V for 500mS

    Ooh that does sound messy image

     

    The other way I was thinking of doing it was to convert the inputs to 5v using 2 LM7805 regulators (one for each input), and using 7400 series logic. The thinking was that the regulators will clean up the supply a bit. Looks like I'd still need the capacitor and zener diode to deal with spikes though.

     

    And, of course, in either case the outputs would be using transistors to switch the lights.

     

    Thanks for making me aware of exactly how messy the power can be. I was thinking it was give or take a few volts!

     

    Thanks,

    -Nico