• Products and Partners
    Products and Partners
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
Member's Forum Trailer Lights Logic
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 632 subscribers
  • Views 1928 views
  • Users 0 members are here
  • logic
  • signal
  • light
  • brake
  • towing
  • trailer
Related

Trailer Lights Logic

ntewinkel
ntewinkel over 9 years ago

Hi all,

 

Remember this discussion (https://www.element14.com/community/message/201594/l/re-using-12v-at-base-of-transistor) a while back?

 

That's when I started a project involving a little travel trailer and trying to use a basic 4-wire wiring connection to properly light up separate brake and signal lights.

 

To sum up: the 4 wire connection from the car consists of: Ground, Marker lights (for night use), Left, and Right.

What that really means is that the brake and signal lights are combined in the 2 wires for left and right. Usually trailers just have a red light on the left and a red light on the right, and they do their thing.

 

But I bought fancy LED lights that separate out the brakes and the signal lights. Which left me trying to figure out if it was possible to do some logic to properly handle the brake and signal lights to their full potential... without rewiring the harness on the car!

 

I think I've found a way to do this using logic chips. And from what I can tell, the 4000 series chips will handle up to 18 volts, which is plenty to handle whatever the tow vehicle will throw my way.

 

I played around with it on this website I found (Simulator.io), and it seems to work like I want it to.

http://simulator.io/board/qQCIfvpreQ/3

1. If either the left or right wire is on, that orange indicator will go on, giving properly blinking

2. if both wires are on, the red brake lights go on, giving proper brake light function

3. if the brakes go on, the brake lights will remain on as long as there is power to the system (ie, at least one of the left or right wires has power)

4. if the brakes are on and one of the left or right wire goes off, then that indicator light goes one - essentially, the one side that's blinking will end up blinking but in reverse to how the car is blinking.

 

image

 

If you follow that URL above, you can play with the circuit - clicking on the "0" box beside the "Left" and "Right" inputs simulate the wire coming from the car.

 

I was going to test this using the 7400 series chips I have (using 5 volts and LEDs), but sadly I don't have any OR chips! (I'll have to fix that soon!). And making them from NAND chips looks to be very painful.

 

Here is my logic (edit: I had the wrong picture here earlier)

image

Special thanks goes to Michael Kellett michaelkellett for the idea of latching the brake lights ON and keeping it on until both wires are off.

And another special thanks goes to Douglas Wong dougw for the idea of putting together a logic truth table - that helped me get things straight in my mind, and gave me the idea to try using logic chips.

 

Anyway, what do you all think? Am I overlooking any potential problems?

 

ps, I think I also figured out a way to achieve this using just relays, but I figured solid state would be smaller and easier.

 

Thanks,

-Nico

 

edit: Note mostly to self: I have updated the trailer lights logic to now also reset when both blinker lights are off: https://simulator.io/board/qQCIfvpreQ/4

This allows the circuit to retain power and still function properly. The previous logic required power to be shut down in order to reset. The new logic allows battery or super-cap backup to keep it on.

  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 9 years ago

    Somehow I missed this part of the discussion.

     

    I was due to have a similar issue, where here in NZ we use the seperate indicator lights, but american cars combine everything.

     

    I spent some considerable time trying to work it out, and in the end opted to just buy one of these.

    https://www.amazon.com/Tow-Ready-118158-Taillight-Converter/dp/B001GKQZQG

     

    I haven't tried it ... that car got killed before the tow bar went on, and I'm still deciding whether to add one to the replacement.

     

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    I might go that route if my project doesn't succeed.

     

    It's $40 CAD on the Canadian Amazon site, so that's not too bad.

     

    But I've come this far to not at least try it out image

     

    ps, I bought some TVS diodes (transient voltage suppressors), which appear to function like zener diodes but can handle far higher amperage (or else I just bought zener diodes by another name, haha).

    So I hope that, coupled with some capacitors, will save the chips from the worst, but I'm willing to take some chances.

     

    I'll wire it up so that if all fails I can just default back to the red turn/stop lights.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 9 years ago in reply to mcb1

    I might go that route if my project doesn't succeed.

     

    It's $40 CAD on the Canadian Amazon site, so that's not too bad.

     

    But I've come this far to not at least try it out image

     

    ps, I bought some TVS diodes (transient voltage suppressors), which appear to function like zener diodes but can handle far higher amperage (or else I just bought zener diodes by another name, haha).

    So I hope that, coupled with some capacitors, will save the chips from the worst, but I'm willing to take some chances.

     

    I'll wire it up so that if all fails I can just default back to the red turn/stop lights.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mcb1
    mcb1 over 9 years ago in reply to ntewinkel

    I might go that route if my project doesn't succeed.

    I spent a lot of time coming up with the logic required for this.

    At some point I decided it needed a latch and I hadn't even got to Brake lights plus Hazard lights on.

     

    They don't run any extra power and it handles incandescent and LED lighting.

     

     

    I figured I had more projects than I could finish in my lifetime, and I really didn't need to emabrk on this one.

    Mark