Member's Forum What beginners mistakes have I made?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 1685 views
  • Users 0 members are here
Related

What beginners mistakes have I made?

mpiechotka
mpiechotka over 8 years ago

Sorry if this is incorrect forum/basic question. While I have a background in programming and some experience with FPGAs the I didn't know much about EE before. I run into a hobby project for which I'd like to create a PCB and soon I found myself in deep waters. So I decided to step back and create a simple PCB to learn basics. I tried to create a simple AVR board with an GPIO header, JTAG connector and USB-to-UART bridge. I've created something but I'm sure I've done many basic mistakes and strange decisions so I'd be grateful for pointing them out.

 

PS. I know there is no power switch but I couldn't find one on with eagle library.

image

image

image

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 8 years ago

    Not sure how important this is, but the FT230X documentation calls for 27 ohm resistors inline on on the D+ and D- lines.  Also, I am not sure that on the FT230X, that the VCC pin should be tied to the VCCIO and 3V3OUT pins.  Power should be connected to VCC (with a 0.1uF bypass cap to ground) and VCCIO, RESET and 3V3OUT should be connected together with another 0.1uF cap to ground.  I would also add a diode between the power jack and the regulator for reverse power protection.

     

    Good luck with your project!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago

    Not sure how important this is, but the FT230X documentation calls for 27 ohm resistors inline on on the D+ and D- lines.  Also, I am not sure that on the FT230X, that the VCC pin should be tied to the VCCIO and 3V3OUT pins.  Power should be connected to VCC (with a 0.1uF bypass cap to ground) and VCCIO, RESET and 3V3OUT should be connected together with another 0.1uF cap to ground.  I would also add a diode between the power jack and the regulator for reverse power protection.

     

    Good luck with your project!

    Gene

    • Cancel
    • Vote Up +3 Vote Down