• Products and Partners
    Products and Partners
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
Member's Forum What beginners mistakes have I made?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 1714 views
  • Users 0 members are here
Related

What beginners mistakes have I made?

mpiechotka
mpiechotka over 8 years ago

Sorry if this is incorrect forum/basic question. While I have a background in programming and some experience with FPGAs the I didn't know much about EE before. I run into a hobby project for which I'd like to create a PCB and soon I found myself in deep waters. So I decided to step back and create a simple PCB to learn basics. I tried to create a simple AVR board with an GPIO header, JTAG connector and USB-to-UART bridge. I've created something but I'm sure I've done many basic mistakes and strange decisions so I'd be grateful for pointing them out.

 

PS. I know there is no power switch but I couldn't find one on with eagle library.

image

image

image

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 8 years ago

    By the way Maciej, since you're using EAGLE, be sure to run the design rules check (DRC) too, and also _never_ forget to type 'run length' in the EAGLE command line, before you feel you are ready to submit the PCB to the factory (you'll only make this mistake once : ) That command will tell you if you've forgotten to route an air-wave.

    I'm not very good at intuitively routing PCBs, so for me what works is approximately routing things, and then ripping up and re-routing traces to tidy them up. Basically I manually do two passes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    By the way Maciej, since you're using EAGLE, be sure to run the design rules check (DRC) too, and also _never_ forget to type 'run length' in the EAGLE command line, before you feel you are ready to submit the PCB to the factory (you'll only make this mistake once : ) That command will tell you if you've forgotten to route an air-wave.

    I'm not very good at intuitively routing PCBs, so for me what works is approximately routing things, and then ripping up and re-routing traces to tidy them up. Basically I manually do two passes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mpiechotka
    mpiechotka over 8 years ago in reply to shabaz

    I knew and use DRC - you can often download DRU files from PCB manufacturers websites to get more specific rules for that particular one.

     

    While looking for the command I run into length_freq_ri and my 3.3 V signal (from current iteration of board) has R of 861.49 mOhm (I don't think the tool have 5 s.f. accuracy and at least 3 numbers are 'fake'?) and GND, despite being pour, 156.43 mOhm. Are those numbers reasonable or should I be worried (I don't know how much 'resistance' IC has[1])

     

    [1] I put in quotes as I know IC are not linear so word resistance doesn't really applies here.