• Products and Partners
    Products and Partners
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
Member's Forum What beginners mistakes have I made?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 632 subscribers
  • Views 1712 views
  • Users 0 members are here
Related

What beginners mistakes have I made?

mpiechotka
mpiechotka over 8 years ago

Sorry if this is incorrect forum/basic question. While I have a background in programming and some experience with FPGAs the I didn't know much about EE before. I run into a hobby project for which I'd like to create a PCB and soon I found myself in deep waters. So I decided to step back and create a simple PCB to learn basics. I tried to create a simple AVR board with an GPIO header, JTAG connector and USB-to-UART bridge. I've created something but I'm sure I've done many basic mistakes and strange decisions so I'd be grateful for pointing them out.

 

PS. I know there is no power switch but I couldn't find one on with eagle library.

image

image

image

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    michaelkellett over 8 years ago

    Things you might consider:

     

    1) use a ground plane on the lower (non component side) of the baord.

    2) keep all the components on one side (if you will hand solder a couple of prototypes this doesn't matter but for production it always costs more to populate both sides.)

    3) don't ever make sharp V shapes with track - it causes problems in etching

    4) try to take tracks out of sm components on axis and the same for all

    5) you have some very thin tracks and some tiny vias - you don't need to use such aggressive design rules a board like this.

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • mpiechotka
    mpiechotka over 8 years ago in reply to michaelkellett

    Thanks Michael

     

    AD 3. Thanks - I haven't realized that one - the explanations I read was about current flow which is why I tried to kept angles for flow <45°.

     

    AD 4. Sorry - I have no clue what you mean.

     

    AD 5. I use default 6 mils for signals and for power/ground signals that supply a lot of components I choose 20. I'm not sure what to choose if default are not correct - obviously the thinner the track the less conductivity it has and I know I could calculate in principle the resistance but probably there are some good rules of thumb.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to mpiechotka

    Hi Maciej,

     

    Its easiest if you can find some example physical PCBs, and examine them closely, to see patterns to follow.

    Here is an example.

    Position 1 is a pad belonging to an IC. You can see that the trace marked 2 comes off at a nice angle (zero degrees) before it bends at position 3.

    Similarly, look at the pad marked 4. This belongs to a surface mount resistor or capacitor. Again, the trace comes off at a nice angle (zero degrees) before it gets bent near position 5, and then disappears off into a via shown in green.

     

    Similarly, position 6 shows a capacitor. Here the trace comes off at 90 degrees before it bends at any other angle.

    Now look to position 7. This is a through-hole pad for a dual-in-line header, like you are using in your design. Here there was not enough room to easily come off at zero or 90 degrees, so 45 degrees was used, but exactly through the centre of the pad, as if the pad were a clock face, and the trace was one of the clock hands, starting at the centre of the pad. In other words, don't bring a trace to a through-hole pad in a way that the trace and pad together look like a music note (or golf club) shape combined.

     

    Also, 6 mil is unnecessary for your design. The example PCB below is more dense than yours, and all the visible traces are nearly all 10mil (with a few that are 8mil, you can just about see the difference widths if you look closely). There are no 6mil traces here.

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    That is look great I like that you entered the  FT230XSFT230XS from the opposite side thus avoiding the crossover vias very nice(I may have to try that if I re-layout my board

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mpiechotka
    mpiechotka over 8 years ago in reply to genebren

    Thanks. I think I'm starting getting the basic rules (I restructured the board so it fits in 2" x 3").

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    This is looking a lot better.  Funny, that the pin-out of the microUSB and FT230X require a crossover on the D+/D- signals.  I used the same combination recently and was annoyed that I had to use vias to cross the two signals.

    Looking good!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    This is looking a lot better.  Funny, that the pin-out of the microUSB and FT230X require a crossover on the D+/D- signals.  I used the same combination recently and was annoyed that I had to use vias to cross the two signals.

    Looking good!

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    That is look great I like that you entered the  FT230XSFT230XS from the opposite side thus avoiding the crossover vias very nice(I may have to try that if I re-layout my board

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mpiechotka
    mpiechotka over 8 years ago in reply to genebren

    Thanks. I think I'm starting getting the basic rules (I restructured the board so it fits in 2" x 3").

    image

    • Cancel
    • Vote Up +3 Vote Down