Member's Forum How to manage a power-on/off sequence
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 631 subscribers
  • Views 529 views
  • Users 0 members are here
Related

How to manage a power-on/off sequence

mpiechotka
mpiechotka over 8 years ago

Simple ICs can be just connected almost directly to power source . However more complicated ones have rules about various supplied voltages such as that VCC_0 needs to be stable first before VCC_1 reaches certain level. While I'm aware that I can delay voltage by resistor and capacitor I think there are <blank> IC which allows to do it much more reliably. However I cannot find information about them as I don't know how <blank> are called.

  • Sign in to reply
  • Cancel
Parents
  • mpiechotka
    mpiechotka over 8 years ago

    It looks like I found such system under name of Power Manage IC (PMIC). I'm still not clear about the difference between DCDC output and LDO though...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    DCDC includes a lot of possible devices, but typically it refers to a device that used high speed switching and a storage element (inductor or capacitor) to more efficiently generate a DC voltage.  This can be used to either generate a higher or lower voltage than the input to the device.  LDO (Low Drop Out) regulators are a specialized form of regulator that is designed to have a low inline voltage drop (across the device), usually < 1.0V.  As with any linear regulator, the difference between the input and the output is drop across the device.  This voltage drop times the current flow, equal the power dissipated in the device.  DCDC do not suffer from this same power dissipation, as the duty cycle of the switching lowers the power dissipation as current is only flowing through the device for very short periods of the switching frequency.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • genebren
    genebren over 8 years ago in reply to mpiechotka

    DCDC includes a lot of possible devices, but typically it refers to a device that used high speed switching and a storage element (inductor or capacitor) to more efficiently generate a DC voltage.  This can be used to either generate a higher or lower voltage than the input to the device.  LDO (Low Drop Out) regulators are a specialized form of regulator that is designed to have a low inline voltage drop (across the device), usually < 1.0V.  As with any linear regulator, the difference between the input and the output is drop across the device.  This voltage drop times the current flow, equal the power dissipated in the device.  DCDC do not suffer from this same power dissipation, as the duty cycle of the switching lowers the power dissipation as current is only flowing through the device for very short periods of the switching frequency.

     

    Gene