• Products and Partners
    Products and Partners
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
Member's Forum game showbuzzer
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 632 subscribers
  • Views 639 views
  • Users 0 members are here
  • gameshow buzzer issues
Related

game showbuzzer

sluga
sluga over 8 years ago

i have made a 5 player lockout gameshow buzzer

im using a audrino uno

audrino is hooked up to a breadboard with 5 v from audrino goint to it

all 5 buttons have 1.3kohm risisters on them

the reset is on pin 2

ad does not go to the breadboard  but goes straight to the button with earth pin 14 i think ?

all buttons are hooked to each box through a rj45 keystone

all buttons work fine

BUT as soo as my hand goes anywhere near the reset switch it triggers  the reset button

touching the reset box,putting hand anywhere within 4 inches of reset box triggers the reset switch

WHAT IS MY SOLUTION

any help would be great

can attach the buzzer code if needed

peter

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • mcb1
    mcb1 over 8 years ago

    can attach the buzzer code if needed

    That would be helpful.

    The Inputs either need a pullup, or pulldown resistor externally, OR you can define it in the software under setup().

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • sluga
    sluga over 8 years ago in reply to mcb1

    it would be great if i could add solution through cod as ive mounted it in box damn but i can always pull it out its only mouneted lightly

    Attachments:
    quiz-game-buttons-master.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to sluga

    sluga

    To insert code ... paste it in, then highlight it and select the >> on the menu.

    Select Syntax Highlighting and then C++.

     

    //This code was written by Bob Clagett for I Like To Make Stuff - 2016
    //It accompanies the project at http://www.iliketomakestuff.com/make-quiz-game-buttons
    //This is for a simple 4 player quiz game setup.
    //Only one button will light at a time, until the reset button is pressed.
    //The reset button turns off all LEDs and sets everything up for the next "round".
    
    ///Define Buttons
    //Reset Button
    int resetButtonPin = 2;
    
    //Button1
    int button1Pin = 13;
    int led1Pin = 12;
    int button1State = 0; 
    
    //Button2
    int button2Pin = 11;
    int led2Pin = 10;
    int button2State = 0; 
    
    //Button3
    int button3Pin = 9;
    int led3Pin = 8;
    int button3State = 0; 
    
    //Button4
    int button4Pin = 7;
    int led4Pin = 6;
    int button4State = 0; 
    
    int resetButtonState = 0;
    boolean pollingForPresses = 1;
    
    int lastbutton1State = LOW;
    int lastbutton2State = LOW;
    int lastbutton3State = LOW;
    int lastbutton4State = LOW;
    int lastResetState = LOW;
    
    void setup() {
      Serial.begin(9600);
      // initialize the LED pin as an output:
      pinMode(led1Pin, OUTPUT);
      pinMode(led2Pin, OUTPUT);
      pinMode(led3Pin, OUTPUT);
      pinMode(led4Pin, OUTPUT);
      // initialize the pushbutton pin as an input:
      pinMode(resetButtonPin, INPUT);
      pinMode(button1Pin, INPUT);
      pinMode(button2Pin, INPUT);
      pinMode(button3Pin, INPUT);
      pinMode(button4Pin, INPUT);
    }
    
    void loop() {
    
      int reading1 = digitalRead(button1Pin);
      int reading2 = digitalRead(button2Pin);
      int reading3 = digitalRead(button3Pin);
      int reading4 = digitalRead(button4Pin);
      int readingReset = digitalRead(resetButtonPin);
    
        if(pollingForPresses==1){
          //Button 1
          if (reading1 != button1State && reading1 != lastbutton1State) {
            button1State = reading1;
            button1State = digitalRead(button1Pin);
              
                  if (button1State == HIGH) {
                    // turn LED on:
                      Serial.print("Button 1 ON");
                    digitalWrite(led1Pin, HIGH);
                    pollingForPresses = 0;
                  }
             button1State = 0;
          }
       
          //Button 2
          if (reading2 != button2State && reading2 != lastbutton2State) {
            button2State = reading2;
            button2State = digitalRead(button2Pin);
              
                  if (button2State == HIGH) {
                    // turn LED on:
                      Serial.print("Button 2 ON");
                    digitalWrite(led2Pin, HIGH);
                    pollingForPresses = 0;
                  }
             button2State = 0;
          }
    
          //Button 3
          if (reading3 != button3State && reading3 != lastbutton3State) {
            button3State = reading3;
            button3State = digitalRead(button3Pin);
              
                  if (button3State == HIGH) {
                    // turn LED on:
                      Serial.print("Button 3 ON");
                    digitalWrite(led3Pin, HIGH);
                    pollingForPresses = 0;
                  }
             button3State = 0;
          }
    
          //Button 4
          if (reading4 != button4State && reading4 != lastbutton4State) {
            button4State = reading4;
            button4State = digitalRead(button4Pin);
              
                  if (button4State == HIGH) {
                    // turn LED on:
                      Serial.print("Button 4 ON");
                    digitalWrite(led4Pin, HIGH);
                    pollingForPresses = 0;
                  }
             button4State = 0;
          }
          
        }
       //Check reset button
       
        if (pollingForPresses==0) {
        
          if (readingReset != resetButtonState && readingReset != lastResetState) {
                  resetButtonState = digitalRead(resetButtonPin);
              
                  if (resetButtonState == HIGH) {
                    Serial.print("Reset button HIGH");
                    resetButtons();
                  }
             
             resetButtonState = 0;
          }
        }
      lastResetState = readingReset;
      lastbutton1State = reading1;  
      lastbutton2State = reading2;
      lastbutton3State = reading3;  
      lastbutton4State = reading4;
    }
    
    
    void resetButtons() {
      
      lastbutton1State = 0;
      lastbutton2State = 0;
      lastbutton3State = 0;
      lastbutton4State = 0;
      resetButtonState = 0;
      lastResetState = 0;
      
      button1State = 0;
      button2State = 0;
      button3State = 0;
      button4State = 0;
      
      Serial.print("All the Buttons where reset!");
      
      digitalWrite(led1Pin, LOW);
      digitalWrite(led2Pin, LOW);
      digitalWrite(led3Pin, LOW);
      digitalWrite(led4Pin, LOW);
      digitalWrite(resetButtonPin, LOW);
      
      pollingForPresses = 1;
    }

     

     

    The first issue is Pin13 is normally the one with an onboard LED.

    Using it as button1 will cause issues.

    I'd suggest swapping the LED and the button.

     

    I was wrong about the internal pull down resistor ... sorry.

    The Atmel328 has 50k pullups internally.

     

    If your bttons are connected to a common point, you could change this from +5v and make it ground.

    You'd need to enable the pull-ups and invert the code at lines like this if (button1State == HIGH) to if (button1State == LOW)

     

    Sorry if I got your hopes up. I always have buttons between the pin and ground.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • sluga
    sluga over 8 years ago in reply to mcb1

    ok added risistors to reset

    looks like 3 buttons work now

    and 2 faulty keystone connectors are the problem now

    so thanks for now the reset button NOW WORKS EXCELLENT

    and when i get time ill do the 2 faulty keystones

    BUT 3 IS GOOD FOR NOW

    thanks

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • sluga
    sluga over 8 years ago in reply to mcb1

    ok added risistors to reset

    looks like 3 buttons work now

    and 2 faulty keystone connectors are the problem now

    so thanks for now the reset button NOW WORKS EXCELLENT

    and when i get time ill do the 2 faulty keystones

    BUT 3 IS GOOD FOR NOW

    thanks

    • Cancel
    • Vote Up +3 Vote Down