• Products and Partners
    Products and Partners
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
Member's Forum Unexpected voltage at base of transistor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 631 subscribers
  • Views 947 views
  • Users 0 members are here
Related

Unexpected voltage at base of transistor?

Sean_Miller
Sean_Miller over 7 years ago

I have a situation I hadn't encountered before that is really bringing out my inner "noob".  Below is a circuit I'm developing for one of my 4D Game Engine IoT devices (future Element14 Presents video).

 

The simple question is - would one expect to see a voltage at an open base of a transistor?

 

Here's the details:

The SV1 is a 2x4 female header to plug in a ESP8266.  JP1 receives a 9V battery.  IC1 and IC2 are regulating down to 5Vs and then to 3.3V.

 

With the ESP8266 not installed, I probe pin three (the transistor base) to ground, I get 1.5 volts.  For that pin, if the ESP8266 sees voltage on power on, it will enter its bootloader mode.  In turn, its made the pin not an option to trigger the transistor because the voltage is instantly there when powered on and the circuit will be "bricked".

 

Is it normal to see a voltage on an base?  I rebuilt the board from scratch and breadboarded it just to ensure it wasn't a short, but the problem persisted.  I also added a 10K at the base hoping to "pull it down", but it did nothing for it.

 

image

 

 

My solution, of course, was to use another pin, but I sure would like to have that one for other projects in the future.

 

Thanks,

Sean

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    If I'm reading it right, the 10K base resistor you tried should have pulled the base right to ground.

    If there is 1.5V on the base there is something very wrong - as in blown transistor - the base should not be able to exceed about 0.7V because the base-emitter diode will conduct above that voltage.

    If pin3 on SV1 is an output, the base can only be driven up to 0.7V so it needs a current limiting resistor between pin 3 and the base.

    I would use a FET like a BSS138 or a 2N7000 instead of the  2N22222N2222 where a high value resistor would be sufficient to pull the gate down

    A series base resistor will work with the  2N22222N2222 but you probably also want a pull down on the base to make sure the transistor is off when the base is floating

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to dougw

    I realized my original sketch didn't show the resistor to the base, but had a 1K there.  However, I didn't have a flyback diode on the relay.  That could have been eating transistors on me.

     

    My 10K pull down resistor was totally backwards thinking for my problem.  What I needed was a pull up which a lot of people have said have worked for the ESP8266.  However, I could not get it to work.  The pull up resistor would simply trigger the transistor and keep it there despite what the code was doing.

     

    So here is the circuit now, but I will loop back to try your FET suggestion at some point as the switch solution is goofy.

    image

     

    Thanks for the help!

    Sean

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to dougw

    I realized my original sketch didn't show the resistor to the base, but had a 1K there.  However, I didn't have a flyback diode on the relay.  That could have been eating transistors on me.

     

    My 10K pull down resistor was totally backwards thinking for my problem.  What I needed was a pull up which a lot of people have said have worked for the ESP8266.  However, I could not get it to work.  The pull up resistor would simply trigger the transistor and keep it there despite what the code was doing.

     

    So here is the circuit now, but I will loop back to try your FET suggestion at some point as the switch solution is goofy.

    image

     

    Thanks for the help!

    Sean