• Products and Partners
    Products and Partners
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
Member's Forum Unexpected voltage at base of transistor?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 631 subscribers
  • Views 947 views
  • Users 0 members are here
Related

Unexpected voltage at base of transistor?

Sean_Miller
Sean_Miller over 7 years ago

I have a situation I hadn't encountered before that is really bringing out my inner "noob".  Below is a circuit I'm developing for one of my 4D Game Engine IoT devices (future Element14 Presents video).

 

The simple question is - would one expect to see a voltage at an open base of a transistor?

 

Here's the details:

The SV1 is a 2x4 female header to plug in a ESP8266.  JP1 receives a 9V battery.  IC1 and IC2 are regulating down to 5Vs and then to 3.3V.

 

With the ESP8266 not installed, I probe pin three (the transistor base) to ground, I get 1.5 volts.  For that pin, if the ESP8266 sees voltage on power on, it will enter its bootloader mode.  In turn, its made the pin not an option to trigger the transistor because the voltage is instantly there when powered on and the circuit will be "bricked".

 

Is it normal to see a voltage on an base?  I rebuilt the board from scratch and breadboarded it just to ensure it wasn't a short, but the problem persisted.  I also added a 10K at the base hoping to "pull it down", but it did nothing for it.

 

image

 

 

My solution, of course, was to use another pin, but I sure would like to have that one for other projects in the future.

 

Thanks,

Sean

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    If I'm reading it right, the 10K base resistor you tried should have pulled the base right to ground.

    If there is 1.5V on the base there is something very wrong - as in blown transistor - the base should not be able to exceed about 0.7V because the base-emitter diode will conduct above that voltage.

    If pin3 on SV1 is an output, the base can only be driven up to 0.7V so it needs a current limiting resistor between pin 3 and the base.

    I would use a FET like a BSS138 or a 2N7000 instead of the  2N22222N2222 where a high value resistor would be sufficient to pull the gate down

    A series base resistor will work with the  2N22222N2222 but you probably also want a pull down on the base to make sure the transistor is off when the base is floating

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to dougw

    Ok...Got the FET installed and now all is well!

     

    I needed at least 5V to get the relay to pull in so I used the FET at 3.3V to switch a  2N22222N2222 transistor This arrangement isolated pin 3 from being pulled down at boot up allowing an added 10K pull up resistor to keep the pin high allowing it to boot to my flashed code So now this IoT circuit can switch on AC or DC appliances over the web running on a battery or power source anywhere from 5V-15V DC

     

     

    image

     

    The board turned out pretty sleek:

     

    With ESP8266:

    image

     

    With ESP8266 removed:

    image

     

    See ya',

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to dougw

    Ok...Got the FET installed and now all is well!

     

    I needed at least 5V to get the relay to pull in so I used the FET at 3.3V to switch a  2N22222N2222 transistor This arrangement isolated pin 3 from being pulled down at boot up allowing an added 10K pull up resistor to keep the pin high allowing it to boot to my flashed code So now this IoT circuit can switch on AC or DC appliances over the web running on a battery or power source anywhere from 5V-15V DC

     

     

    image

     

    The board turned out pretty sleek:

     

    With ESP8266:

    image

     

    With ESP8266 removed:

    image

     

    See ya',

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Sean_Miller
    Sean_Miller over 7 years ago in reply to Gough Lui

    Thanks for linking.  I have seen these.  Ebay definitely has some good gizmos at a fair price out there.  However, I recently got burned on a power supply that claimed to be good for 40V to step down to 3.3V, though.  It shorted through and toasted my MRK1000.

     

    My current obsessions are a bit retro.  I want to understand the analog world as best as I can while growing my code & circuit design blocks to later build bigger single boards for our projects.

     

    See ya',

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 7 years ago in reply to Sean_Miller

    A bit late to the party myself - but I'm not sure if you're aware of these cheap boards on eBay:

    https://www.ebay.com.au/itm/5V-ESP8266-ESP-01S-Relay-Module-Remote-Switch-Phone-APP-DIY-Kit-Project-Design/282743533090?…

     

    Basically, an ESP-01 module, a relay, voltage regulator and a transistor and resistors on a PCB for AU$1.88. You can reprogram the ESP-01 to whatever you'd like and at that price, it's a lot of fun. Of course, I'm not discouraging people from designing their own and  learning in the process - but at that price, it's hard to want to deal with the headaches ... although delivery is often a bit of an issue with goods sourced from China as it can take forever and incur some customs duties.

     

    - Gough

     

    EDIT: Actually the one above doesn't include the ESP-01 module itself.

    https://www.ebay.com.au/itm/ESP8266-ESP-01S-5V-Wifi-Relay-Module-TOI-APP-Controled-For-Smart-Home/282649817635?hash=item…

    The one with the module is about AU$4.06. Still absurdly cheap if you ask me image. I've actually got a few of these on hand but haven't had the chance to put it into good use yet.