• Products and Partners
    Products and Partners
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
Member's Forum TTL Video Chip
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 631 subscribers
  • Views 364 views
  • Users 0 members are here
Related

TTL Video Chip

2-zons
2-zons over 7 years ago

I'm working on a 68000 home-brew computer.  I'm in the very early stages (planning, and acquiring parts).  I plan on building an 8 bit system as a pre-cursor to the 68K 16 bit one as a bit of a warm-up / refresher.  My plan is to use the 6809 for the first system.  Can anyone suggest a chip that I could use as a video device for the 8 bit system?  Something that works at TTL levels and is relatively simple to program and interface with.   I thought of using a 6567 Vic II from a commodore 64, but those are hard to get.  If I can get one I might try it, but ideally i would like something with a more capabilities, and possibly a VGA, or even HDMI output.  I know that might be a tall order and I'm willing to live with composite video if there is something i can get easily.

 

Thanks

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 7 years ago

    Try an MC6847. Still available on Ebay.

    Apparently the prototype TRS-80 Color Computer (which used an MC6809 CPU) also used an MC6847 for display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • 2-zons
    2-zons over 7 years ago in reply to dougw

    That just might work for the 6809 system.  Thhe TRS-80 CoCo used the 6809 as well.  It would be a bit limited for the 68000 system however, but I did find a potential candidate for that.

     

    VLSI Solution-VS23S040 - 4 Mbit Versatile SPI / 8-Bit Parallel Bus SRAM

     

    A memory chip with built in video controller.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 2-zons
    2-zons over 7 years ago in reply to dougw

    That just might work for the 6809 system.  Thhe TRS-80 CoCo used the 6809 as well.  It would be a bit limited for the 68000 system however, but I did find a potential candidate for that.

     

    VLSI Solution-VS23S040 - 4 Mbit Versatile SPI / 8-Bit Parallel Bus SRAM

     

    A memory chip with built in video controller.