Member's Forum PCB-RULER Project --- a ruler to rule them all
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 634 subscribers
  • Views 1999 views
  • Users 0 members are here
  • pcb-ruler
  • vcp
Related

PCB-RULER Project --- a ruler to rule them all

mayermakes
mayermakes over 7 years ago

EDIT: added more photos of other rulers!

So as dissused in the latest call, we want to do b project that revolves around designing and manufacturing a handy PCB-Ruler. like the one I showed on stream.

 

Here are some pictures and some ideas for it:

this specimen has a header for RPI with pinout on it, every usable GPIO leads to a pad where you can solder smd resistors and leds onto it to have indication of pin state

image

Also some general cheatsheets for raspbian and desing references are marked, the holes act as drill guides if you want to mount your rpi inside something

image

I'd find it handy  to add a function like this header extender, but solid and tidier to attach a breadboard directly to the pi, or beaglebone or arduino..

image

A debug board of some sorts would be handy, imagine pluging an arduino (like on the pic) into it and having a breadboard interface and leds to indicate pinstates on it

image

this one shows footprints for pcb designs

image

references for mechanical and pcb design as well a schematic cheatsheet

image

image

image

Because we talked about doing this as a community project I'd have the following suggestion:

 

Everybody and his grandma has done a ruler to rule them all (AvE has the best one/ and most offensive one without a doubt) we need enough space to do something cool on it (thus creating an interesting video(series?)).and doing multiple sections would make it very long and inconvenient(+expensive)
So I'd opt for a PCB-triangle-ruler,  that means more space for everybody. for example 3 VCPs everybody gets one corner, the middle is e14 presents branded. metric and freedom units + funny made up ones. (for example a dot as reference of a plank-lenght)

If we have more than 3 willing VCPs we could let the community vote on which corners should be present on the final production unit. a BOM (one click cart) should be provided so users can populate it themselves if they get one as a giveaway.
I'd prefer to focus on the abuility to plug in an sbc or MCU + provdide code that uses the functionality of the design.

 

I'll also add a poll on which software you people use for pcbs, because it would be much easier to combine everything when we usd the same software suite.

please add your ideas to the comments.

Some guidelines I made up:

Function should be there even if no parts are soldered onto it.
MCUS etc should be for plug in

everything should be hand solderable (except if you want to do an smd challenge corner)

keep parts on one side only to ensure the ruler still lays flat when populated.

  • Sign in to reply
  • Cancel
  • e14phil
    e14phil over 7 years ago

    For further inspiration

    image

    "I have been fascinated with systems like the Altair 8800 for some time now and decided to up-the-anti with my second iteration of the Digirule by making a programmable binary computer built into a PCB ruler."

     

    https://bradsprojects.com/digirule2/

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to kk99

    8-O

     

    If only I had known about this before setting off to build my Altair!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kk99
    kk99 over 7 years ago

    Here is another example of ruler:
    https://hackaday.com/2019/03/02/programmable-ruler-keeps-1970s-computing-alive/

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to airbornesurfer

    oOoh a hinged PCB - that's spicy

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago in reply to cstanton

    And a compass! Don't forget the compass!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    A strain gauge would be something fun to include and used in the following way to weigh small items. Place ruler on the edge of a table at the marked point (perhaps 100mm coverage of table) - and then at the end place the item to weigh. How that is used would be up to the firmware setup.

     

    A small load cell like those in the Sixth Sense Challenge might be interesting as well.

     

    On that note, a place for the STMicroelectronics SensorTile from the above challenge would add a huge range of expansion opportunities if necessary. Add in plenty of solderbridges to allow the end user to customise the ruler as required.

    image

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14phil
    e14phil over 7 years ago

    You all seem way ahead of me on the RPi idea. image

     

    How about a riddle or challenge in the silkscreen?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to cstanton

    Alternatively the full maths set, triangle, ruler, protractor ?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • airbornesurfer
    airbornesurfer over 7 years ago

    What about a header for RPi/Arduino with a small breadboard breakout similar to some of the Feathers that Lady Ada makes?

     

    OOH! It needs an add-on header, too!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • 14rhb
    14rhb over 7 years ago

    ...and a gyro, magnetometer, accelerometer.

     

    Rod

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>