• 3D Snowflake Ornament with BLE Connectivity

    Snowflake themed Christmas ornament with RGB lights and BLE connectivity. Full project write-up on Hackster.io: 3D Snowflake Ornament with BLE Connectivity This is a 3D Snowflake themed ornament with…
  • Choo Choo Go Stick

    Modify battery operated Christmas train engine so my 4 year old grandson can make it go and stop - all by himself. For many of us, there is a magical bond between Christmas and toy trains. One of the few…
  • Santa Countdown

    A fun little Christmas display project with full build instruction. If you can’t wait for Santa to visit this display will automatically count down to his arrival. Suitable for "kids" of "all" ages. Requirements…
  • Christmas Music Box!

    Battery-powered Christmas tune box for decorations and Christmas Trees! Introduction Last year I bought a Solar-Powered Christmas light set. It works great with my small Christmas tree as I normally…
  • Christmas Warmth

    Fake miniature fire barrel - to add ambiance to the inflatable Christmas cows. It's Christmas in Wisconsin and what could possibly be more Wisconsin Christmassy than festive cows? Yes, the one on the…
  • Festive Interactive LED Wreath with Music and Motion Magic

    This project presents an advanced interactive LED wreath designed to elevate holiday decor with dynamic lighting effects and synchronized audio playback. Built around the Arduino Uno microcontroller, the…
  • LED night lamp painting

    I was looking for a way to make painting more interesting in availability of light and in complete darkness. The only requirement is that the painting should be intresting. Painting looks beautiful on…
  • Naughty Elf Animatronic Holiday Air Freshener

    How about an mischievous Elf on the Shelf that farts peppermint, butter cookie dough, or holiday pine scents as an air freshener ? An Elf doesn’t fart continuously, only attempting secretly ninja style…
  • Playstation 1 Replacing CD-Rom

    Replacing the original Playstation 1 CD-Rom with a CD-Rom from an audio player. New Year is a time of magic, when the world is filled with the expectation of miracles and the fulfillment of cherished desires…
  • Santa's Mailbox

    The goal of this project is to create a Santa's mailbox, which will be a template to be modified each year as kids grow up. For this first year, the mailbox was painted and a eink screen was used to show…