Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog DragonBoard 410C I2C to drive a servo
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 3 Jun 2016 11:38 AM Date Created
  • Views 1125 views
  • Likes 3 likes
  • Comments 2 comments
  • i2c
  • pwm
  • servo
  • dragonboard 410c
Related
Recommended

DragonBoard 410C I2C to drive a servo

Workshopshed
Workshopshed
3 Jun 2016

During my earlier experiments with GPIO on this board, I realised that it does not natively support PWM. I had a 4tronix Picon Zero board from my preparation for the Gnomes event and thought that could work with the DragonBoard.

imageimage

As for the LED and IR detector I needed to use level shifters to connect up the board, so I added a second set to my breadboard and wired that up to the power and first I2C bus on the DragonBoard. This board has three I2C buses, two on the low speed connector and one on the high speed. It was a bit of a lashup as I had neither the right connectors for the DragonBoard(male 2x20x2mm) or the Picon (male 2x20x2.54mm).

image

I checked that it was working with the i2cdetect command. This needs elevated privileges to run.

 

To list the buses use:

 

sudo i2cdetect -l

 

To probe for devices on bus 0 use:

 

sudo i2cdetect -r 0

 

This will report a warning, but did not cause any issue for the 4tronix board.

 

WARNING! This program can confuse your I2C bus, cause data loss and worse!
I will probe file /dev/i2c-0 using read byte commands.
I will probe address range 0x03-0x77.
Continue? [Y/n] Y
     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- 22 -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

 

It correctly detected the board at address 22 so I was happy that it was working. I tried to get the board to detect with Libsoc by combining a Libsoc test script with the getRevision function from the piconzero library that did not work reporting a timeout or no data returned so instead I followed the instructions on the 4tronix blog to install the library and examples.

 

wget http://4tronix.co.uk/piconz.sh -O piconz.sh
bash piconz.sh

 

I also installed the python-smbus moduel which is a dependency for the piconz library.

 

sudo apt-get install python-smbus

 

Finally the library needed a minor change at the top as I was using bus 0 not bus 1. Edit piconzero.py and change the line that sets up the bus, as follows.

 

bus = smbus.SMBus(1)

 

I tested the version script and that produced a result.

 

linaro@linaro-alip:~/piconzero$ sudo python version.py
Board Type: Picon Zero
Firmware version: 7

 

I then added a servo and tested that.

 

linaro@linaro-alip:~/piconzero$ sudo python servoTest.py
Tests the servos by using the arrow keys to control
Press <space> key to centre
Press Ctrl-C to end
Up 85
Up 80
Up 75
Up 70
Up 65
Up 60
Up 55
Up 50
Up 45
Up 40
Up 35

 

Here's the results. Although the competition is over and my video presentation is submitted I'd still like to finish off the project with a 3D printed knight.  If you are interested in my adaptions to the box, you can find those on the Workshopshed blog. Boxing the Dragon - Workshopshed

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Workshopshed
    Workshopshed over 10 years ago in reply to clem57

    No the box was bought like that second hand from a cigar shop. The jointing method is called "box jointing", something I will try out at some point (along with dovetails)

     

    maxresdefault.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 10 years ago

    Very cool indeed! Did you make your box? If so I like the ongue and groves in it.

    Cheers,

    Clem