Personal Blogs
  • Community Hub
  • More
Personal Blogs

Andy Clark's Blog

  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Andy Clark's Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Workshop Walls

    Workshopshed
    Workshopshed
    Not posted for a few months, have been busy with a number of things such as visiting Ireland and Scotland, attending EMF camp, painting the house and show casing the company's new products as a fashion model. But there has been progress on tbe Wo...
    • 18 Oct 2026
  • Workshop progress

    Workshopshed
    Workshopshed
    Been a busy weekend for the workshopshed. Got lots of wood cut up and have secured the fixings into the base. All the drilling was done using an SDS drill which I won in 2019 for the Project14 A Question of Scale
    • 4 May 2026
  • New Workshop

    Workshopshed
    Workshopshed
    The garage and studio that came with the house in Suffolk have shown not to be really fit for purpose. The garage is leaking and the roof is made from asbestos making repairs problematic. The studio is ok other than needing to block out the light fro...
    • 20 Apr 2026
  • Year in review 2025

    Workshopshed
    Workshopshed
    2025 was the first full year in the new house and although pretty much everything is unpacked there's still been a lot to do around the house and garden such as decorating, DIY and lots of enhancements to the garden. In February, I managed to get...
    • 4 Jan 2026
  • Tray for serial

    Workshopshed
    Workshopshed
    I've been working on a project with a small microcontroller that's programmed via UDPI. So have been using a USB to Serial adapter with a resistor to do the programming. I also wanted to do some serial monitoring for debugging so have a secon...
    • 13 Sep 2025
  • Visit to Element 14's Distribution Centre in Leeds

    Workshopshed
    Workshopshed
    Last week, e14phil  from the element14 community invited me to see the Farnell office and warehouse in Leeds. The office is located next to the old warehouse near to the centre of town. Once we were past the big security gates and guar...
    • 5 Aug 2025
  • Cheap Yellow Display Talk 29th July, Liverpool

    Workshopshed
    Workshopshed
    Later this month, I'll be over in Liverpool giving a talk on putting dot Net nanoFramework onto a Cheap Yellow Display (ESP32). https://dotnetliverpool.org.uk/ The ESP32 CPU is supported by the framework out of the box but there were still chall...
    • 12 Jul 2025
  • Technology Museums in Cambridge

    Workshopshed
    Workshopshed
    The other weekend I had the chance to visit both the Centre for Computing History and the Cambridge Museum of Technology. We first visited the Centre for Computing history, the entrance houses a small shop and seating area, serviced by a tuck shop....
    • 22 Mar 2025
  • Testcard generator revisted

    Workshopshed
    Workshopshed
    Back in 2016 I created a test card generator to help check a small composite monitor that wasn't working. For an upcoming project I need to test a HDMI monitor so I thought I could just use that again. But when I came to dig it out the SDCard was...
    • 1 Mar 2025
  • Year in review 2024

    Workshopshed
    Workshopshed
    I've not been that active on Element14 the last year due to working on fixing up the new house. Have found some "shocking" electrics such as this socket which was live but the loose wire was not. So the socket tester go a good work out...
    • 1 Jan 2025
  • Moved again

    Workshopshed
    Workshopshed
    Just finishing packing up and moving out of Scotland. New home will be in Ipswich, expect some photos of the new workshop in up coming weeks
    • 22 Feb 2024
  • Makers Central

    Workshopshed
    Workshopshed
    Makers Central is on this weekend at the National Exhibition Centre in Birmingham. When I last visited in 2019 it was mostly focused on woodworking. But I thought I would check it out again as there's quite a lot of other types of makers there t...
    • 11 May 2023
  • KiCAD-GPT is here

    Workshopshed
    Workshopshed
    I’ve been experimenting with a Beta version of KiCAD that adds an AI based interface to the a popular electronics design application. It has been trained on example circuits found in datasheets, old magazines and discussion forums. Rather than ...
    • 1 Apr 2023
  • Setting the default hardware for Pulse Audio

    Workshopshed
    Workshopshed
    Mycroft.AI recommends using Pulse Audio for audio inputs and outputs. This can be installed using: sudo apt install pulseaudio Once you've plugged in your hardware you can configure the default devices for input and output so that ...
    • 27 Feb 2023
  • Simple Fan Controller

    Workshopshed
    Workshopshed
    As mentioned at the end of my last video for the remote temperature monitoring, I've a problem with the base unit having a noisy fan. So I designed a simple control system to reduce the fan speed when it's not needed. https://github.com...
    • 15 Aug 2022
  • Coil Winder

    Workshopshed
    Workshopshed
    So that I could wind 6 identical coils, I needed some way of counting the turns. So I made a simple addon to my milling machine. This consisted of a few 3D printed parts. Firstly a cam that could be bolted onto the milling machine spindle. And also a...
    • 23 Apr 2022
  • A big RGB LED

    Workshopshed
    Workshopshed
    Whilst I was building the book nook project I got reading about the WS2811 chips, these are the controller chips behind the NeoPixel RGB LEDs. And that got me wondering if I could make a big version of an RGB LED in a similar way to I'd created o...
    • 13 Jan 2022
  • MBed and magic red light

    Workshopshed
    Workshopshed
    I was in the Arduino forum the other day, in the Portenta section and I read something rather odd about a bit of MBed software. It's called, as I understand it... Serial crash dump. I have been experimenting with Arduino Portenta and an Adaf...
    • 24 Aug 2021
  • Cross Compiling Micropython on WSL for STM32

    Workshopshed
    Workshopshed
    Following on from my posts looking at the Portenta H7 Vision Shield I wanted to see if I could get the dual boot working with Micropython running on the M7 core and C running on the M4 core. So I posted in a bunch of forums and got some help from Ibr...
    • 5 Aug 2021
  • 2020 A Year in Review

    Workshopshed
    Workshopshed
    When looking at 2020, I have mixed feelings.I started January on a high note, I had just been published in Popular Science for my Dancemat project. I'd also been looking at power management in the TMC2300 Stepper Motor driver. And had successfully us...
    • 19 Jan 2021
  • New Workshop

    Workshopshed
    Workshopshed
    Having moved house back in September I'm slowly getting the workshop into shape. I've bought some benches and given the first one a coat of "garage floor" paint. This should make for a hard wearing surface. I've also decided tha...
    • 2 Nov 2020
  • USB Keyboard / HID

    Workshopshed
    Workshopshed
    I've been experimenting with the Arduino MKR Zero board and wanted it to act as a USB keyboard. This board is based on the SAMD21 processor core which has a native USB wired to one of the sercom peripherals. But when I tried it out the keyboard w...
    • 24 May 2020
  • VNC2 - Getting to Blink

    Workshopshed
    Workshopshed
    After experimenting with the V2DIP1-48V2DIP1-48 from FTDI connecting over SPI, SPI Slave on an Arduino MKR Zero, I wasn't sure if the Arduino code or the FTDI firmware was the problem. After some more experiments I concluded that there was definitely...
    • 18 May 2020
  • SPI Slave on an Arduino MKR Zero

    Workshopshed
    Workshopshed
    I've a device which acts as a SPI Master and sends data over to my microcontroller which is acting as a slave. Simple, I thought, there'll be some stuff in the Arduino SPI library that will help with that. But no, that's just for the mast...
    • 17 May 2020
  • Using a hash function Tokenization during Text Classification on memory constrained devices

    Workshopshed
    Workshopshed
    I've recently been looking at machine learning techniques for analysing data, in particularly text classification and sentiment analysis. For this I'm using Tensor Flow Lite which can be run against edge devices such as microcontrollers. Thanks to Si...
    • 13 May 2020
>