Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Dragonboard 410c Installing software
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 9 May 2016 1:41 PM Date Created
  • Views 2568 views
  • Likes 5 likes
  • Comments 6 comments
  • dragonboard 410c
Related
Recommended

Dragonboard 410c Installing software

Workshopshed
Workshopshed
9 May 2016

Following on from Getting started with Dragonboard 410c

For my project to work, I need the following:

 

  • Internet connectivity
  • Webcam
  • Python
  • OpenCV
  • GPIO

 

I decided to tackle the software elements first as those were the areas I was least familiar with.

 

Trouble with Wifi

Now that I had a working Linux install my next step was to get the Wifi connected. That was very straight forward, or so I thought. The Linaro/Debian desktop provided a status bar widget where you could select the Wifi and enter pass code. I did that an it connected just fine. However, shortly after it dropped out reporting that it was disconnected. I moved the board slightly and it reconnected.

I tried a range of different locations and even turned off the Rii keyboard incase that was interfering with it. Nothing improved the situation. However, I did have a USB to Ethernet dongle from work which I plugged in and connected up. That was detected automatically I was now on the net reliably. If I have time I'll investigate the Wifi further but for my purposes the Ethernet is just fine.

 

I installed Bonjour on my desktop and was able to connect to the Dragonboard by name using SSH without any issues.

image

Camera

I was expecting the camera to cause me problems as it was an old one from my Dad's junk box.

 

I plugged it in and ran lsusb, it correctly detected it as a Logitech QuickCam Express.

imageimage

To test the camera I installed "streamer", and captured a test picture of a cat. I've yet to play with the settings on streamer so this is just a low colour version.

image

Python

 

I wanted to use Python to control my project as it is quick and easy to prototype code like this.  I also wanted to communicate with the internet for the purpose of notify the user, so I installed Pycurl too.

To install Pycurl, I need to install PIP (the python package manager), so I used the get-pip.py script to do that. I had to install a few pre-requisites too.

 

sudo apt-get update
sudo apt-get install libcurl4-openssl-dev python-dev
pip install pycurl

 

To test PyCurl was working, I downloaded a simple web page.

 

from StringIO import StringIO
import pycurl
import signal,sys

def call_api(url):
    r = StringIO()
    c = pycurl.Curl()
    c.setopt(c.URL, url)
    c.setopt(c.CONNECTTIMEOUT, 10)
    c.setopt(c.TIMEOUT, 60)
    c.setopt(c.WRITEFUNCTION, r.write)
    c.perform()
    c.close()
    return r.getvalue()

def main():
    r = call_api("http://csb.stanford.edu/class/public/pages/sykes_webdesign/05_simple.html")
    print r

# Handle exit and kill from OS
def set_exit_handler(func):
    signal.signal(signal.SIGTERM, func)
def on_exit(sig, func=None):
    print "exit handler triggered"
    sys.exit(1)


# Run program
if __name__ == '__main__':
     set_exit_handler(on_exit)
     sys.exit(main())

 

OpenCV

 

After trying to compile software on the Arduino Yún last year, I expected that OpenCV was going to be an issue. However, I followed the instructions to install any dependencies, and configured the make file. That all went smoothing. The compile took a couple of hours, I was not surprised as OpenCV is quite sophisticated.

image

It compiled successfully, but I've yet to test it as it was quite late when it finished.

 

Next up GPIO, there's a few different libraries for this but Intel's MRAA seems to have the most potential for what I'm trying to achieve.

 

Reference

 

Framegrabbing Applications

https://pip.pypa.io/en/stable/installing/

Installation in Linux — OpenCV 2.4.13.0 documentation

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 10 years ago +2
    The success of a good board is "infrastructure" behind it. In this case there is 96Boards providing support forums for the hardware and software, Linaro providing the O/S distribution and Qualcom providing…
  • tonyboubady
    tonyboubady over 10 years ago +1
    Nice board though...
  • DAB
    DAB over 10 years ago +1
    Nice update Andy. I find these detailed walk through posts useful in assessing the usability of these new boards. Thanks DAB
Parents
  • DAB
    DAB over 10 years ago

    Nice update Andy.

     

    I find these detailed walk through posts useful in assessing the usability of these new boards.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 10 years ago

    Nice update Andy.

     

    I find these detailed walk through posts useful in assessing the usability of these new boards.

     

    Thanks

    DAB