Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Picon Zero on the Pi with NodeJS
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 18 Jul 2017 8:13 AM Date Created
  • Views 1216 views
  • Likes 9 likes
  • Comments 6 comments
  • raspberry pi zero
  • nodejs
Related
Recommended

Picon Zero on the Pi with NodeJS

Workshopshed
Workshopshed
18 Jul 2017

I've used the Picon Zero board from 4Tronix before when I was working on the Dragon Detector project. It is the same size as the Pi Zero and can drive 6 outputs, 4 inputs and 2 motors via H-Bridges. So it seemed a good option for driving my latest car project.

image

Prepare the Pi

The Picon Zero runs via I2C so you need to run raspi-config and enable I2C in the settings.

 

It's also worth updating the apt-get cache as we'll be installing some software.

sudo apt-get update

 

Install tools

This step is optional but it's good to have some tools for diagnosing what's going on.

 

sudo apt-get install i2ctools

 

This then allows you to see what I2C adapters are available. This will be different on early pi but most modern Pi are have the I2C bus numbered as "1"

sudo i2cdetect -l

 

That will return something like:

i2c-1   i2c             bcm2835 I2C adapter                     I2C adapter

 

Then the scan command will detect if the board is plugged in and can be detected.

sudo i2cdetect -r 1

 

It will return something like the following:

 

WARNING! This program can confuse your I2C bus, cause data loss and worse!

I will probe file /dev/i2c-1 using read byte commands.

I will probe address range 0x03-0x77.

Continue? [Y/n] Y

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:          -- -- -- -- -- -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: -- -- 22 -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --

 

Install software

First I removed any existing versions of node and npm (the node package manager)

sudo apt-get remove --purge npm node nodejs

 

Then I used an excellent script from Steven de Salas to install the latest version of node.

wget -O - https://raw.githubusercontent.com/sdesalas/node-pi-zero/master/install-node-v.last.sh | bash

 

After checking the versions I installed an I2c libraries so that Node could communicate with the I2C bus

node -v
npm -v
npm install i2c

 

Porting the Picon Zero code to Node

I tried out the "jiphy" tool to see if I could automate some of the code migration. That seemed to work ok with the smaller samples but it choked on the main library. So I ended up porting the code by hand. So far I've just done the version funtion as that allows me to see that communication is happening. I've also tried to mimic the Python version so that people can easily work with either. Here's the two versions side by side.

 

PythonNodeJS

#! /usr/bin/env python

# GNU GPL V3
# Test code for 4tronix Picon Zero

import piconzero as pz

pz.init()
vsn = pz.getRevision()
if (vsn[1] == 2):
    print("Board Type:", "Picon Zero")
else:
    print("Board Type:", vsn[1])
print("Firmware version:", vsn[0])
print()
pz.cleanup()

#!/usr/bin/env node

// GNU GPL V3
// Test code for 4tronix Picon Zero

var pz = require('./piconzero');

pz.init();
var vsn = pz.getRevision();
if  (vsn[1] == 2) {
    console.log("Board Type:", "Picon Zero")
}
else { 
    console.log("Board Type:", vsn[1])
}
console.log("Firmware version:", vsn[0])
console.log();
pz.cleanup();

 

So far it's a proof of concept but it seems to be working reliably so I can't see any problems with porting the rest.

 

Watch this space https://github.com/Workshopshed/PiconZero/tree/master/NodeJS

 

Reference

https://blog.miniarray.com/installing-node-js-on-a-raspberry-pi-zero-21a1522db2bb

https://github.com/sdesalas/node-pi-zero

https://github.com/timothycrosley/jiphy/blob/develop/README.md

Using the I2C Interface – Raspberry Pi Projects

https://www.npmjs.com/package/i2c

  • Sign in to reply

Top Comments

  • Workshopshed
    Workshopshed over 9 years ago +3
    I tested the Digital I/O using an RGB LED, that seems to be working fine. players.brightcove.net/.../index.html
  • mconners
    mconners over 9 years ago +1
    Nice Workshopshed . Neat stuff. Mike
  • Workshopshed
    Workshopshed over 9 years ago +1
    For the motor test, I swapped the power to come from the external USB. Even with that configured I could not get motion from my old motor. I swapped to a motor that I'd created by modifying a micro-servo…
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    For the motor test, I swapped the power to come from the external USB. Even with that configured I could not get motion from my old motor. I swapped to a motor that I'd created by modifying a micro-servoimage and that worked fine. I'll try my other test motor and some bigger motors via the external power supply connectors.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    To modify a servo for continual rotation there are a couple of changes needed. Firstly you'll need to either strip out the electronics, if you want to control the speed externally or to fit a resistor you want constant speed. Then there is a small tab on the gears that acts as a mechanical stop. That needs cutting off. Have a look on Instructables for many different examples of how to do that.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Workshopshed
    Workshopshed over 9 years ago

    For the motor test, I swapped the power to come from the external USB. Even with that configured I could not get motion from my old motor. I swapped to a motor that I'd created by modifying a micro-servoimage and that worked fine. I'll try my other test motor and some bigger motors via the external power supply connectors.

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

     

    To modify a servo for continual rotation there are a couple of changes needed. Firstly you'll need to either strip out the electronics, if you want to control the speed externally or to fit a resistor you want constant speed. Then there is a small tab on the gears that acts as a mechanical stop. That needs cutting off. Have a look on Instructables for many different examples of how to do that.