Personal Blogs
  • Community Hub
  • More
Personal Blogs
Andy Clark's Blog Setting the default hardware for Pulse Audio
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Workshopshed
  • Date Created: 27 Feb 2023 3:47 PM Date Created
  • Views 3456 views
  • Likes 10 likes
  • Comments 1 comment
  • raspberry pi
Related
Recommended

Setting the default hardware for Pulse Audio

Workshopshed
Workshopshed
27 Feb 2023

Mycroft.AI recommends using Pulse Audio for audio inputs and outputs. This can be installed using:

sudo apt install pulseaudio

Once you've plugged in your hardware you can configure the default devices for input and output so that they will be selected on next reboot.

We can find the output devices using the pulse audio command line tool. This is quite verbose we can filter the output using grep.

pacmd list-sinks | egrep "name:|index"

A similar command can then be used to check the for input devices

pacmd list-sources | egrep "name:|index"

Once you've identified these you can test them using the set default command with the index number of the device you think is the right one.

pacmd set-default-sink 1

The output can be tested using the speaker test command with the number of output channels. In my case 2.

speaker-test -t wav -c 2

And once that's working you can test the input using

arecord test.wav

followed by

aplay test.wav

Finally you can set these as defaults by editing the configuration file

sudo nano /etc/pulse/default.pa

You'll need to use the full name so these are properly detected. Reboot the machine to test.

  • Sign in to reply
  • colporteur
    colporteur over 3 years ago

    In the long past I played with audio  Alsa no audio (glitch) issue Pi 4 fix I used the post to keep track of audio related stuff. I've linked your to this post. 

    When I need to refresh my understanding of audio, I only have to jump to the one link.