Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs 1870's Programmable Clock Project...
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jonivanart
  • Date Created: 11 Jan 2016 2:03 AM Date Created
  • Views 1876 views
  • Likes 3 likes
  • Comments 7 comments
  • imbedded
  • robotics
  • collectable
  • horology
  • old
  • clocks
  • art
  • electronics
  • arduino
  • programmable
  • opensource
Related
Recommended

1870's Programmable Clock Project...

jonivanart
jonivanart
11 Jan 2016

First off, I have no idea how to do a blog so if this goes tot he wrong place then sorry in advance. LOL!

I am working on my 4th art project in a series called "TIME". Everything is in #steampunk style art. I have built a Violin, a lamp and a Guitar. (#JonIvanArt) The latest and No. 4 is a clock dated around 1870 or earlier. I'm calling it the "#ExplodedClock" because it will be as if the top right exploded and the steam generator grew out of it.

image

When I received the clock it was in the case that was damaged and the mechanics was in terrible shape. I had to tear it down and clean and polish the whole mechanism. It will be driven by 2 Arduino's. The first #Arduino has the tasks of moving the clock drive gear train with a stepper, the LCD display, and a solenoid that will engage every half second. I have a video that shows the operation of the solenoid posted here and on YouTube under my Jon Ivan channel. The second Arduino will operate the chimes which will be vibrating cell phone motors with Haptic drivers. It will also operate the chime side of the drive gears with a stepper. On top of this there will be a couple vaccum tubes lit with LED's from whichever source I can control it from, Arduino1 or 2.

At the moment I have removed the clock for the wooden mount I built and am building the case. This is the front of the clock with it's crack built in but not the final color.

image

Here is a picture of it mounted and the #solenoid cover installed.

image

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 10 years ago +1
    Hi Jon, It looks like you are off to a great start. I like to see the mixture of art and technology. I look forward to following your project. By the way your blog post turned out perfect. John
  • balearicdynamics
    balearicdynamics over 10 years ago +1
    Great idea ! Wait to see how the stuff proceed Enrico
  • jonivanart
    jonivanart over 10 years ago +1
    I'm guessing that I just add updates in the comment section so here goes! :-) I've got most of the mounting frame work cut to shape, the glass in it's frame and fitted to the clock face. In the picture…
Parents
  • jonivanart
    jonivanart over 10 years ago

    During my building phases I constantly have to assemble and reassemble certain sections a lot for fitting purposes. At this point I use screws but if the part becomes permanent I use glue and usually dowels and sometimes screws and glue if needed. There is one guarantee tho, if it is permanent it is "PERMANENT"! LOL! In this picture the main chassis is temporary with screws. After figuring out the drive shaft assemblies I will have to disassemble it to drill the holes in a drill press to keep them lined up properly. Also I am fitting the tubing for one of the special features of the clock. The "Second" hand. This will be displaying 60 second rotations in the housing of a 2" clock piece at the end of the tubing. I will run the wires for the stepper through this tubing to the stepper driver or mount the driver with the stepper and just run the wires required for the driver board in the tubing to the Arduino.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jonivanart
    jonivanart over 10 years ago

    During my building phases I constantly have to assemble and reassemble certain sections a lot for fitting purposes. At this point I use screws but if the part becomes permanent I use glue and usually dowels and sometimes screws and glue if needed. There is one guarantee tho, if it is permanent it is "PERMANENT"! LOL! In this picture the main chassis is temporary with screws. After figuring out the drive shaft assemblies I will have to disassemble it to drill the holes in a drill press to keep them lined up properly. Also I am fitting the tubing for one of the special features of the clock. The "Second" hand. This will be displaying 60 second rotations in the housing of a 2" clock piece at the end of the tubing. I will run the wires for the stepper through this tubing to the stepper driver or mount the driver with the stepper and just run the wires required for the driver board in the tubing to the Arduino.