Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arduino: R-2R: Setting the Output Frequency
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 25 Apr 2018 2:23 PM Date Created
  • Views 5551 views
  • Likes 7 likes
  • Comments 15 comments
  • r2r
  • arduino uno project
Related
Recommended

Arduino: R-2R: Setting the Output Frequency

jc2048
jc2048
25 Apr 2018

I've made a bit more progress. I now have my test code connected to the SCPI parser. That was very easy to do: I simply copied their generator example, took out the lines specific to the chip they were using, and adapted it slightly to calculate the table step. Much to my amazement it works and I can now program the output frequency.

 

Here's the sketch. The two includes that the highlighting wipes out are:

 

#include <scpiparser.h>
#include <Arduino.h>

 

#include 
#include 
struct scpi_parser_context ctx;
float frequency;
scpi_error_t identify(struct scpi_parser_context* context, struct scpi_token* command);
scpi_error_t get_frequency(struct scpi_parser_context* context, struct scpi_token* command);
scpi_error_t set_frequency(struct scpi_parser_context* context, struct scpi_token* command);
unsigned int tableOffset = 0;             // output count
unsigned int tableStep = 5120;
//
//  --- Sine table - generated by sineTable.exe 
//
unsigned int sineTable[512] = {
   0x8000,0x8192,0x8324,0x84b6,0x8647,0x87d9,0x896a,0x8afb,0x8c8b,0x8e1b,0x8fab,0x9139,0x92c8,0x9455,0x95e2,0x976d,
   0x98f8,0x9a82,0x9c0b,0x9d93,0x9f19,0xa09f,0xa223,0xa3a6,0xa528,0xa6a8,0xa826,0xa9a3,0xab1f,0xac98,0xae11,0xaf87,
   0xb0fb,0xb26e,0xb3de,0xb54d,0xb6ba,0xb824,0xb98c,0xbaf2,0xbc56,0xbdb8,0xbf17,0xc073,0xc1ce,0xc325,0xc47a,0xc5cd,
   0xc71c,0xc869,0xc9b4,0xcafb,0xcc3f,0xcd81,0xcebf,0xcffb,0xd133,0xd269,0xd39b,0xd4ca,0xd5f5,0xd71d,0xd842,0xd964,
   0xda82,0xdb9d,0xdcb4,0xddc7,0xded7,0xdfe3,0xe0ec,0xe1f1,0xe2f2,0xe3ef,0xe4e8,0xe5dd,0xe6cf,0xe7bd,0xe8a6,0xe98c,
   0xea6d,0xeb4a,0xec24,0xecf9,0xedca,0xee96,0xef5f,0xf023,0xf0e2,0xf19e,0xf255,0xf307,0xf3b5,0xf45f,0xf504,0xf5a5,
   0xf641,0xf6d9,0xf76c,0xf7fa,0xf884,0xf909,0xf98a,0xfa05,0xfa7d,0xfaef,0xfb5d,0xfbc5,0xfc29,0xfc89,0xfce3,0xfd39,
   0xfd8a,0xfdd6,0xfe1d,0xfe5f,0xfe9d,0xfed5,0xff09,0xff38,0xff62,0xff87,0xffa7,0xffc2,0xffd8,0xffe9,0xfff6,0xfffd,
   0xffff,0xfffd,0xfff6,0xffe9,0xffd8,0xffc2,0xffa7,0xff87,0xff62,0xff38,0xff09,0xfed5,0xfe9d,0xfe5f,0xfe1d,0xfdd6,
   0xfd8a,0xfd39,0xfce3,0xfc89,0xfc29,0xfbc5,0xfb5d,0xfaef,0xfa7d,0xfa05,0xf98a,0xf909,0xf884,0xf7fa,0xf76c,0xf6d9,
   0xf641,0xf5a5,0xf504,0xf45f,0xf3b5,0xf307,0xf255,0xf19e,0xf0e2,0xf023,0xef5f,0xee96,0xedca,0xecf9,0xec24,0xeb4a,
   0xea6d,0xe98c,0xe8a6,0xe7bd,0xe6cf,0xe5dd,0xe4e8,0xe3ef,0xe2f2,0xe1f1,0xe0ec,0xdfe3,0xded7,0xddc7,0xdcb4,0xdb9d,
   0xda82,0xd964,0xd842,0xd71d,0xd5f5,0xd4ca,0xd39b,0xd269,0xd133,0xcffb,0xcebf,0xcd81,0xcc3f,0xcafb,0xc9b4,0xc869,
   0xc71c,0xc5cd,0xc47a,0xc325,0xc1ce,0xc073,0xbf17,0xbdb8,0xbc56,0xbaf2,0xb98c,0xb824,0xb6ba,0xb54d,0xb3de,0xb26e,
   0xb0fb,0xaf87,0xae11,0xac98,0xab1f,0xa9a3,0xa826,0xa6a8,0xa528,0xa3a6,0xa223,0xa09f,0x9f19,0x9d93,0x9c0b,0x9a82,
   0x98f8,0x976d,0x95e2,0x9455,0x92c8,0x9139,0x8fab,0x8e1b,0x8c8b,0x8afb,0x896a,0x87d9,0x8647,0x84b6,0x8324,0x8192,
   0x8000,0x7e6d,0x7cdb,0x7b49,0x79b8,0x7826,0x7695,0x7504,0x7374,0x71e4,0x7054,0x6ec6,0x6d37,0x6baa,0x6a1d,0x6892,
   0x6707,0x657d,0x63f4,0x626c,0x60e6,0x5f60,0x5ddc,0x5c59,0x5ad7,0x5957,0x57d9,0x565c,0x54e0,0x5367,0x51ee,0x5078,
   0x4f04,0x4d91,0x4c21,0x4ab2,0x4945,0x47db,0x4673,0x450d,0x43a9,0x4247,0x40e8,0x3f8c,0x3e31,0x3cda,0x3b85,0x3a32,
   0x38e3,0x3796,0x364b,0x3504,0x33c0,0x327e,0x3140,0x3004,0x2ecc,0x2d96,0x2c64,0x2b35,0x2a0a,0x28e2,0x27bd,0x269b,
   0x257d,0x2462,0x234b,0x2238,0x2128,0x201c,0x1f13,0x1e0f,0x1d0d,0x1c10,0x1b17,0x1a22,0x1930,0x1842,0x1759,0x1673,
   0x1592,0x14b5,0x13db,0x1306,0x1235,0x1169,0x10a0,0x0fdc,0x0f1d,0x0e61,0x0daa,0x0cf8,0x0c4a,0x0ba0,0x0afb,0x0a5a,
   0x09be,0x0926,0x0893,0x0805,0x077b,0x06f6,0x0675,0x05fa,0x0582,0x0510,0x04a2,0x043a,0x03d6,0x0376,0x031c,0x02c6,
   0x0275,0x0229,0x01e2,0x01a0,0x0162,0x012a,0x00f6,0x00c7,0x009d,0x0078,0x0058,0x003d,0x0027,0x0016,0x0009,0x0002,
   0x0000,0x0002,0x0009,0x0016,0x0027,0x003d,0x0058,0x0078,0x009d,0x00c7,0x00f6,0x012a,0x0162,0x01a0,0x01e2,0x0229,
   0x0275,0x02c6,0x031c,0x0376,0x03d6,0x043a,0x04a2,0x0510,0x0582,0x05fa,0x0675,0x06f6,0x077b,0x0805,0x0893,0x0926,
   0x09be,0x0a5a,0x0afb,0x0ba0,0x0c4a,0x0cf8,0x0daa,0x0e61,0x0f1d,0x0fdc,0x10a0,0x1169,0x1235,0x1306,0x13db,0x14b5,
   0x1592,0x1673,0x1759,0x1842,0x1930,0x1a22,0x1b17,0x1c10,0x1d0d,0x1e0e,0x1f13,0x201c,0x2128,0x2238,0x234b,0x2462,
   0x257d,0x269b,0x27bd,0x28e2,0x2a0a,0x2b35,0x2c64,0x2d96,0x2ecc,0x3004,0x3140,0x327e,0x33c0,0x3504,0x364b,0x3796,
   0x38e3,0x3a32,0x3b85,0x3cda,0x3e31,0x3f8c,0x40e8,0x4247,0x43a9,0x450d,0x4673,0x47db,0x4945,0x4ab2,0x4c21,0x4d91,
   0x4f04,0x5078,0x51ee,0x5367,0x54e0,0x565c,0x57d9,0x5957,0x5ad7,0x5c59,0x5ddc,0x5f60,0x60e6,0x626c,0x63f4,0x657d,
   0x6707,0x6892,0x6a1d,0x6baa,0x6d37,0x6ec6,0x7054,0x71e4,0x7374,0x7504,0x7695,0x7826,0x79b8,0x7b49,0x7cdb,0x7e6d};

void setup()
{
  struct scpi_command* source;
  struct scpi_command* measure;

  /* First, initialise the parser. */
  scpi_init(&ctx);
  /*
   * After initialising the parser, we set up the command tree.  Ours is
   *
   *  *IDN?         -> identify
   *  :SOURCE
   *    :FREQuency  -> set_frequency
   *    :FREQuency? -> get_frequency
   */
  scpi_register_command(ctx.command_tree, SCPI_CL_SAMELEVEL, "*IDN?", 5, "*IDN?", 5, identify);
  source = scpi_register_command(ctx.command_tree, SCPI_CL_CHILD, "SOURCE", 6, "SOUR", 4, NULL);
  scpi_register_command(source, SCPI_CL_CHILD, "FREQUENCY", 9, "FREQ", 4, set_frequency);
  scpi_register_command(source, SCPI_CL_CHILD, "FREQUENCY?", 10, "FREQ?", 5, get_frequency);
  
  frequency = 1e3;
  // set the pins used as outputs:
  
  PORTD = 0;
  
  pinMode(0, OUTPUT);
  pinMode(1, OUTPUT);
  pinMode(2, OUTPUT);
  pinMode(3, OUTPUT);
  pinMode(4, OUTPUT);
  pinMode(5, OUTPUT);
  pinMode(6, OUTPUT);
  pinMode(7, OUTPUT);
  
  pinMode(A0, OUTPUT);
  pinMode(A1, OUTPUT);
  pinMode(A2, OUTPUT);
  pinMode(A3, OUTPUT);
  digitalWrite(A0, HIGH);   
  digitalWrite(A1, HIGH);   
  digitalWrite(A2, HIGH);   
  digitalWrite(A3, LOW);   
  // timer 2 set up
  cli();                  // disable interrupts
  TCCR2A = 0;             // control register all 0
  TCCR2B = 0;             // control register all 0
  TCNT2 = 0;              // set count to 0
  OCR2A = 159;            // period = 160 x 1/16MHz = 10uS
  TCCR2A |= (1 << WGM21); // mode is clear on match
  TCCR2B |= (1 << CS20);  // no prescaler   
  TIMSK2 |= (1 << OCIE2A);  // enable interrupt on match
  sei();                  // enable interrupts
  Serial.begin(9600);
}
// timer 2 interrupt routine
ISR(TIMER2_COMPA_vect) {
  tableOffset = tableOffset + tableStep;
  PORTD = (sineTable[tableOffset >> 7]) >> 8;
}
// main loop
void loop()
{
  char line_buffer[256];
  unsigned char read_length;
  
  while(1)
  {
    /* Read in a line and execute it. */
    read_length = Serial.readBytesUntil('\n', line_buffer, 256);
    if(read_length > 0)
    {
      scpi_execute_command(&ctx, line_buffer, read_length);
    }
  }
}
/*
 * Respond to *IDN?
 */
scpi_error_t identify(struct scpi_parser_context* context, struct scpi_token* command)
{
  scpi_free_tokens(command);
  Serial.println("E14,Arduino Audio Signal Generator,1,10");
  return SCPI_SUCCESS;
}
/**
 * Read the current frequency setting.
 */
scpi_error_t get_frequency(struct scpi_parser_context* context, struct scpi_token* command)
{
//  float voltage;
  Serial.println(frequency,4);
  scpi_free_tokens(command);
  return SCPI_SUCCESS;
}
/**
 * Set the audio output frequency.
 */
scpi_error_t set_frequency(struct scpi_parser_context* context, struct scpi_token* command)
{
  struct scpi_token* args;
  struct scpi_numeric output_numeric;
//  unsigned char output_value;
  args = command;
  while(args != NULL && args->type == 0)
  {
    args = args->next;
  }
  output_numeric = scpi_parse_numeric(args->value, args->length, 1e3, 20, 2e4);
  if(output_numeric.length == 0 ||
    (output_numeric.length == 2 && output_numeric.unit[0] == 'H' && output_numeric.unit[1] == 'z'))
  {
    tableStep = (unsigned int)(65536.0 * output_numeric.value / 100000.0);
    frequency = (unsigned long)constrain(output_numeric.value, 20, 2e4);
  }
  else
  {
    scpi_error error;
    error.id = -200;
    error.description = "Command error;Invalid unit";
    error.length = 26;
    
    scpi_queue_error(&ctx, error);
    scpi_free_tokens(command);
    return SCPI_SUCCESS;
  }
  scpi_free_tokens(command);
  return SCPI_SUCCESS;
}

 

Here are the results for the following SCPI messages

 

:SOUR:FREQ 20Hz

 

image

 

:SOUR:FREQ 1234Hz

 

image

 

:SOUR:FREQ 2e4Hz

 

image

 

The frequencies are fairly accurate, being within a few Hertz of those requested.

 

This is the line that does the real work (line 158)

 

    tableStep = (unsigned int)(65536.0 * output_numeric.value / 100000.0);

 

it takes the frequency from the parser (a float in Hertz) and calculates the table step necessary to generate it. The 100k is the sample rate, the 65536 is the number of intervals one complete cycle is divided into.

 

There are a couple of issues I've identified from doing this:

 

1/ The amplitude dimishes at high frequencies. That means that either I've got my filter values wrong or that the variable gain section is a mess. To look at that I'm going to go back to my test code and rework it to do a frequency sweep - then I'll be able to see directly the frequency response on the 'scope. It also looks like there might be other problems with the 20kHz one.

 

2/ The serial side seems a bit fragile. I can't seem to talk to it with PuTTY (probably just me not being able to get the settings right), but have also once got it into a state where it wouldn't talk to the Arduino serial tool either, so maybe the error recovery isn't very good.

 

However, it's looking quite promising as a very low cost way to generate waveforms.

 

The original blog by Jan, where he introduced us to the SCPI library that he'd found, is here: Arduino in Test Instrumentation - Part 1: SCPI Lib

 

This is the SCPI parser library on GitHub: https://github.com/LachlanGunn/oic

 

 

Part one: Arduino: R-2R Experiment

Part two: Arduino: R-2R: Sine On You Crazy Diamond

Part three: Arduino: R-2R: Buffer, Attenuate, and Filter

Part four: Arduino: R-2R: "We Interrupt This Programme..."

Part five: Arduino: R-2R: "Resistance is..."?

Part six: Arduino: R-2R: Setting the Output Frequency

Part seven: Arduino: R-2R; "A Sweep is as Lucky, as Lucky Can Be..."

Part eight: Arduino: R-2R: Setting the Signal Amplitude

  • Sign in to reply

Top Comments

  • fmilburn
    fmilburn over 8 years ago +3
    A nice well documented series - I have enjoyed following along.
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    for the PuTTY settings, you may have to turn on local echo, so that you see what you type, and maybe CR + LF. it works reliable with the Arduino Serial Monitor if you have the speed setting correct.
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048 +3
    I’ll check tomorrow, when I’m back in the country. it may also be related with the cpu reset that happens on an Arduino UNO when you start up a serial communication over the USB.
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    for the PuTTY settings, you may have to turn on local echo, so that you see what you type, and maybe CR + LF. it works reliable with the Arduino Serial Monitor if you have the speed setting correct.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    I turned on local echo. I also turned off 'XON/XOFF', but I wasn't very sure about the CR and LF settings - I'll give it another go; it should to be possible to make it work.

     

    The time that it failed on the Arduino monitor I had had it working, shut down the monitor and tried using PuTTY, and then tried the Arduino monitor again. It didn't pick up again on the Arduino serial monitor, so PuTTY had got it into a mess that it couldn't recover from. Perhaps that doesn't matter - serial over USB is going to be very robust - but I still like to see things recover for themselves.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    I also can't get it to work with PuTTY. It works ok with the Arduino monitor and LabVIEW.

    No idea what's happening ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    I got it working.

    set No CR/LF extra's -  leave all default.

    Set local echo ON, local edit OFF.

     

    serial settings: <your baud>, 8, 1, 0, N

     

    Have a notepad file with the command, example:

    *IDN?

     

    Copy the *IDN? - just that, and then right click on putty to paste it. Don't press the enter button.

    That's it.

    It works like that for all commands. It seems that our lib doesn't like individually typed characters, and doesn't like CR/LF

    image

     

    It's not related to PuTTY. It has the same behaviour in Ubuntu using the screen terminal (screen /dev/ttyACM0 38400,cs8)

     

    edit:

    It's not really the library. It's the code stolen from the example:

      char line_buffer[256];
      unsigned char read_length;
    
    
      while(1)   {
        /* Read in a line and execute it. */
        read_length = Serial.readBytesUntil('\n', line_buffer, 256);
        if(read_length > 0)     {
          scpi_execute_command(&ctx, line_buffer, read_length);
        }
      }
    }

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to Jan Cumps

    That works for me too. So what's the Arduino Serial Monitor doing? Does it just send a LF and no CR?

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jc2048

    It's actually the way we read the serial string, not the lib itself. I stole it from the example that came with the lib:

     

      while(1)   {
        /* Read in a line and execute it. */
        read_length = Serial.readBytesUntil('\n', line_buffer, 256);
        if(read_length > 0)     {
          scpi_execute_command(&ctx, line_buffer, read_length);
        }
      }

     

    I'll check if I can fix it and still have it working with  LabVIEW lib.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    This one works with putty (carriage return instead of newline):

    void loop() {
      char line_buffer[256];
      unsigned char read_length;
    
    
      while(1)   {
        /* Read in a line and execute it. */
    //    read_length = Serial.readBytesUntil('\n', line_buffer, 256);
        read_length = Serial.readBytesUntil('\r', line_buffer, 256);
        if(read_length > 0)     {
          scpi_execute_command(&ctx, line_buffer, read_length);
        }
      }
    }

     

    It doesn't work with my LabVIEW driver (because I'm using '\n' in all my SCPI commands image ). Not hard to change though ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    This one works with putty (carriage return instead of newline):

    void loop() {
      char line_buffer[256];
      unsigned char read_length;
    
    
      while(1)   {
        /* Read in a line and execute it. */
    //    read_length = Serial.readBytesUntil('\n', line_buffer, 256);
        read_length = Serial.readBytesUntil('\r', line_buffer, 256);
        if(read_length > 0)     {
          scpi_execute_command(&ctx, line_buffer, read_length);
        }
      }
    }

     

    It doesn't work with my LabVIEW driver (because I'm using '\n' in all my SCPI commands image ). Not hard to change though ...