Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arduino: R-2R: Sine On You Crazy Diamond
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 13 Apr 2018 11:15 PM Date Created
  • Views 6033 views
  • Likes 12 likes
  • Comments 12 comments
  • arduino_projects
  • r2r
Related
Recommended

Arduino: R-2R: Sine On You Crazy Diamond

jc2048
jc2048
13 Apr 2018

Part one is here:
https://www.element14.com/community/people/jc2048/blog/2018/04/12/arduino-r-2r-experiment

 

I was going to do some hardware next but got sidetracked into playing with software instead.

 

Here's a very well-known waveform being produced by the simple resistor-ladder DAC I built in part one.

 

 

image

 

and here's what it looked like before I got the arithmetic right

 

 

image

 

That's generated by this sketch

 

//
//  --- Sine table - generated by sineTable.exe 
//

unsigned int sineTable[256] = {
   0x0000,0x00c9,0x0192,0x025b,0x0324,0x03ed,0x04b6,0x057f,0x0647,0x0710,0x07d9,0x08a2,0x096a,0x0a33,0x0afb,0x0bc3,
   0x0c8b,0x0d53,0x0e1b,0x0ee3,0x0fab,0x1072,0x1139,0x1201,0x12c8,0x138e,0x1455,0x151b,0x15e2,0x16a8,0x176d,0x1833,
   0x18f8,0x19bd,0x1a82,0x1b47,0x1c0b,0x1ccf,0x1d93,0x1e56,0x1f19,0x1fdc,0x209f,0x2161,0x2223,0x22e5,0x23a6,0x2467,
   0x2528,0x25e8,0x26a8,0x2767,0x2826,0x28e5,0x29a3,0x2a61,0x2b1f,0x2bdc,0x2c98,0x2d55,0x2e11,0x2ecc,0x2f87,0x3041,
   0x30fb,0x31b5,0x326e,0x3326,0x33de,0x3496,0x354d,0x3604,0x36ba,0x376f,0x3824,0x38d8,0x398c,0x3a40,0x3af2,0x3ba5,
   0x3c56,0x3d07,0x3db8,0x3e68,0x3f17,0x3fc5,0x4073,0x4121,0x41ce,0x427a,0x4325,0x43d0,0x447a,0x4524,0x45cd,0x4675,
   0x471c,0x47c3,0x4869,0x490f,0x49b4,0x4a58,0x4afb,0x4b9e,0x4c3f,0x4ce1,0x4d81,0x4e21,0x4ebf,0x4f5e,0x4ffb,0x5097,
   0x5133,0x51ce,0x5269,0x5302,0x539b,0x5433,0x54ca,0x5560,0x55f5,0x568a,0x571d,0x57b0,0x5842,0x58d4,0x5964,0x59f3,
   0x5a82,0x5b10,0x5b9d,0x5c29,0x5cb4,0x5d3e,0x5dc7,0x5e50,0x5ed7,0x5f5e,0x5fe3,0x6068,0x60ec,0x616f,0x61f1,0x6271,
   0x62f2,0x6371,0x63ef,0x646c,0x64e8,0x6563,0x65dd,0x6657,0x66cf,0x6746,0x67bd,0x6832,0x68a6,0x6919,0x698c,0x69fd,
   0x6a6d,0x6adc,0x6b4a,0x6bb8,0x6c24,0x6c8f,0x6cf9,0x6d62,0x6dca,0x6e30,0x6e96,0x6efb,0x6f5f,0x6fc1,0x7023,0x7083,
   0x70e2,0x7141,0x719e,0x71fa,0x7255,0x72af,0x7307,0x735f,0x73b5,0x740b,0x745f,0x74b2,0x7504,0x7555,0x75a5,0x75f4,
   0x7641,0x768e,0x76d9,0x7723,0x776c,0x77b4,0x77fa,0x7840,0x7884,0x78c7,0x7909,0x794a,0x798a,0x79c8,0x7a05,0x7a42,
   0x7a7d,0x7ab6,0x7aef,0x7b26,0x7b5d,0x7b92,0x7bc5,0x7bf8,0x7c29,0x7c5a,0x7c89,0x7cb7,0x7ce3,0x7d0f,0x7d39,0x7d62,
   0x7d8a,0x7db0,0x7dd6,0x7dfa,0x7e1d,0x7e3f,0x7e5f,0x7e7f,0x7e9d,0x7eba,0x7ed5,0x7ef0,0x7f09,0x7f21,0x7f38,0x7f4d,
   0x7f62,0x7f75,0x7f87,0x7f97,0x7fa7,0x7fb5,0x7fc2,0x7fce,0x7fd8,0x7fe1,0x7fe9,0x7ff0,0x7ff6,0x7ffa,0x7ffd,0x7fff};

void setup() {
  // set the digital pin as output:
  pinMode(0, OUTPUT);
  pinMode(1, OUTPUT);
  pinMode(2, OUTPUT);
  pinMode(3, OUTPUT);
  pinMode(4, OUTPUT);
  pinMode(5, OUTPUT);
  pinMode(6, OUTPUT);
  pinMode(7, OUTPUT);
}

void loop() {
    for(i=0;i<256;i++)
        PORTD = (sineTable[i] + 0x8000) >> 8;
    for(i=255;i>0;i--)
        PORTD = (sineTable[i] + 0x8000) >> 8;
    for(i=0;i<256;i++)
        PORTD = (0x8000 - sineTable[i]) >> 8;
    for(i=255;i>0;i--)
        PORTD = (0x8000 - sineTable[i]) >> 8;
}

 

The sine is done with a look-up table rather than the floating point library in order to save space and because it's much faster. I generated the table (only the first quadrant, to save space) using the following simple C program. That was compiled in Visual C++ on a PC and run simply by double-clicking on the filename (the text file ends up in the same directory and it's quicker than typing into a console window). Then I simply open it with Notepad and copy and paste it into the Arduino sketch. Probably not a very elegant approach, but it works.

 

/****************************************************************/

/* sineTable.c                                                  */

/*           Data values for one-quadrant sine look-up table    */

/*           256 values in int array                            */

/*           Output file is called sineTable.txt                */

/*           13th April 2018    Jon Clift                       */

/*--------------------------------------------------------------*/

/* Rev   Date     Comments                                      */

/* 1.0   13/04/18                                               */

/****************************************************************/

#include 

#include 

#include 

#include 

#include 

#include 

// variables

FILE *handle;

char temp_string[256];

unsigned int sineTable[256];

// main routine

void main(int argc,char *argv[])

{   int i,j;

    /* print banner */

    printf("\n--- sineTable DOS UTILITY PROGRAM V1.0 ---\n");

    printf("Builds sine table for Arduino R-2R experiment blog.\n");

 

    /* generate sine table in array */

   for(i=0;i<256;i++) {

        sineTable[i]=(unsigned int) (((sin((3.1415926/512)*i)) * 32768) + 0);

        }

     /* open output file */

    if((handle=fopen("sineTable.txt","wt"))==NULL) {

        printf("Failed to open output file.\n");

        _fcloseall();

        }

 else {

  /* write file banner */

  fprintf(handle,"//\n");

  fprintf(handle,"//  --- Sine table - generated by sineTable.exe \n");

  fprintf(handle,"//\n");


  fprintf(handle,"unsigned int sineTable[256] = {");

  /* write table to file */

  fprintf(handle,"\n");

  for (i=0;i<16;i++) {

   fprintf(handle,"   ");

   for(j=0;j<16;j++) {

    fprintf(handle,"0x%04x",sineTable[(i*16) + j]);

    if(j<15)

     fprintf(handle,",");

    else {

     if(i==15)

      fprintf(handle,"};\n");

     else

      fprintf(handle,",\n");

     }

    }

   }

  /* close output file */

  fclose(handle);

     printf("Done.\n");

  }

 

 

Part one: Arduino: R-2R Experiment

Part two: Arduino: R-2R: Sine On You Crazy Diamond

Part three: Arduino: R-2R: Buffer, Attenuate, and Filter

Part four: Arduino: R-2R: "We Interrupt This Programme..."

Part five: Arduino: R-2R: "Resistance is..."?

Part six: Arduino: R-2R: Setting the Output Frequency

Part seven: Arduino: R-2R; "A Sweep is as Lucky, as Lucky Can Be..."

Part eight: Arduino: R-2R: Setting the Signal Amplitude

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to genebren +6
  • dougw
    dougw over 8 years ago +5
    Now I'm thinking - what kind of circuit would produce this concave square wave...... It might be one example where performing a Fourier transform would provide insight into the answer.
  • jc2048
    jc2048 over 8 years ago in reply to shabaz +5
    I don't actually know where I'm going with this. I started with seeing the R-2R ladder in an old databook application note and at the same time Jan introduced us to a free SCPI open-source parser, so I…
Parents
  • dougw
    dougw over 8 years ago

    Now I'm thinking - what kind of circuit would produce this concave square wave......

    It might be one example where performing a Fourier transform would provide insight into the answer.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to dougw

    I'd just got the offsetting wrong for each quadrant. Essentially it's a sine wave modulated with a square wave of the same frequency, so I imagine the spectrum would look much like that of the square wave but presumably with more energy at the fundamental. My scope has some sort of rudimentary FFT, so I'll see what that shows.

     

    I suppose you could generate it with a modulator fed with a sine wave and a sliced and inverted version of the same sine wave. The modulator would be a multiplier, so you'd be looking at a Gilbert cell or something like that.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to jc2048

    What I wrote there was quite wrong; I should think BEFORE I post

    things, not afterwards. It's not a multiplication and all my talk of

    modulation is way off the mark.

     

    It's simply the addition of a sine wave and a 180 degree out of

    phase square wave.

     

    Here's a circuit that will generate the waveform (given the

    square wave and the sine wave in the appropriate form). It's simply

    an op-amp summing circuit.

     

    image

     

    Here are the waveforms:

     

    image

     

    Now I have it in the simulator, it's easy to look at the spectrum.

     

    It's still the spectrum of a square wave but with the fundamental

    depressed (that comes from the sine wave partially cancelling the

    fundamental of the square wave).

     

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 8 years ago in reply to jc2048

    What I wrote there was quite wrong; I should think BEFORE I post

    things, not afterwards. It's not a multiplication and all my talk of

    modulation is way off the mark.

     

    It's simply the addition of a sine wave and a 180 degree out of

    phase square wave.

     

    Here's a circuit that will generate the waveform (given the

    square wave and the sine wave in the appropriate form). It's simply

    an op-amp summing circuit.

     

    image

     

    Here are the waveforms:

     

    image

     

    Now I have it in the simulator, it's easy to look at the spectrum.

     

    It's still the spectrum of a square wave but with the fundamental

    depressed (that comes from the sine wave partially cancelling the

    fundamental of the square wave).