Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arduino Simulator : UnoArduSim
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: meera_hussien
  • Date Created: 8 Dec 2018 2:08 AM Date Created
  • Views 14725 views
  • Likes 5 likes
  • Comments 5 comments
  • tutorial
  • fritzing
  • arduino_tutorials
  • arduino
Related
Recommended

Arduino Simulator : UnoArduSim

meera_hussien
meera_hussien
8 Dec 2018
In this tutorial, we will look at the readily available simulator for Arduino. There are a lot of simulators available in the market. Some need to be purchased and some are freeware, which means you can use it for free. Today we will look at the ArduUnoSim, which is a free simulator for Arduino.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image





This software can be downloaded from the link below:

Click Here For The Software

Below is the screenshot of the ArduUnoSim



image



This software is designed based on the Arduino Uno ( as the name of this simulator goes). Overall this software is useful for test code which does not require interfacing with other devices such as the LCD, Dot Matrix and other interactive devices. The software GUI is pretty much straightforward, which is user-friendly and easy to handle. After using for a while, you will be able to figure out how to play around with this software.




Let us walk through the software a little bit more. For easy reference, I have labeled the GUI window in numbers starting from 1 to 24.


image


Below is the simple explanation of the available buttons


image

In our next tutorial, we will look into detail on using this software.

That's all for now.


Thank you.





  • Sign in to reply

Top Comments

  • theo44
    theo44 over 6 years ago +1
    I've download it and its so cool but can we add some composant or not? thanks
  • dubbie
    dubbie over 6 years ago +1
    Looks an interesting simulator. Good for testing out some simpler programmes. However, one of the reasons I like the Arduino so much is that the real hardware is really low cost and pretty much easy to…
  • meera_hussien
    meera_hussien over 6 years ago in reply to dubbie +1
    Hi dubbie , Yes, this is a simple simulator to test simpler programmes. I agree with you on the reason to choose Arduino. During my early involvement in microcontroller, i used to play with PIC microcontroller…
Parents
  • dubbie
    dubbie over 6 years ago

    Looks an interesting simulator. Good for testing out some simpler programmes.

     

    However, one of the reasons I like the Arduino so much is that the real hardware is really low cost and pretty much easy to use (apart from the odd passing quirk).

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • meera_hussien
    meera_hussien over 6 years ago in reply to dubbie

    Hi dubbie,

     

    Yes, this is a simple simulator to test simpler programmes.

     

    I agree with you on the reason to choose Arduino. During my early involvement in microcontroller, i used to play with PIC microcontroller. And at that time, most of the interfacing between other devices are to be done manually. But now with the Arduino, it is totally a different thing. One can purchase a module base sensor and just plug it to Arduino. No more wasting time on troubleshooting on the interfacing circuit.

     

    Thank you.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • meera_hussien
    meera_hussien over 6 years ago in reply to dubbie

    Hi dubbie,

     

    Yes, this is a simple simulator to test simpler programmes.

     

    I agree with you on the reason to choose Arduino. During my early involvement in microcontroller, i used to play with PIC microcontroller. And at that time, most of the interfacing between other devices are to be done manually. But now with the Arduino, it is totally a different thing. One can purchase a module base sensor and just plug it to Arduino. No more wasting time on troubleshooting on the interfacing circuit.

     

    Thank you.