Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Arduino UNO Clone for DIYers - Updated!!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: andrewsays
  • Date Created: 3 Sep 2019 1:54 PM Date Created
  • Views 17085 views
  • Likes 17 likes
  • Comments 14 comments
  • ardbeginner
  • arduino uno
  • tht
  • arduino_tutorials
  • diy
  • through-hole
  • arduino_tutorial
  • arduino clone
Related
Recommended

Arduino UNO Clone for DIYers - Updated!!

andrewsays
andrewsays
3 Sep 2019

One of my kids has just started studying Arduino and she is working on simple projects. She wants to build her own Arduino someday but she still has a long way to go until reaching to that level. She is just barely doing the simple programming with knowing almost nothing about electronics. She is not good at soldering as well.
I made an Arduino kit for her hoping it easily let her build her own Arduino clone and use it for her projects.
I think it may also be helpful to others and I’d like to share its details with you, including its BOM, schematic, PCB design and etc.
Please understand that the completeness of this may not meet your expectation as it is designed solely for my personal use.

 

image

[PIC 1] R0

image

[PIC 2] R1

 

1. Objective

 

a. It should be compatible with Arduino UNO.


- Arduino IDE should work with it.
- It should not additionally require any programmer, adaptor, Serial to TTL(UART) converter or etc. to program.


b. Shields for Arduino UNO should work with it as well.


- The board size and the shape should exactly be the same with the original Arduino UNO.
- All components except for the Barrel Jack for external power source, shouldn’t be taller than headers to be able to use various shields designed for genuine Arduino UNO.


c. It should be easy to build and easy to use.


- Bigger through-hole components should mostly be used for the people doesn’t enjoy soldering SMD.
- Most common 5PIN Micro B type USB cable should be used instead of Standard B type.


d. Its circuit should be simplified for a better understanding.


- Use the parts easy to find or I currently have.
- Eliminate or simplify power selection circuit, crystal, 2nd microcontroller for Serial to TTL converting, headers for reprogramming the 2nd microcontroller and etc.

 

 

2. Circuit Design

 

a. Power Source Selection:


- Genuine Arduino UNO has a function to select power source automatically when multiple power sources are available. It requires an OP AMP IC and a p-channel MOSFET which are normally too big to the relatively small Arduino’s PCB especially if they are through-hole type.
- I replaced the circuit with diodes to simplify it. It makes highest voltage power source used among multiple power sources.
- However, it has a problem. Diode has drop-down voltage normally around 0.7~1.2V. It makes the actual supplied voltage to the circuit will be 0.7~1.2V lower than voltage supplied by the power source.
- I used Schottky Diode as its drop-down voltage is only around 0.3V. It means around 4.7V will be supplied to the circuit if 5V power source such as USB power is used. It is still not good for a commercial product but it looks fine for hobbyists.

 

b. Power Regulators:


- I had many 7805 voltage regulators in stock and I used one of them for 5V power regulation. As its drop-down voltage is around 2V, the voltage of the external power source should be higher than 7.5V(= 5V + 2V drop-down by regulator + 0.3V drop-down by Schottky diode + 0.2V margin) which is not much different from Genuine Arduino’s 7V.
- 78xx series regulators don’t have reverse-bias protection and it may cause them broken down when the output voltage is higher than the input voltage. It happens a lot if the capacitance of the smoothing capacitor at the output is high. Placing a diode between the input pin and the output pin as the protection is recommended.
- I decided not to use this diode for R0 model even if 47uF capacitor is at the output. The diode is not required as the output voltage won’t go higher than 5V and the regulator will normally be fine as long as the output voltage is not greater than 7V.
- 3.3V regulator should have low drop-down voltage and LD1117V33LD1117V33 with 1.2V drop-down will be good enough as it can supply 3.3V(= 5V – 1.2V drop-down by the regulator – 0.3V forward voltage drop by Schottky diode – 0.2V margin) safely to the circuit.


c. Serial to TTL(UART):


- I looked for a way to build a Serial to TTL circuit with through-hole devices for long time but I found no way to make it small enough to fit in the small space on the Arduino’s PCB. I just gave it up and decided to use a surface-mount type IC.
- ATmega16u2 microcontroller is used for genuine Arduino but it is an overkill for this purpose. It will take up much space of the PCB as many additional parts are required for this microcontroller to function properly.
- I decided to use CH340C for R0 model. Unlike the popular CH340G, it doesn’t require external crystal and load capacitors while it has exactly same pinout with CH340G and can directly replace CH340G without modifying PCB layout. I can’t use CH330N this time even if it looks better than CH340C as the parts have already delivered when I just find it out.

- I used CH330N for R1 model. It is smaller than CH340C/G while it has all necessary functions for Arduino and much easier to solder than CH340E.

 

d. Buffer to drive the built-in LED for the digital pin 13.


- A small NPN type transistor is used instead of an OP AMP used for genuine Arduino UNO.
- A LED and a resistor are directly connected to the digital pin 13 in series in case of some cheap Arduino compatible boards. It delays the response of external components driven by the digital output and causes unexpected failures including the overcurrent damage to the ATmega328 microcontroller.

 

e. USB Jack


- First of all, I don’t have any spare USB B to A cable. I just want to use Micro B type USB port just like Arduino Leonardo. I think it’s handier for many people.
- Unfortunately, I couldn’t find a through-hole type of Micro B type jack.

 

3. Schematic

 

image

[PIC 3] R0 Schematic

image

[PIC 4] R1 Schematic

 

4. Parts

 

a. BOM for R0 Model

 

AnnotationProductType/ValueQuantityPart NumberRemark
U1ICCH340C1CH340CJiangsu Qin Heng - USB to Serial Converter
U2ICMC78051MC7805CTGON SEMICONDUCTOR - Linear Voltage Regulator, 7805, Fixed, 5V And 1A Out, TO-220-3
U3ICLD1117V33CLD1117V33C1LD1117V33CSTMICROELECTRONICS - IC, V REG LDO +3.3V, 1117, TO-220-3, 0.95A
U4ICATMEGA328P U1ATMEGA328-PUMICROCHIP - 8 Bit MCU, Low Power High Performance, AVR ATmega Family ATmega328 Series Microcontrollers, 20 MHz
IC Socket28P DIP(N)11-2199298-9TE CONNECTIVITY - IC & Component Socket, 28 Contacts, DIP Socket, 2.54 mm, 7.62 mm
Q1TransistorBC182LBC182L1BC182LMULTICOMP - BIPOLAR TRANSISTOR, NPN, 50V, TO-92
A1Header6P, 2.54 mm12212S-06SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 6 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
Header8P, 2.54 mm22212S-08SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 8 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
Header10P, 2.54 mm12212S-10SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 10 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
J1JackBarrel Jack1FC68148CLIFF ELECTRONIC COMPONENTS - DC Power Connector, Jack, 5 A, 2.1 mm, Through Hole Mount, Through Hole
J2JackUSB B Micro1USB3075-30-AGCT - USB Connector, Micro USB Type B, USB 2.0, Receptacle, 5 Positions, Surface Mount, Right Angle
J3Header6P(ICSP), 2.54 mm12213S-06GMULTICOMP - Board-To-Board Connector, 2.54 mm, 6 Contacts, Header, 2213S Series, Through Hole, 2 Rows
R1, R2, R3, R4,
R8, R9
Resistor1K Ohm6MCF 0.25W 1KMULTICOMP - Through Hole Resistor, 1 kohm, MCF Series, 250 mW, ± 5%, Axial Leaded, 250 V
R5, R7Resistor10K Ohm2MCF 0.25W 10KMULTICOMP - Through Hole Resistor, 10 kohm, MCF Series, 250 mW, ± 5%, Axial Leaded, 250 V
R6Resistor1M Ohm1MCF 0.25W 1MMULTICOMP - Through Hole Resistor, 1 Mohm, MCF Series, 250 mW, ± 5%, Axial Leaded, 250 V
C1, C3, C4, C5,
C6, C8, C9
Capacitor0.1uF7ECW-FD2W104KBPANASONIC - FILM CAPACITOR, 0.1uF, 450V, 10%, RADIAL
C2Capacitor47uF 25V1UHE1E470MDD1TDNICHICON - Electrolytic Capacitor, Miniature, 47 µF, 25 V, HE Series, ± 20%, Radial Leaded, 5 mm
C10Capacitor47uF 6.3V1USR0J470MDD1TPNICHICON - Electrolytic Capacitor, Ultra-miniature, 47 µF, 6.3 V, SR Series, ± 20%, Radial Leaded, 4 mm
C7Capacitor10uF 6.3V1EEA-GA1C100HPANASONIC - Electrolytic Capacitor, 10 µF, 16 V, GA Series, ± 20%, Radial Leaded, 4 mm
SW1Switch2P or 4P tect1MJTP1230AAPEM - Tactile Switch, MJTP Series, Top Actuated, Through Hole, Round Button, 160 gf, 50mA at 12VDC
D1, D2, D3Schottky Diode1N581931N5819RLGON SEMICONDUCTOR - Schottky Rectifier, 40 V, 1 A, Single, DO-41, 2 Pins, 600 mV
D4LEDRed, Rectangular1L-144HDTKINGBRIGHT - LED, Rectangular, Red, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.25 V, 700 nm
D5LEDYellow, Rectangular1L-144YDTKINGBRIGHT - LED, Rectangular, Yellow, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.1 V, 590 nm
D6LEDBlue, 4mm, Oval1C4SMG-BJF-CQ0T0351CREE - LED, 4MM, BLUE, 1.52CD, 470NM
D7LEDGreen, Rectangular1L-144GDTKINGBRIGHT - LED, Rectangular, Green, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.2 V, 565 nm
Y1Resonator16MHz, 20~30pF1AWCR-16.00MDABRACON - Resonator, Ceramic, 16 MHz, Through Hole, 3 Pin, 40 ohm, ± 0.5%, 30pF, AWCR Series
PCB1PCBCustom(R0)1NA-

 

b. BOM for R1 Model

 

AnnotationProductType/ValueQuantityPart NumberRemark
U1ICCH330N1CH330NJiangsu Qin Heng CH330N - USB to Serial Converter
U2ICMC78051MC7805CTGON SEMICONDUCTOR - Linear Voltage Regulator, 7805, Fixed, 5V And 1A Out, TO-220-3
U3ICLD1117V33CLD1117V33C1LD1117V33CSTMICROELECTRONICS - IC, V REG LDO +3.3V, 1117, TO-220-3, 0.95A
U4ICATMEGA328P U1ATMEGA328-PUMICROCHIP - 8 Bit MCU, Low Power High Performance, AVR ATmega Family ATmega328 Series Microcontrollers, 20 MHz
IC Socket28P DIP(N)11-2199298-9TE CONNECTIVITY - IC & Component Socket, 28 Contacts, DIP Socket, 2.54 mm, 7.62 mm
Q1TransistorBC182LBC182L1BC182LMULTICOMP - BIPOLAR TRANSISTOR, NPN, 50V, TO-92
A1Header6P, 2.54 mm12212S-06SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 6 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
Header8P, 2.54 mm22212S-08SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 8 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
Header10P, 2.54 mm12212S-10SG-85MULTICOMP - Board-To-Board Connector, 2.54 mm, 10 Contacts, Receptacle, 2212S Series, Through Hole, 1 Row
J1JackBarrel Jack1FC68148CLIFF ELECTRONIC COMPONENTS - DC Power Connector, Jack, 5 A, 2.1 mm, Through Hole Mount, Through Hole
J2JackUSB B Micro1USB3075-30-AGCT - USB Connector, Micro USB Type B, USB 2.0, Receptacle, 5 Positions, Surface Mount, Right Angle
J3Header6P(ICSP), 2.54 mm12213S-06GMULTICOMP - Board-To-Board Connector, 2.54 mm, 6 Contacts, Header, 2213S Series, Through Hole, 2 Rows
R1, R2Resistor1K Ohm, 125mW2MCCFR0W8J0102A20MULTICOMP - Through Hole Resistor, 1 kohm, MCCFR0W8J Series, 125 mW, ± 5%, Axial Leaded, 200 V
R3, R4Resistor10K Ohm2

MCCFR0W8J0103A20

MULTICOMP - Through Hole Resistor, 10 kohm, MCCFR0W8J Series, 125 mW, ± 5%, Axial Leaded, 200 V
R5Resistor1M Ohm1

MCCFR0W8J0105A20

MULTICOMP - Through Hole Resistor, 1 Mohm, MCCFR0W8J Series, 125 mW, ± 5%, Axial Leaded, 200 V
RN1Resistor Array4 x 1k Ohm

1

4605X-101-102LFBOURNS - Fixed Network Resistor, 1 kohm, 4600X Series, 4 Elements, Bussed, SIP, 5 Pins
C1, C3, C4, C5,
C6, C8, C9
Capacitor0.1uF7

MCFYU6104Z6

MULTICOMP - Ceramic Disc Capacitor, 0.1 µF, 50 V, MCFY Series, +80%, -20%, Y5V, 5 mm
C2, C10Capacitor47uF 25V2UHE1E470MDD1TDNICHICON - Electrolytic Capacitor, Miniature, 47 µF, 25 V, HE Series, ± 20%, Radial Leaded, 5 mm
C7Capacitor10uF 6.3V1EEA-GA1C100HPANASONIC - Electrolytic Capacitor, 10 µF, 16 V, GA Series, ± 20%, Radial Leaded, 4 mm
SW1Switch2P or 4P tect1MJTP1230AAPEM - Tactile Switch, MJTP Series, Top Actuated, Through Hole, Round Button, 160 gf, 50mA at 12VDC
D1, D2, D3Schottky Diode1N581931N5819RLGON SEMICONDUCTOR - Schottky Rectifier, 40 V, 1 A, Single, DO-41, 2 Pins, 600 mV
D4LEDRed, Rectangular1L-144HDTKINGBRIGHT - LED, Rectangular, Red, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.25 V, 700 nm
D5LEDYellow, Rectangular1L-144YDTKINGBRIGHT - LED, Rectangular, Yellow, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.1 V, 590 nm
D6LEDBlue, 4mm, Oval1C4SMG-BJF-CQ0T0351CREE - LED, 4MM, BLUE, 1.52CD, 470NM
D7LEDGreen, Rectangular1L-144GDTKINGBRIGHT - LED, Rectangular, Green, Through Hole, 1.9mm x 3.9mm, 20 mA, 2.2 V, 565 nm
D8Diode1N400211N4002RLGON SEMICONDUCTOR - Standard Recovery Diode, 100 V, 1 A, Single, 1.1 V, 30 A
Y1Resonator16MHz, 20~30pF1AWCR-16.00MDABRACON - Resonator, Ceramic, 16 MHz, Through Hole, 3 Pin, 40 ohm, ± 0.5%, 30pF, AWCR Series
F1FuseResettable, 500mA10ZRR0050FF1EBEL FUSE  - PPTC Resettable Fuse, Through Hole, 0ZRR Series, 500 mA, 1 A, 60 VDC, -40 °C
PCB1PCBCustom(R1)1NA-

 

5. PCB

 

Do Not Apply Higher Voltage Than 25V even if "7.5V~35V" is printed on the PCB.It should have been corrected to "7.5V~25V".

image

[PIC 5] PCB Layout for R0

image

[PIC 6] PCB Layout for R1

 

- Please find the attached gerber files.

Attachments:
Simplino R0_20190711.zip
Simplino R1_20190813_Recovered.zip
  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +9
    What a fun little project. Good to see that your daughter has such big dreams. Here is a possible through hole USB micro B connector https://www.newark.com/gct-global-connector-technology/usb3130-30-a…
  • shabaz
    shabaz over 7 years ago +7
    Hi Andrew, Nice project. Also, the USB socket you've chosen is a good choice anyway. While it's not as straightforward as an all-through-hole connector, but since it has two through-hole lugs, then it…
  • neilk
    neilk over 7 years ago +6
    Hi Andrew, Great project! Thanks for sharing it. How old is your daughter? Wonderful that she should have such a dream! I hope she realises it Neil
Parents
  • tronixstuff
    tronixstuff over 4 years ago

    Well done, always like to see how people make their own boards. I was looking at the data sheet for the CH330N you use in the R1 revision, you might want to take note of the following:

    The figure below is the reference circuit for the MCU microcontroller to connect the CH330 chip through the TTL serial port to realize USB communication under the dual power supply mode. CH330 is powered by USB bus VBUS, MCU uses another power supply VDD, VDD supports 3V ~ 5V, diodes D6 and D7 in the figure are used to alleviate the problem of current inflow between CH330 and MCU through RXD or RX internal diode in dual power supply mode. The RX pin of the MCU in the figure should enable the internal pull-up resistor. If not, it is recommended to add a resistor of 8KΩ~30KΩ to the RX pin. 

    Diode D6 is for the case where CH330 has no power but MCU is powered and TX high level flows back current to CH330 through RXD internal diode; diode D7 is for the case where MCU has no power but CH330 is powered and TXD high level flows back current to MCU through RX internal diode situation. If it is determined that a certain situation will not occur, the corresponding diode can be removed. For example, if the MCU has a permanent self-supplied power supply, then D7 can be short-circuited. 

    The diodes are preferably low-power Schottky diodes, but ordinary diodes such as IN4148 can usually be used. In general, it is not recommended to separate power supply for CH330 and MCU, and use it only when necessary. 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • andrewsays
    andrewsays over 4 years ago in reply to tronixstuff

    I did checked that part in the datasheet when I design the circuit and made both CH330N & the microcontroller powered by single power source.

    That means the diodes are not required between the chips.

    I don't clearly understand why you've mentioned that here though.....

    Thanks much for the comment anyway.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • andrewsays
    andrewsays over 4 years ago in reply to tronixstuff

    I did checked that part in the datasheet when I design the circuit and made both CH330N & the microcontroller powered by single power source.

    That means the diodes are not required between the chips.

    I don't clearly understand why you've mentioned that here though.....

    Thanks much for the comment anyway.