Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Behind the Scenes of "Who Wins?"
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 15 Oct 2013 7:26 PM Date Created
  • Views 813 views
  • Likes 1 like
  • Comments 3 comments
Related
Recommended

Behind the Scenes of "Who Wins?"

e14 Contributor
e14 Contributor
15 Oct 2013

So element14 has asked us here at SYN/HAK, an Akron, Ohio-based Hackerspace,  to share with you what went into the making of the "Who Wins?" video. The video is meant to settle an age-old question. If a certain starship and it's rival spacestation collided in the cosmos, who would win?

 

It all started when-

 

element14Dave from element14  approached us last summer with the below coorespondence.- We had met Dave at the Cleveland Mini Maker Faire last April,


To celebrate our 200,000 member milestone we decided to appeal to the fun, quirky, geeky side of the engineers, makers and hobbysits that call the element14 Community home.


We at element14 are big science fiction fans, and we know the same goes for lot of our members.

 

In support of the hackerspace community we would like to commision SYN/HAK to create a video that continues a spirited debate in the sci fi community: Who would win a fight between two iconic feats of science fiction engineersing? The challenge to your group is to build models we will affectionaitly call the siOrg³ starship and the Lifeless Spherical Space Station, incorporating a single board computer and using parts avalaible via Newark.com...

 

We would like SYN/HAK's help in designing and building the models of both, using single board computers to control things like led lights or whatever else you can come up with. We'd also like you to make an introductory video to using the two models.

 

These should be no bigger than a bowling ball and they do not need to be at scale.

 

Have fun!


 

First things first, we did not want to purchase pre-made props, because frankly, there is no fun in that! We  found the dimensions of  a hamster ball and an acrylic display case to be perfect for encasing all the necessary hardware.

 

The first order of business was attacking  the Lifeless Sphere prop. We used a hole saw to cut the "crater". We adjusted the size to approximate scale. We then reversed the cut out, added a 1/4" pvc spacer, and epoxied it in place. Next, we convered  all the vent holes from the inside with tape. This then allowed us to Bondo the crap out of this thing. Seriously, that's a lot of Bondo. After a few applications and some sanding, a touch up, more sanding, etc,  you get the idea. We used high fill primer to mask any imperfections.


Next, we built the light unit. We used a fiber optic lamp similar to this one (http://tinypic.com/r/250ox9d/5), then 3D- printed- a smaller base (pretty cool,huh?) and built a driver board with RGB LEDs (the stock lights were blue). Then came the task of drilling all the holes and routing fibers in bundles through the holes. Before installing the filaments we finished the paint job. Fun fact: The stenciled shapes are waste ribbon from a circuit board pick and place machine. We originally made the mistake of using hot glue to secure the bundles in place. This caused the filaments to melt, diffusing the light and just generally not working properly. We then used two part plastic epoxy with great results. Finally, an Arduino with a custom- built  LED control board was installed,  finishing the Lifeless Sphere.


We tackeled the siOrg³ a little differently. We started with pillaging the junk pile for scrap computer boards and some not- so- scrap boards (sorry Andy). We layered the boards as well as many, many scrap Tinyduinos (thanks to Ken at TinyCircuits)  inside of the cube. We then sourced modelers flash aka "trees" to build up the outside. Everything was spritzed with just enough black paint to allow the cube to be translucent. RGB LEDs were installed inside and outside the cube. We did end up having to internally brace the cube, formally an acrylic display case, as its one origninal purpose was to keep dust off of prized sports memorabilia. The cube was then driven by a similar Arduino and LED control board combo designed by our very own Torrie Fischer


The fighters used in the comming battle videos were constructed from ball bearings, small plastic tubing, and more scrap Tinyduinos.

 

More questions about our hacks?

 

Feel free to ask in the comments section below. Don't forget to watch out video here, also, make sure you log in or register to vote for your favorite in the " Who Wins?" showdown.


Specs:

=========

Lifeless sphere

=========

Diameter: 304mm

Chassis: Hampster Ball

=========

siOrg³

=========

Dimensions: 250mm x 250mm x 250mm

Chassis: Basketball Display Cube


Source code:


#define CHANNEL_COUNT 4

int pins[] = {3, 5, 6, 9};

int brightness[] = {0, 0, 0, 0};

int fadeSpeed[]= {2, 3, 4, 5};


void setup() {

  for(int i = 0;i<CHANNEL_COUNT;i++) {

    pinMode(pins[i], OUTPUT);

  }

}


void loop() {

  for(int i = 0;i<CHANNEL_COUNT;i++) {

    brightness[i] += fadeSpeed[i];

    if (brightness[i] >= 255 || brightness[i] <= 0) {

      fadeSpeed[i] *= -1;

      brightness[i] += fadeSpeed[i]*2;

    }

    analogWrite(pins[i], brightness[i]);

  }

  delay(10);

}

 

 

 

Below are some pictures of the props "in production"

 

image

 

 

 

 

image

 

We had a great time meeting and discussing the state of the project. Dave from element14 stopped by as we went though our original brainstorming session on the frames and electronics.

 

image

 

The Lifeless Spherical Space Station gets prepped

 

 

 

   imageimageimage

 

The siOrg³ being assimilated.

 

 

 

I hope everyone enjoyed the video. Let us know what you thought in the comments section below. Thanks element14!

 

 

SYN/HAK

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    My money is on the Borg cube. I mean really, one little proton torpedo took down the deathstar while one Borg cube wiped out the entire Federation Fleet at Wolf 395. Granted, the Federation ships are junk…
Parents
  • DAB
    DAB over 12 years ago

    My money is on the Borg cube.

     

    I mean really, one little proton torpedo took down the deathstar while one Borg cube wiped out the entire Federation Fleet at Wolf 395.

     

    Granted, the Federation ships are junk, but you just cannot beat a self repairing ship like the Borg Cube.

     

    Just my opinion.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    My money is on the Borg cube.

     

    I mean really, one little proton torpedo took down the deathstar while one Borg cube wiped out the entire Federation Fleet at Wolf 395.

     

    Granted, the Federation ships are junk, but you just cannot beat a self repairing ship like the Borg Cube.

     

    Just my opinion.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to DAB

    Nice job.

     

    I pick the cube to win, since the round ball like objects only need a single device to explode.

     

    In a previous life, we used plastic fibre optics for lighting effects.

    We had issues with holding individual fibres in place, and I found that poking them through and heating the end with a soldering iron, resulted in a lens effect and stopped them pulling back through.

    A spot of silicon sealant on the rear was sufficient to hold fibres that wouldn't stay put.

     

    Mark