Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Blog #1  Concept
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wtos03
  • Date Created: 23 Jul 2020 3:48 AM Date Created
  • Views 1247 views
  • Likes 7 likes
  • Comments 6 comments
Related
Recommended

Blog #1  Concept

wtos03
wtos03
23 Jul 2020

Concept of the project

f we can reduce the food waste from every house. It will reduce the cost of garbage management for the city.  And if we can recycle food waste. it’s will improve the environment.

This project “ Food waste recycle bin “  will convert waste food into natural organic which we can use to plant the tree.

 

 

 

image

 

Users just put waste food into the slot for the crusher.  Food will be shred into small pieces and the controller will open the valve to fill up the tank with EM compost.

This substance will help dehydrate the waste.  The controller will start motor to stir the waste to mix all together.  This bin will be installed outside house

for solar heating. We are planning to use DC motor 12 V which make it possible to use solar cell in the future which is suitable for remote area or camping site.

 

Next step

We are looking into any available components that can use in this project. To make all from start is expensive and time-consuming.  But if we can select some

part that available in the market will help us reduce cost and time. For example, waste food crusher we may use meat grinder to crush waste by simple add motor

to power it.

  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 6 years ago +3
    I think the concept is good as it would be nice to have some sort of machine/box thingy that you could just put organic waste into and get useable compost out of it. This is the basic process of a compost…
  • wtos03
    wtos03 over 6 years ago in reply to dubbie +2
    Hi Thanks for the comments and point out some good suggestions. I will put these points in my consideration when built the project.
  • genebren
    genebren over 6 years ago +1
    It looks like you have posted you blog to the wrong area. This one seems to be in your personal space as opposed to the Design Challenge space.
Parents
  • dubbie
    dubbie over 6 years ago

    I think the concept is good as it would be nice to have some sort of machine/box thingy that you could just put organic waste into and get useable compost out of it. This is the basic process of a compost heap and I do much the same with that. Cut up the organic waste into smaller pieces, pile it up, occasionally add some garrotta and then very occasionally remove the rotted material and put onto my vegetable beds, although I have never had any liquid come out of the bottom.  There are problems with an automated process as cutting or grinding the waste can be difficult as everything can get jammed up, especially with hard sticks and 'mush'. I do have a stirring rod thingy for the pile but it is really difficult to get it to turn and mix up the rotting compost and I'm thinking of getting two compost bins so I can mix up the rotting material by just moving it from one bin to the other.

     

    I look forward to seeing your implementation.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wtos03
    wtos03 over 6 years ago in reply to dubbie

    Hi

    Thanks for the comments and point out some good suggestions. I will put these points in my consideration when built the project.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wtos03
    wtos03 over 6 years ago in reply to dubbie

    Hi

    Thanks for the comments and point out some good suggestions. I will put these points in my consideration when built the project.