Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs CAN communication with Hercules Safety Microcontroller - part 2: Communication between 2 Devices
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 7 Oct 2017 9:41 PM Date Created
  • Views 2597 views
  • Likes 4 likes
  • Comments 1 comment
  • automotive
  • hercules
  • launchpad
  • can
Related
Recommended

CAN communication with Hercules Safety Microcontroller - part 2: Communication between 2 Devices

Jan Cumps
Jan Cumps
7 Oct 2017

I'm trying out basic CAN communication on a Hercules microcontroller.

This second test is sending data between two controllers. I'm using interrupts for reading and writing this time.

It's not yet a complete CAN implementation. The physical CAN BUS components are missing.

 

image

 

 

Simplified CAN driver

 

CAN communication requires line drivers. The microcontrollers that I'm using have CAN peripherals but their pins are generic IO that operate on the logic 3.3V level.

I'm using a poor man's CAN driver that requires one resistor and two diodes. Check my 2014 blog TI Hercules LaunchPad -  test the CAN with a poor man's CAN driver.

image

 

 

In the next blog I'll start to design the physical layer. I have 2 driver ICs at hand, but no schematic or PCB yet.

 

I'm using two Hercules LaunchPads. The smallest of the family, a TMS570LS04 and the biggest, the TMS570LC43.

The code for both is the same. Both send packages of data to each other and write what they receive to memory.

I'm using CAN peripheral 1 on both, mailbox 1 for sending, 2 for receiving.

The pinouts to get at those signals is shown in the images below.

 

 

image

image

 

Firmware

 

I've set a baud rate of 500 kBit/s.

image

The message boxes, different than in the previous blog, use unique IDs.

image

The small LaunchPad sends with ID 2 and listens to ID 1.

image

The big LaunchPad the other way around.

Because they are on the same bus, they should each read each others data and ignore their own messages.

The high priority interrupt for CAN1 is enabled on both.

image

image

 

The C code is straightforward. A few buffers and assorted other things are declared.

 

#define D_COUNT  8

uint32 cnt=0, error =0, tx_done =0;
uint8 tx_data[D_COUNT][8] = {0};
uint8 rx_data[D_COUNT][8] = {0};
uint8 *tx_ptr = &tx_data[0][0];
uint8 *rx_ptr = &rx_data[0][0];
uint8 *dptr=0;

 

The main() function initialises CAN, enables interrupts and error handling.

 

    /* enable irq interrupt in Cortex R4 */
    _enable_interrupt_();

    /** - writing a random data in RAM - to transmit */
    dumpSomeData();

    /** - configuring CAN1 */
    canInit();

    /** - enabling error interrupts */
    canEnableErrorNotification(canREG1);

 

Then it goes on to write some random data. Reading doesn't happen in main(). It's done in the interrupt service routine.

the tx_done flag is set in the ISR too, when the controller calls the interrupt after transmission is completed.

 

    /** - starting transmission */
     for(cnt=0;cnt<d_count;cnt++)
    {
      canTransmit(canREG1, canMESSAGE_BOX1, tx_ptr); /* transmitting 8 different chunks 1 by 1 */
      while(tx_done == 0){};                 /* ... wait until transmit request is through        */
      tx_done=0;
      tx_ptr +=8;    /* next chunk ...*/
    }

 

Here is that service routine.

 

#pragma WEAK(canMessageNotification)
void canMessageNotification(canBASE_t *node, uint32 messageBox)  
{

    if((node==canREG1)&& (messageBox == canMESSAGE_BOX1)) // transmit box
    {
      tx_done=1; /* confirm transfer request */
    }


    if((node==canREG1)&& (messageBox == canMESSAGE_BOX2)) // receive box
    {
     while(!canIsRxMessageArrived(canREG1, canMESSAGE_BOX2));
     canGetData(canREG1, canMESSAGE_BOX2, rx_ptr); /* copy to RAM */
     rx_ptr +=8;
    }

}

 

The first part handles the write interrupt. The full reading functionality is performed in the second part.

 

This simple program does nothing more than sending a few chunks of random data to each other, but that's ok for now.

It's a proof that two separate CANs can talk over a wire. A good start for the design with real physical CAN bus drivers.

 

Here's a capture of traffic generated by this setup:

image

 

Road Test Blog
part 1: First trials
part 2: Inject CAN Messages
part 3: Analyzer as Test Tool
part 4: Analyze the Physical layer of CAN Bus
Related Blog
part 1: tryout
part 2: Communication between 2 Devices
part 3a: Design a Bus Driver PCB
part 3b: Design a Bus Driver PCB - Schematics and Custom Components
part 3c: Design a Bus Driver PCB - Layout
part 3d: Design a Bus Driver PCB - Test
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago +1
    I have used the Microchip CAN Bus Analyser from the RoadTest on this setup - it works . I'll document my whereabouts on the RoadTest pages. Here's a preview: www.youtube.com/watch
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    I have used the Microchip CAN Bus Analyser from the RoadTest on this setup - it works image.

     

    I'll document my whereabouts on the RoadTest pages. Here's a preview:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago

    I have used the Microchip CAN Bus Analyser from the RoadTest on this setup - it works image.

     

    I'll document my whereabouts on the RoadTest pages. Here's a preview:

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview