Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Combined NFC reader / keypad
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Fred27
  • Date Created: 25 Oct 2018 9:12 PM Date Created
  • Views 2076 views
  • Likes 11 likes
  • Comments 15 comments
  • nfc
  • msp430
  • trf7970a
  • capacitive touch
Related
Recommended

Combined NFC reader / keypad

Fred27
Fred27
25 Oct 2018

So, the board is back from the fab. It looks really nice - especially as it only cost $1 (+$8 shipping) for 3 from Seeed. It's been pasted, populated and toasted and ready for test. Well - it would be ready for test if it wasn't missing just one component - an out-of-stock 32.768kHz crystal.

image

The board will eventually be the way into my house. There's a small NFC antenna that I'm hoping will be tuned well enough for the tiny NFC implant in my hand. There's a capacitive touch keypad (hence the MSP430FR2633 microcontroller) because even I don't think getting my kids chipped is a great idea.

 

Unfortunately without the missing crystal it will be a pain to get the capacitive touch or the SPI comms with the TRF7970A NFC transceiver working. I'll wait for it and work on other stuff for now.

 

I can confirm that the reverse mount RGB LED that shines through the circular gap in the soldermask seems to work really well though. The FR4 diffuses it nicely. Blinky is always a good start to prove the MSP430 is running happily. I'll have to wait to see how my QFN soldering went. It looks borderline under the microscope. This time I decided to solder down the thermal pad first and check alignment and then use some paste and a hot air gun to do the leads. That should minimise the chance of any shorts under there that I can't see. At least I hope it does - I've never tried it that way before.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 7 years ago in reply to genebren +4
    Hehe I've been looking too (since I'm close by). I've found some wire-ended ones that are about the size of those in old casio watches (about 2mm dia, 6mm long maybe) part code AB26TRB-32.768KHZ-T and…
  • Fred27
    Fred27 over 7 years ago +3
    Thanks for the advice about bodging in another crystal. I did that, adapted some basic NFC reading code and what do you know - it works! Despite my questionable QFN soldering and guesswork at antenna tuning…
  • Fred27
    Fred27 over 7 years ago +3
    The capacitive touch keypad is also working pretty well, including decoding key presses and checking for the right code. The proximity / guard sensor works, but may need some tuning so I've disabled it…
Parents
  • Fred27
    Fred27 over 7 years ago

    Thanks for the offers, guys. I'm sure I've probably also got some old crystals lying around somewhere that could be bodged in. However, I've also got other things to take a look at right now - such as continuing with the FPGA stuff.

     

    I've email Farnell to ask if they could swap in an alternative component. It's frustrating when you pick one because it's in stock but by the time the order goes through it's out of stock and there's another pretty much identical one with thousands available.

     

    The solder really isn't that good up close!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to Fred27

    It looks pretty good from the photo : ) there are no bulging blobs on every resistor like I often have! (I've solved my problem recently by getting thinner solder).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 7 years ago in reply to Fred27

    It looks pretty good from the photo : ) there are no bulging blobs on every resistor like I often have! (I've solved my problem recently by getting thinner solder).