Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs CPLD Controlled Door Lock - Final Schematic
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oldmanraskers
  • Date Created: 2 May 2015 3:01 PM Date Created
  • Views 1305 views
  • Likes 0 likes
  • Comments 7 comments
  • mav
  • max_v_cpld
Related
Recommended

CPLD Controlled Door Lock - Final Schematic

oldmanraskers
oldmanraskers
2 May 2015

The design has slowed because of work commitments etc. but I have now included an oscillator and the JTAG header - hopefully this is the final design. I will be having a careful look, and if all seems okay I will move onto routing the board. If anyone wants to download the file and comment, please feel free image

Attachments:
imageMain Board.pdf
  • Sign in to reply
Parents
  • oldmanraskers
    oldmanraskers over 11 years ago

    Ah, I did try to insert the PDF but received a file type forbidden error - but I obviously did something wrong because it is now working image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to oldmanraskers

    I can read it now.

     

    A few suggestions:

    I don't like your 24 -> 3.3V regulator - it's far to weedy and will fry. If we assume 100mA it has to get rid of 2W (approx) so you need a decent sized chip  or a switcher. You don't need a switcher for the 1.8V regulator - much better with a linear because even if it has to take 50 mA that's only 75mW.

    A reasonable choice for the linear 3.3V regulator would be:

    • Manufacturer: STMICROELECTRONICS
    • Order Code: 1467771
    • Manufacturer Part No LD1086D2T33TR

     

    You don't say the frequency of your oscillator but whatever it is I would put a 47R resistor between it and the CPLD. And I wouldn't put  a capacitor to ground. And I'd use 1uF 0603 caps for chip decoupling everywhere - you've got a mix of 0.01 and 0.1 which is something you often see in app notes but it doesn't work as well as lots of 1uFs.

     

    I would also add some test pins for gnd (more than one of those) and the power supplies and since you have some spare pins on the CPLD connect 8 of them and two grounds to some sort of 10pin connector for debugging. (Then when you are developing the code and it isn't doing what you expect you'll be able to connect a scope or logic analyser to the debug pins and look at interesting signals that you can route out to them.)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oldmanraskers
    oldmanraskers over 11 years ago in reply to michaelkellett

    I'm sorry it took so long to enable visibility image

     

    1.) What should I be looking at in the data sheet to determine if the 24 -> 3.3 regulator will fry?

    2.) The oscillator is 10MHz and the data sheet recommends the 15pF cap, there is no mention of a resistor. I'm willing to take your advice but I'm curious about the design choice?

    3.) Using 1uF caps seems to make sense image

    4.) Ground and power test pins image

    5.) Debug header - you would just run the pins in case you needed to make the CPLD output... anything... like an internal signal etc.?

    6.) What design software do you use for capture and simulation?

     

    Thanks, MR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to oldmanraskers

    Thermal resistance to ambient will tell you how hot the chip will get, I know form experience that a SOT23 size regulator won't get rid of 2W - TI are suggesting about 40degress pwer W for these chips for junction to board and I reckon you'll do very well to manage less than 20 from chip feet to ambient so 2W would give you a max allowed ambient temperature of 30C. It's just easier to use a bigger regulator.

    Putting caps to ground usually interacts with parasitic inductance to make things ring - are you sure the data sheet isn't just telling you that it can drive 15pF ? the series ressitot will often reduce ringing and improve waveforms - but you can always change its value if necessary (and you have a good enough scope to tell the difference.)

     

    I use EasyPC for PCB design - cheap, simple and adequate for most things but running out of steam a bit with >256 pin BGA or when you get to impedance controlled tracks.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oldmanraskers
    oldmanraskers over 11 years ago in reply to michaelkellett

    I'm not really sure what the data sheet means in terms of 15pF - I have attached it if you want to check it out. In terms of the regulator, wow... I am so surprised by the difference in size - I guess the package says it all.

     

    Thanks, MR.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 11 years ago in reply to oldmanraskers

    It's badly worded so you can't be sure but I think they mean that it expects to drive a total load of 15pF, so you don't need to add a capacitor.

     

    Tried to post this a while ago (yesterday) but it didn't work - trying again.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oldmanraskers
    oldmanraskers over 11 years ago in reply to michaelkellett

    I wasn't sure either - I think I will make provision for the cap and leave it out of circuit if not required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • oldmanraskers
    oldmanraskers over 11 years ago in reply to michaelkellett

    I wasn't sure either - I think I will make provision for the cap and leave it out of circuit if not required.