Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs CPLD Controlled Door Lock - Input Circuit
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oldmanraskers
  • Date Created: 25 Apr 2015 9:22 AM Date Created
  • Views 1649 views
  • Likes 1 like
  • Comments 11 comments
  • max_v_cpld
Related
Recommended

CPLD Controlled Door Lock - Input Circuit

oldmanraskers
oldmanraskers
25 Apr 2015

Input Circuit


The input circuit is very simple. Consider that 24V is present at the connector X1-1; this will allow 20mA to flow through LED1 and indicate there is an input present.  Approximately 2mA will flow via R2 and R3, thereby pulling the CPLD IN01 pin to 3V (the device can accept unto 4V).


image

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 11 years ago in reply to oldmanraskers +1
    You're mixing up output drive currents and input currents. The MAXV will draw a tiny 10uA current on an input (unless you program a pullup current for that pin) so when Q1 is off you would expect to see…
Parents
  • clem57
    clem57 over 11 years ago

    Good now

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 11 years ago

    Good now