Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Create a Programmable Instrument with SCPI - Part 7: Talk to Hardware Registers
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 30 Sep 2016 2:02 PM Date Created
  • Views 4139 views
  • Likes 6 likes
  • Comments 10 comments
  • smart_instrument
  • pwm
  • measurement
  • labview
  • scpi
  • automation
  • lab
  • instrument
Related
Recommended

Create a Programmable Instrument with SCPI - Part 7: Talk to Hardware Registers

Jan Cumps
Jan Cumps
30 Sep 2016
For a hardware evaluation project I'm working on, I want to create a device that can be controlled via LabVIEW.
LabVIEW can talk to instruments using serial out of the box, and it knows how to talk Standard Commands for Programmable Instruments (SCPI).

 

image

 

In this blog I adapt the LabVIEW Virtual Instrument and the firmware to give direct access to the Hercules PWM Time base control registers.

You'll be able to independently set all 7 PWM modules that are available on the controller.

 

 

The FirmWare Support for Direct Register Access

I provided a SCPI command that can receive a numeric value from LabVIEW and write that to the correct PWM module.

Here's the pattern:

    {.pattern = "PWM#:TBCTL", .callback = SCPI_HerculesPwmTBCTL,},

 

The implementation is very simple. Just like in the previous blog, we'll retrieve the PWM module, and the register value, from the SCPI command we get from LabVIEW.

LabView will send something like this:

PWM2:TBCTL #H200

 

We'll have to derive from this string that the PWM register set we have to address is that of PWM module 2.

And we'll have to write 0x0200 into its TBCTL register.

 

I have refactored my code since the first blog, to separate the Hercules PWM details from the SCPI parser. And I've factored out some functionality that can be reused accross many functions.

The code to get the right PWM module has gotten its own function:

 

static scpi_result_t PwmGetModule(scpi_t *context, uint32_t *uModule) {
  int32_t numbers[1];

  // retrieve the PWM channel. Can be 1 - 7
  SCPI_CommandNumbers(context, numbers, 1, 1);
  if (! ((numbers[0] > 0) && (numbers[0] < 8) )) {
  // todo push error on stack if the PWM CHANNEL not between 1 and 7
  return SCPI_RES_ERR;
  } else {
  *uModule = numbers[0];
  return SCPI_RES_OK;
  }
}

 

And here's the code that parses ut the register value and sends all to the Hercules PWM side:

/**
 * Set PWM register TBCTL
 *
 * Return SCPI_RES_OK
 *
 */
static scpi_result_t SCPI_HerculesPwmTBCTL(scpi_t * context) {

    int32_t param1;
    uint32_t uModule;
    if (PwmGetModule(context, &uModule) == SCPI_RES_ERR) {
        return SCPI_RES_ERR;
    }

     /* read first parameter if present */
     if (!SCPI_ParamInt32(context, &param1, TRUE)) {
         return SCPI_RES_ERR;
     }
     pwmTBCTL(uModule, param1);

    return SCPI_RES_OK;
}

 

In that PWM part, I simply write the value to the relevant register of the correct module:

// array of the 7 PWM registers of the RM46
etpwmBASE_t *pwmRegs[7] ={etpwmREG1, etpwmREG2, etpwmREG3, etpwmREG4, etpwmREG5, etpwmREG6, etpwmREG7} ;

void pwmTBCTL(uint32_t uModule, uint16_t uValue) {
  pwmRegs[uModule-1] -> TBCTL = uValue;
}

 

TBCTL is a 16 bit register that drives the following PWM behaviour (and more, that I don't discuss here):

Bit 9 - 7 are the high speed clock divider bits. A few examples

0b111: /14

0b001: /2

0b000: /1

 

Bit 1 - 0 indicate the counter mode. We'll use these two in our example:

0b00: normal up count

0b11: freeze counter

 

That's why you'll see the following useful Hex codes on the LabVIEW display below:

PWM 1 MHz: 0

PWM 500 kHz: 80

PWM 125 kHz: 200

PWM of: 3

 

This register isn't the one where you will later define the exact frequencies. I'll provide additional SCPI functionality to talk to those.

But for the things we want to show here - that we can select to what module we talk, and can push data to a register - TBCTL  will do just fine.

 

The LabVIEW Design

This version of the LabVIEW panel has two user editable controls.

There's a dial that allows you to select PWM module 1 to 7.

image

 

When you run the LabVIEW process, it will talk to that PWM module of your Hercules LaunchPad.

 

The second control is an edit box where you can type the hexadecimal value of what you want to write to that PWM module's TBCTL  register.

image

For convenience, I've added a table with some useful values next to it.

Use this edit box together with your controller's technical reference manual.

The LabVIEW program here is a great tool for you to better learn your controller's PWM module.

You can type in any value you like (better base it on the instructions in the TRM image ), and beam them directly into the register.

You can attach a scope and see the results.

 

Here's the very simple LabVIEW block diagram.

image

The string constant holds the following value:

PWM%u:TBCTL\s#H%s\n

 

That is sent into a Format Into String block, together with the values of the dial and the edit control.

At the output of the block, you'll get:

PWM2:TBCTL #H80\n

 

That is sent off to the Hercules LaunchPad over USB.

 

The results

Let's see how the outputs of PWM module 1 and 2 look lik when we send a few commands.

 

After sending 0x3 to both modules (both off):

image

 

After sending 0x80 to PWM 2 (500kHz):

image

 

After sending 0x0 to PWM 1 (1MHz):

 

image

 

It's easier to understand why 0x03 switches off the PWM signal and why the other magical HEX values do what they do if you know the layout of the register we're addressing. Here are the relevant bits explained.

Source:  http://www.ti.com/lit/pdf/spnu514

image

 

 

The source for LabVIEW and the Hercules CCS project are attached to this blog.

You can try this yourself.

 

 

Related Blog

Create a Programmable Instrument with SCPI - Part 1: Parser Library
Create a Programmable Instrument with SCPI - Part 2: Serial over USB
Create a Programmable Instrument with SCPI - Part 3: First Conversation *IDN?
Create a Programmable Instrument with SCPI - Part 4: Error Handling by Default
Create a Programmable Instrument with SCPI - Part 5: First Hardware Commands
Create a Programmable Instrument with SCPI - Part 6: LabVIEW Integration
Create a Programmable Instrument with SCPI - Part 7: Talk to Hardware Registers
Attachments:
blog.zip
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to fmilburn +3
    Frank, Processor power will not be an issue. You'll have to check if the MSP430 has enough memory left for your non-SCPI firmware though. I could not fit the library in an Arduino (that has 32 K RAM too…
  • jc2048
    jc2048 over 8 years ago in reply to fmilburn +3
    Something to watch if you try the SCPI parser is that it uses allocated dynamic memory when it runs. The amount depends on the command tree that you define. I found on the Arduino that just adding a couple…
  • DAB
    DAB over 9 years ago +2
    Great update Jan. Getting the control sequence right sets up project for lots of expansion. DAB
Parents
  • DAB
    DAB over 9 years ago

    Great update Jan.

     

    Getting the control sequence right sets up project for lots of expansion.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    Thanks, Don!

     

    If you count progress as lines of code, there isn't a lot happening. Most effort goes into fiddling around and searching, trying.

    In theory I should now be able to calculate how long it will take to finalise full support for all PWM functionality, because the number of registers is a given, and the mechanism I used here can just be re-applied.

     

    I'm going to investigate first how I can best support reading a register first, before extending the design.

     

    Once I get to the next functionality, it will be fine control for frequency, duty cycle and deadband.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    Thanks, Don!

     

    If you count progress as lines of code, there isn't a lot happening. Most effort goes into fiddling around and searching, trying.

    In theory I should now be able to calculate how long it will take to finalise full support for all PWM functionality, because the number of registers is a given, and the mechanism I used here can just be re-applied.

     

    I'm going to investigate first how I can best support reading a register first, before extending the design.

     

    Once I get to the next functionality, it will be fine control for frequency, duty cycle and deadband.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • michaelkellett
    michaelkellett over 9 years ago in reply to Jan Cumps

    Are you using a paid for version of LabView or have you found a free one ?

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to michaelkellett

    A paid version. I bought one in June when Clint from Digilent was on The Amp Hour, and announced a 15% off code during the show.

    It's still mentioned on the Amp Hour site.