Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs DAC8775 Quad-Channel DAC EVM - part 4: Current Mode
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 23 Jul 2018 1:56 PM Date Created
  • Views 4448 views
  • Likes 12 likes
  • Comments 16 comments
  • dac
  • spi
  • dac8775
  • texas_instruments
  • hercules
  • ti_rt
Related
Recommended

DAC8775 Quad-Channel DAC EVM - part 4: Current Mode

Jan Cumps
Jan Cumps
23 Jul 2018

In this post, I program the current mode of the DAC8775, the subject of the Quad-Channel, Analog Output Module RoadTest.

image

The DAC will, within limits, try to source the current you're defining

 

 

Configurable Current

 

Additional to the traditional voltage mode, this DAC can source current. It has a number of ranges that can be controlled:

image

 

image

In this exercise I'm setting the mode to 0101: 0 - 20 mA.

 

In code:

 

    TX_Data_Master[0] = 0x04;
    TX_Data_Master[1] = 0x10; // output on, default slew rate
    TX_Data_Master[2] = 0x05; // slew rate off, 0 - 20 mA mode
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

I've used the EEVBlog µCurrent to measure the current. I've wired it straight over the outputs. The DAC has the duty to generate the requested current for the µCurrent's shunt.

It has headroom of +15 to -15 V to do this, because that's the range I've set the DAC's internal Buck-Boosters at.

image

In the photo at the top of the article, I'm pushing 20 mA, and have set the µCurrent to mA mode. It uses a 0R01 shunt in that case.

The µCurrent outputs 1 mV per mA of current in that mode and my multimeter reads 19 mA. We're in the ballpark.

Note: my DMM, a Brymen BM235, doesn't have a lower voltage range. All measurements are within the specs of meter, µCurrent and DAC.

 

The code to generate 20 mA:

 

    TX_Data_Master[0] = 0x05;
    TX_Data_Master[1] = 0xff;
    TX_Data_Master[2] = 0xff;
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

For these current levels, you don't need a µCurrent. Most DMMs have a low enough Burden voltage (internal shunt) to deal with that.

Once we're in the lower bit range of the DAC, the µCurrent shows it value.

 

0xffff is 20 mA. If we divide the value by 1024, we get 0x003f, and the output should be 19.53125 µA.

 

    TX_Data_Master[0] = 0x05;
    TX_Data_Master[1] = 0x00;
    TX_Data_Master[2] = 0x3f;
    /* Initiate SPI3 Transmit and Receive through Polling Mode */
    spiTransmitAndReceiveData(spiREG3, &dataconfig1_t, 3, TX_Data_Master, RX_Data_Master);

 

With the µCurent in µA mode (shunt is 10R), I measure 18 µA. Again close.

 

image

 

Related Blog
DAC8775 Quad-Channel DAC EVM - unlicensed roadtest part 1: Raw SPI
DAC8775 Quad-Channel DAC EVM - part 2: Firmware
DAC8775 Quad-Channel DAC EVM - part 3: Slew Rate Control
DAC8775 Quad-Channel DAC EVM - part 4: Current Mode
DAC8775 Quad-Channel DAC EVM - part 5: HART Interface
  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +4
    Hi Jan, Posting about this type of experiment is very interesting and important for the forum. I always learn some new things from your blogs. What do the Stars know? John
  • michaelkellett
    michaelkellett over 8 years ago +4
    I've just bumped up the user rating - not that I pay them any attention. This is the kind of stuff we want to see - I wish I had more time to do some more of my own. I've not encountered HART before -…
  • snidhi
    snidhi over 8 years ago +3
    Hi Jan, You are doing great work. I am following your blog very closely. I myself wanted to dive in the unique world of ADCs and DACs. By following your measurement techniques I kind of am getting the…
Parents
  • Jan Cumps
    Jan Cumps over 8 years ago

    The DAC8775 has a HART interface. You can modulate current output with a superimposed current, by providing an AC voltage of 500 mV pp at 1200 and 2200 Hz.

    The signal has to be capacitively coupled.

    The result is that the constant current output (here 6 mA) is modulated with a 500 µA component.

    image

     

    To enable this, you have to set the Enable HART bit in register 0x04.

    image

     

    The Evaluation Kit PCB will have to be modified, because all HART pins are by defult coupled to ground via a capacitor.

    image

    Here's the schematic for channel A:

    image

     

    On the PCB, I'll have to remove the C58 and induct the HART signal. This is an 0603 component. That's in the comfort zone.

    image

     

     

     

    This is a functionality that will translate well to an oscilloscope image, and the HART protocol is something that isn't discussed on the community that much.

    Two good reasons to do the exercise.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    The capacitor C58 is gone, ready to add a breakout wire ...

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    The capacitor C58 is gone, ready to add a breakout wire ...

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I've added the signal to my breakout board. Note to @self, when connecting to the signal generator, add a capacitor. Capacitive coupling is a must according to the datasheet.

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I'm trying to start up the DAC with the HART capacitor removed and it does not want to play along.

    I used an external capacitor temporarily to tie it to ground ... I'll have to recheck ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I'm going to bring the board back to original condition. I've tried a few things and can't get it to work at the moment with the HART signal broken out. Even if I ground it via a .22µ capacitor.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I put the capacitor back. It still didn't work, so it was "something else". I feared for a moment that I destroyed the board.

     

    Luckily, it turned out that it was one of the bodge wires on the break-out board that came loose. The circuit is ok and I can start over.

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Jan Cumps

    I finally got the board working with the HART pin broken out. I'll now update the firmware and do a first test ...