Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Drones Vs. Drones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: plowe
  • Date Created: 25 Jan 2016 2:06 PM Date Created
  • Views 7346 views
  • Likes 5 likes
  • Comments 59 comments
  • multi rotor
  • eagle
  • emerging_tech
  • multi-rotor
  • drone_news
  • multi rotor copter
  • drone_tech
  • drones
  • quadcopter
Related
Recommended

Drones Vs. Drones

plowe
plowe
25 Jan 2016

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

(Robotic falconry via Wired.Com)

 

The rise of Quadcopters and Drones has been a pretty quick one. You only have to look back to Christmas and see the numerous gadget shops that offered all sorts of cheap, off of the shelf remote controlled quadcopters to see that the technology has captured the imaginations of thousands of people around the world.

 

But what happens when that technology then needs to be kept in check? What happens, if that technology is being used for evil instead of good? (Insert your own version of 'with great power comes great responsibility' anecdote here). Well, it appears that the answer is to fight fire with fire...or more accurately Drones with Drones. Mechanical engineers from Michigan Tech University have developed an anti-drone drone that has abilities Spiderman himself would be proud of.

 

The weapon of choice is a giant net that not only fires at the offending drone, but remains attached for the attacking drone to drag its prey off to pretty much where ever it chooses. Mo Rastgaar, associate professor of mechanical engineering, said "It's like robotic falconry. What makes this unique is that the net is attached to our catcher, so you can retrieve the rogue drone or drop it in a designated, secure area."

 

Effective from up to 40 feet away, the drone catching net brings its target down upon impact and the idea of being able to carry it off means any intel that the drone has collected (as long as it's stored locally) is reclaimed and, in worse case scenarios, if the Drone is armed with explosives it can be brought down in a designated safe zone to reduce casualties and/or damage to surrounding buildings.

 

It's not the first attempt at using drones to police other drones,  in August Boeing unleashed their ground to air laser drone defense system which pretty much does what it says on the tin- spots a drone, fires laser, drone is dead...scary stuff. Others seem to be turning to more tech related methods to stop unwanted attention from the sky in the form of geo-fencing systems which prohibit a drone from flying in places by using GPS.

 

With rumors that the UK may be under threat from drones carrying explosives (Disclaimer: not sure just how true that is or how big a risk it is- please don't panic and buy anything to shoot down drones) it appears that this rise in anti-drone tech could be the start of an influx of tech based defenses to protect people from miniature aerial threats...

 

However, seeing as bears and even an eagle has been reported to have taken drones out then maybe a more natural solution could be considered- everyone is familiar with the resident Eagle at the Wimbledon Tennis Tournament which is employed to keep pigeons off of the courts; could we soon see homes and estates employing birds of prey to ward off drones?

 

Cue an epic battle in the skies that will ring throughout the ages: Drones Vs. Eagles...think I'll stay indoors for that one.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to gadget.iom +3
    We have a similar regulation here . It is, if anything, even more unwieldy and more legalese than the US one. I don't know about the states, but here there's a looming crisis. Air regulation relies on…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft…
  • crjeder
    crjeder over 10 years ago in reply to Dudley +3
    With "Drones" which weight much less than a wild goose they are a much smaller problem for aviation than the press makes us believe. Rotors of rescue helicopters can chop small trees easily, there is no…
Parents
  • stevemann
    stevemann over 10 years ago

    In both cases both the hawk and the net-firing drone are targeting stationary drones simply hovering in place.  Wow, big deal. anyone can hit the side of barn while standing next to it.

     

    There is absolutely no factual evidence to support the fear and ignorance around small personal drones. There have been more than a million hours of flight of small drones, yet there is not one verifiable report of a drone crash in the US that resulted in a serious injury as defined by the NTSB* to someone not connected to the flight. Not one. It is a safety rate that all other segments of aviation would be jealous to have. There is also not one verifiable report of a collision between a small drone and a manned aircraft. Not one. When it happens, the aircraft crew is probably not going to be aware of it, and the drone pieces will be scattered over a square mile. An FAA executive speaking to a nervous audience of helicopter operators at HAI Heli-Expo in Orlando (March 2015) and said that while there's never been a reported contact between an sUAS and a civilian aircraft, the military has some experience in that regard. In all cases the aircraft was virtually unscathed while the UAS was "smashed to pieces."

     

    Keep the risk of personal drones in perspective.

     

    Today (if this is an average day in the USA):

    1560 people will die from Cancer

    268 people in US hospitals will die because of medical mistakes.

    162 people will be wounded by firearms in the US.

    117 Americans will die in an automobile accident.

    98 people in the US will die from the flu.

    53 people will kill themselves with a firearm.

    46 children will suffer eye injuries.

    37 will die from AIDS.

    30 people will die in gun-related murders.

    18 pilots will report a Laser Incident

    3 General Aviation airplanes will crash in the US.

    0 people will be seriously injured or killed by a small drone accident.*

     

    Zero. Why are so many otherwise rational people so terrified of zero?

    The panic, here, is completely out of any sort of proportion to reality.

     

    * A band-aid is not a serious injury. CFR 49 §830.2 contains the definition of "Serious Injury" that the FAA and NTSB use in their aircraft and vehicular accident statistics. It is important to hold small UAS accidents to the same metric, otherwise comparisons are meaningless.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to stevemann

    True, but the perceived threat is still very high.

    Unless Drone users demonstrate some restraint in their use, then I am afraid that the press will continue to shout that the sky is falling.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to gadget.iom

    And, you point is ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to stevemann

    Stephen Mann wrote:

     

    And, your point is ??

    My point is that this article was linked from a news topic posted on here....

    And given the subject of Drones and Aviation I thought it might be appropriate.

     

    Do you want a paper bag?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to gadget.iom

    There are reports of drone "sightings" every day - most are unverified.

     

    The frequency of the reported sightings near London is a concern as it is higher than random acts of stupidity would explain.  I am suspecting that could be some idiot trying to deliberately hit an airliner.  If it is and he is caught, then yes, the authorities should throw the book at him.  The odds are that he will not succeed.  And if he somehow does, the odds are that the crew won't even notice the thump as the drone is smashed to smithereens.

     

    It would take remarkable skill or incredible luck for a drone operator to deliberately hit a target moving at 150 MPH or more relative to a top speed of 30 MPH for most personal drones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 10 years ago in reply to stevemann

    Who said anything about deliberate?

     

    I'm more worried about the muppets

    (Not these muppets)image

     

    The kinda muppets that think a video of a plane during take off captured from a UAV from 16ft is "cool".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 10 years ago in reply to shabaz

    The airspace near airports always was regulated. Even before "Drones" became popular. And those laws apply to everything man made which occupies airspace. Just as stevemann sayed: we do not need more laws. BTW: Laser pointer are still unregulated.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • crjeder
    crjeder over 10 years ago in reply to shabaz

    The airspace near airports always was regulated. Even before "Drones" became popular. And those laws apply to everything man made which occupies airspace. Just as stevemann sayed: we do not need more laws. BTW: Laser pointer are still unregulated.