Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Drones Vs. Drones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: plowe
  • Date Created: 25 Jan 2016 2:06 PM Date Created
  • Views 7346 views
  • Likes 5 likes
  • Comments 59 comments
  • multi rotor
  • eagle
  • emerging_tech
  • multi-rotor
  • drone_news
  • multi rotor copter
  • drone_tech
  • drones
  • quadcopter
Related
Recommended

Drones Vs. Drones

plowe
plowe
25 Jan 2016

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

(Robotic falconry via Wired.Com)

 

The rise of Quadcopters and Drones has been a pretty quick one. You only have to look back to Christmas and see the numerous gadget shops that offered all sorts of cheap, off of the shelf remote controlled quadcopters to see that the technology has captured the imaginations of thousands of people around the world.

 

But what happens when that technology then needs to be kept in check? What happens, if that technology is being used for evil instead of good? (Insert your own version of 'with great power comes great responsibility' anecdote here). Well, it appears that the answer is to fight fire with fire...or more accurately Drones with Drones. Mechanical engineers from Michigan Tech University have developed an anti-drone drone that has abilities Spiderman himself would be proud of.

 

The weapon of choice is a giant net that not only fires at the offending drone, but remains attached for the attacking drone to drag its prey off to pretty much where ever it chooses. Mo Rastgaar, associate professor of mechanical engineering, said "It's like robotic falconry. What makes this unique is that the net is attached to our catcher, so you can retrieve the rogue drone or drop it in a designated, secure area."

 

Effective from up to 40 feet away, the drone catching net brings its target down upon impact and the idea of being able to carry it off means any intel that the drone has collected (as long as it's stored locally) is reclaimed and, in worse case scenarios, if the Drone is armed with explosives it can be brought down in a designated safe zone to reduce casualties and/or damage to surrounding buildings.

 

It's not the first attempt at using drones to police other drones,  in August Boeing unleashed their ground to air laser drone defense system which pretty much does what it says on the tin- spots a drone, fires laser, drone is dead...scary stuff. Others seem to be turning to more tech related methods to stop unwanted attention from the sky in the form of geo-fencing systems which prohibit a drone from flying in places by using GPS.

 

With rumors that the UK may be under threat from drones carrying explosives (Disclaimer: not sure just how true that is or how big a risk it is- please don't panic and buy anything to shoot down drones) it appears that this rise in anti-drone tech could be the start of an influx of tech based defenses to protect people from miniature aerial threats...

 

However, seeing as bears and even an eagle has been reported to have taken drones out then maybe a more natural solution could be considered- everyone is familiar with the resident Eagle at the Wimbledon Tennis Tournament which is employed to keep pigeons off of the courts; could we soon see homes and estates employing birds of prey to ward off drones?

 

Cue an epic battle in the skies that will ring throughout the ages: Drones Vs. Eagles...think I'll stay indoors for that one.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to gadget.iom +3
    We have a similar regulation here . It is, if anything, even more unwieldy and more legalese than the US one. I don't know about the states, but here there's a looming crisis. Air regulation relies on…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft…
  • crjeder
    crjeder over 10 years ago in reply to Dudley +3
    With "Drones" which weight much less than a wild goose they are a much smaller problem for aviation than the press makes us believe. Rotors of rescue helicopters can chop small trees easily, there is no…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    its awesome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Dudley
    Dudley over 10 years ago in reply to e14 Contributor

    Catching things in the air with a giant net?

     

    Like this you mean?

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    (Warning, contains bad language)

     

    Begs the question, what happens to the person living underneath the drone that's been entangled. And whose liable for any damage? The drone owner? Or the person that wrapped the drone in a net?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1

    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft(especially some distance away) you can't even see it (white drone on a white cloudy sky ) except for maybe the lights.

    From a drone photography point of view most things you would want to photograph would look like dots or at least rather uninteresting from that height.

     

    That said I'm sure the world is full of sufficiently retarded and ignorant people....not sure the law however can help us here as a mass cull on them would bump off too many voters for our politicians image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to Dudley

    Hi Dudley!

     

    As far as I understand, if something is on your land (tree height is most likely considered your property) then you're entitled to get rid of it, and eject it off your property. I think any damage during the process will not be an issue provided it was not more excessive than necessary to do that. Your freehold extends a certain amount into the ground, and a certain amount into the air as I understand!

    Basically the same as if a shrub was growing on your side of the fence : ) you're entitled to chop it off regardless of it belonging to the neighbour. Provided one throws back the trimmings over the fence (otherwise it would be theft :).

    (I think there was a case where a plane photographed from the air in order to sell photos, and I think it was ruled that was ok, because it was sufficiently high. I could be wrong though, cant remember for sure).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Problemchild

    you can't even see it

    A lot of them now have video from onboard so that isn't an issue.

    Even the smaller versions have GPS, so again a lack of real control.

     

    500ft is not that high if you are looking for Aerial photos and perhaps doing some form of panoramic view.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to Problemchild

    Some place do provide open ranges.

    The local US AF base has a little used runway that they allow RC aircraft and I suspect drones to come and play.

    They provide a large area that is flat and away from anything of value, so people can do all sorts of activities without hurting anyone.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Dudley
    Dudley over 10 years ago in reply to shabaz

    One of the airfields I used to hang around to do skydiving at had an RC plane and drone club on site. There the rule was "if there are parachutes in the sky, drones and RC planes should be on the ground". A sensible arrangement that gave drones a totally clear piece of sky (almost no planes bust a dropzone due to the inherent dangers of hitting a person in freefall, or worse, catching a piece of parachute cord) and plenty of warning of when to bring them back in. Five years of skydiving at that site, and there was only one incident in those five years, and that was on a day when the weather really wasn't jump friendly but people went anyway.

     

    Responsible users aren't the issue tho - the issue is one of what is done about the irresponsible users, and the really big issue with it is the anonymity. The airprox reports I linked earlier all have the phrase "Drone operator could not be traced", and no amount of regulation will work if that regulation isn't enforceable.

     

    And shabaz, I'm not 100% sure of the regulations here, but there is definitely a threshold in property law in the UK where ground becomes sky. From memory, I think it's 250' above your property that is "your" sky, and above that it's "public" sky (but I could be wrong). There are notable exceptions to this, for example, if you live within a 2nm radius of an airport, then the sky belongs to the airport.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Dudley
    Dudley over 10 years ago in reply to shabaz

    One of the airfields I used to hang around to do skydiving at had an RC plane and drone club on site. There the rule was "if there are parachutes in the sky, drones and RC planes should be on the ground". A sensible arrangement that gave drones a totally clear piece of sky (almost no planes bust a dropzone due to the inherent dangers of hitting a person in freefall, or worse, catching a piece of parachute cord) and plenty of warning of when to bring them back in. Five years of skydiving at that site, and there was only one incident in those five years, and that was on a day when the weather really wasn't jump friendly but people went anyway.

     

    Responsible users aren't the issue tho - the issue is one of what is done about the irresponsible users, and the really big issue with it is the anonymity. The airprox reports I linked earlier all have the phrase "Drone operator could not be traced", and no amount of regulation will work if that regulation isn't enforceable.

     

    And shabaz, I'm not 100% sure of the regulations here, but there is definitely a threshold in property law in the UK where ground becomes sky. From memory, I think it's 250' above your property that is "your" sky, and above that it's "public" sky (but I could be wrong). There are notable exceptions to this, for example, if you live within a 2nm radius of an airport, then the sky belongs to the airport.