Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Drones Vs. Drones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: plowe
  • Date Created: 25 Jan 2016 2:06 PM Date Created
  • Views 7372 views
  • Likes 5 likes
  • Comments 59 comments
  • multi rotor
  • eagle
  • emerging_tech
  • multi-rotor
  • drone_news
  • multi rotor copter
  • drone_tech
  • drones
  • quadcopter
Related
Recommended

Drones Vs. Drones

plowe
plowe
25 Jan 2016

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

(Robotic falconry via Wired.Com)

 

The rise of Quadcopters and Drones has been a pretty quick one. You only have to look back to Christmas and see the numerous gadget shops that offered all sorts of cheap, off of the shelf remote controlled quadcopters to see that the technology has captured the imaginations of thousands of people around the world.

 

But what happens when that technology then needs to be kept in check? What happens, if that technology is being used for evil instead of good? (Insert your own version of 'with great power comes great responsibility' anecdote here). Well, it appears that the answer is to fight fire with fire...or more accurately Drones with Drones. Mechanical engineers from Michigan Tech University have developed an anti-drone drone that has abilities Spiderman himself would be proud of.

 

The weapon of choice is a giant net that not only fires at the offending drone, but remains attached for the attacking drone to drag its prey off to pretty much where ever it chooses. Mo Rastgaar, associate professor of mechanical engineering, said "It's like robotic falconry. What makes this unique is that the net is attached to our catcher, so you can retrieve the rogue drone or drop it in a designated, secure area."

 

Effective from up to 40 feet away, the drone catching net brings its target down upon impact and the idea of being able to carry it off means any intel that the drone has collected (as long as it's stored locally) is reclaimed and, in worse case scenarios, if the Drone is armed with explosives it can be brought down in a designated safe zone to reduce casualties and/or damage to surrounding buildings.

 

It's not the first attempt at using drones to police other drones,  in August Boeing unleashed their ground to air laser drone defense system which pretty much does what it says on the tin- spots a drone, fires laser, drone is dead...scary stuff. Others seem to be turning to more tech related methods to stop unwanted attention from the sky in the form of geo-fencing systems which prohibit a drone from flying in places by using GPS.

 

With rumors that the UK may be under threat from drones carrying explosives (Disclaimer: not sure just how true that is or how big a risk it is- please don't panic and buy anything to shoot down drones) it appears that this rise in anti-drone tech could be the start of an influx of tech based defenses to protect people from miniature aerial threats...

 

However, seeing as bears and even an eagle has been reported to have taken drones out then maybe a more natural solution could be considered- everyone is familiar with the resident Eagle at the Wimbledon Tennis Tournament which is employed to keep pigeons off of the courts; could we soon see homes and estates employing birds of prey to ward off drones?

 

Cue an epic battle in the skies that will ring throughout the ages: Drones Vs. Eagles...think I'll stay indoors for that one.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to gadget.iom +3
    We have a similar regulation here . It is, if anything, even more unwieldy and more legalese than the US one. I don't know about the states, but here there's a looming crisis. Air regulation relies on…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft…
  • crjeder
    crjeder over 10 years ago in reply to Dudley +3
    With "Drones" which weight much less than a wild goose they are a much smaller problem for aviation than the press makes us believe. Rotors of rescue helicopters can chop small trees easily, there is no…
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    its awesome

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Dudley
    Dudley over 10 years ago in reply to e14 Contributor

    Catching things in the air with a giant net?

     

    Like this you mean?

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    (Warning, contains bad language)

     

    Begs the question, what happens to the person living underneath the drone that's been entangled. And whose liable for any damage? The drone owner? Or the person that wrapped the drone in a net?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to mcb1

    True, but you only need one little bit to get into the wrong place and you will discover that gravity always wins.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to DAB

    I agree ... it was someone else that thought it was only a small ingestion ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • crjeder
    crjeder over 10 years ago in reply to mcb1

    Show me a copter that is more durable than "flesh and bones".

    But agreed. The test cases should be frozen chicken and DJI Phantom.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to crjeder

    The test cases should be frozen chicken and DJI Phantom.

    I did hear that someone was testing windshields and having problems until they were advised to thaw the bird out before launching it....

     

    The reality about engine design is that it is designed to be able to consume items it encounters in flight under 'normal' circumstances.

    Bird strike is a hazard that is identified at Airports, so ingesting a bird of xx size is mandatory.

     

    The cost of an ingestion is millions, both in physical repair but also rescheduling and sorting out the passengers.

    If they loose an engine on take-off the weight is usually too high to re-land and they sometimes need to dump fuel, as well as doing all the other things in the cockpit for a emergency landing on one engine.

     

    I can understand the desire to not add drones or RC aircraft to engine ingestion.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Dudley
    Dudley over 10 years ago in reply to gadget.iom

    I'm not often right, but seems I'm wrong again. Thanks for keeping me straight shabaz image

     

    And the problem isn't just the engine. Engines, windshields, landing gear, nose cone, wing leading edge, they all get tested for bird strike with a flesh and bone bird, but drones aren't made of flesh and bone. And while a bird is undoubtedly a lot less fragile than a drone - it's not hard to imagine what might happen to a stray piece of metal or a ballbearing hitting the fuselage at a bad angle might do to the fuselage. Bear in mind that closing speeds of 200mph are not uncommon.

     

    The analogy is if you were to hit a small bird when you're doing 110kph, it might do no damage to your car, but if you replaced it with a ballbearing of the same weight as the small bird, it's more likely to do some damage. Especially if it hits something inherently more fragile. Now make the ballbearing a sharp jagged piece of metal, and it's going to do even more.

     

    And also bear in mind that it doesn't have to be the big commercial jets when considering a collision with a drone - it could just as easily be a helicopter, or a light aircraft. They're much more prone to damage from a collision than the bigger planes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Dudley
    Dudley over 10 years ago in reply to gadget.iom

    I'm not often right, but seems I'm wrong again. Thanks for keeping me straight shabaz image

     

    And the problem isn't just the engine. Engines, windshields, landing gear, nose cone, wing leading edge, they all get tested for bird strike with a flesh and bone bird, but drones aren't made of flesh and bone. And while a bird is undoubtedly a lot less fragile than a drone - it's not hard to imagine what might happen to a stray piece of metal or a ballbearing hitting the fuselage at a bad angle might do to the fuselage. Bear in mind that closing speeds of 200mph are not uncommon.

     

    The analogy is if you were to hit a small bird when you're doing 110kph, it might do no damage to your car, but if you replaced it with a ballbearing of the same weight as the small bird, it's more likely to do some damage. Especially if it hits something inherently more fragile. Now make the ballbearing a sharp jagged piece of metal, and it's going to do even more.

     

    And also bear in mind that it doesn't have to be the big commercial jets when considering a collision with a drone - it could just as easily be a helicopter, or a light aircraft. They're much more prone to damage from a collision than the bigger planes.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • shabaz
    shabaz over 10 years ago in reply to Dudley

    Hi Dudley,

    250' may well be the case actually. The Bernstein v Skyviews was just the first case that established that property doesn't extend infinitely upwards, but it was probably refined later with legislation.

    I'm halfway through 'Destination Disaster' since you recommended it - extremely interesting book (and very moving reading in detail exactly what occurred).