Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Drones Vs. Drones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: plowe
  • Date Created: 25 Jan 2016 2:06 PM Date Created
  • Views 7381 views
  • Likes 5 likes
  • Comments 59 comments
  • multi rotor
  • eagle
  • emerging_tech
  • multi-rotor
  • drone_news
  • multi rotor copter
  • drone_tech
  • drones
  • quadcopter
Related
Recommended

Drones Vs. Drones

plowe
plowe
25 Jan 2016

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

(Robotic falconry via Wired.Com)

 

The rise of Quadcopters and Drones has been a pretty quick one. You only have to look back to Christmas and see the numerous gadget shops that offered all sorts of cheap, off of the shelf remote controlled quadcopters to see that the technology has captured the imaginations of thousands of people around the world.

 

But what happens when that technology then needs to be kept in check? What happens, if that technology is being used for evil instead of good? (Insert your own version of 'with great power comes great responsibility' anecdote here). Well, it appears that the answer is to fight fire with fire...or more accurately Drones with Drones. Mechanical engineers from Michigan Tech University have developed an anti-drone drone that has abilities Spiderman himself would be proud of.

 

The weapon of choice is a giant net that not only fires at the offending drone, but remains attached for the attacking drone to drag its prey off to pretty much where ever it chooses. Mo Rastgaar, associate professor of mechanical engineering, said "It's like robotic falconry. What makes this unique is that the net is attached to our catcher, so you can retrieve the rogue drone or drop it in a designated, secure area."

 

Effective from up to 40 feet away, the drone catching net brings its target down upon impact and the idea of being able to carry it off means any intel that the drone has collected (as long as it's stored locally) is reclaimed and, in worse case scenarios, if the Drone is armed with explosives it can be brought down in a designated safe zone to reduce casualties and/or damage to surrounding buildings.

 

It's not the first attempt at using drones to police other drones,  in August Boeing unleashed their ground to air laser drone defense system which pretty much does what it says on the tin- spots a drone, fires laser, drone is dead...scary stuff. Others seem to be turning to more tech related methods to stop unwanted attention from the sky in the form of geo-fencing systems which prohibit a drone from flying in places by using GPS.

 

With rumors that the UK may be under threat from drones carrying explosives (Disclaimer: not sure just how true that is or how big a risk it is- please don't panic and buy anything to shoot down drones) it appears that this rise in anti-drone tech could be the start of an influx of tech based defenses to protect people from miniature aerial threats...

 

However, seeing as bears and even an eagle has been reported to have taken drones out then maybe a more natural solution could be considered- everyone is familiar with the resident Eagle at the Wimbledon Tennis Tournament which is employed to keep pigeons off of the courts; could we soon see homes and estates employing birds of prey to ward off drones?

 

Cue an epic battle in the skies that will ring throughout the ages: Drones Vs. Eagles...think I'll stay indoors for that one.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to gadget.iom +3
    We have a similar regulation here . It is, if anything, even more unwieldy and more legalese than the US one. I don't know about the states, but here there's a looming crisis. Air regulation relies on…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft…
  • crjeder
    crjeder over 10 years ago in reply to Dudley +3
    With "Drones" which weight much less than a wild goose they are a much smaller problem for aviation than the press makes us believe. Rotors of rescue helicopters can chop small trees easily, there is no…
  • PEarle
    PEarle over 10 years ago

    Perhaps this is the lo-tech answer

     

    Police 'ponder eagles to tackle drones' - BBC News

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to mcb1

    The threat of a collision between a personal drone and a manned aircraft isn't being ignored - IT'S NEVER HAPPENED!

    People are panicked over something that has never happened and are trying to legislate the imagined threat out of existence.

     

    Most personal drones, especially the toys that are most likely to be found near manned aircraft, most often by accident or ignorance, are mostly plastic with a little metal and a battery that is mostly wet napkins. It's really no more a threat to an aircraft than a large bird.

     

    This is what we in the rational world call "Fear Mongering". Seriously, a solitary drone in an accident with an air carrier aircraft is never going to bring down the airplane. It took a flock of geese to bring down Captain Sullenberg's "Miracle on the Hudson". One personal drone could, though unlikely, cause enough damage for the airplane to return for a landing, but the likelihood of causing a catastrophic crash is so remarkably remote that it probably won't happen in my lifetime or my kids' lifetimes. Notwithstanding the sensational news reports. "Oh - the pilot saw a drone, we're all gonna' die".

     

    The most likely first contact between a personal drone and a civil aircraft is going to go unnoticed by the crew and pieces of the drone will be scattered over a few square miles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to stevemann

    The stats might be right or may be out because of under-reporting.

     

    Whatever it is the problem will only get worse unless users are educated and do start observing the relevant regulations.

     

    There are many small and very cheap drones becoming available, but with remote viewing technology becoming so much more afordable, the potential problem will grow.

     

     

    Deciding to ignore it until it is a problem is rather foolish IMO.

    Making people aware now before it becomes an issue os the best method ot ensure it doesn't result in a fatality

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    In the US it is a Federal Crime, a felony at that, to interfere with an aircraft. With the new regulations which have gotten so much press most people should now realize that "defending yourself" against a drone is very likely illegal and could result in several years in Federal Prison.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to DAB

    I disagree with your assessment that unless "Drone users demonstrate some restraint".

    There's more than a million of them in the wild and how many have been seen AND VERIFIED near an airport? A dozen? Two?  That would be 2.4E-5 - a miniscule number.  You put a million of anything in the hands of consumers and there will always be a small percentage who don't know or care about the potential problems they may cause.

     

    The math says that 99.99040023039% of the users are flying responsibly. And yet you tarnish the whole community for the irresponsible acts of an extreme minority? No amount of legislation or rulemaking will achieve 100%, but denigrating the entire drone community is certainly not the answer.

     

    I seriously doubt the veracity of many of the drone "sightings" since the vast majority of them are unverified.  Go back 50 years when pilots were saying "I saw a UFO". The transcripts are almost identical. I am a retired commercial pilot and reading the FAA Drone Sighting database is laughable.  It would be hilarious if so many people didn't take it as "the sky is falling".  One of the reports was a drone found in a tree. Wow, the public is in imminent danger from that one.  Another is a drone that followed a twin-engine general aviation airplane 30 miles to an airport at well over 120 knots.  Show me a drone that can follow an aircraft for 30 miles at 120 KPH, and I'll show you the USAF markings on it. Certainly not a personal drone.  Or how about at 24,000 ft and 30 miles over the ocean?  No personal drone can go that high and that far.  There is absolutely no way that most of the reported sightings are actually personal drones, and almost every one of them is unverified. No airline pilot has eyesight so good that they can see a dinner-plate object five hundred feet away from them, especially when the super observer is moving at over 150 KPH.

     

    As I said, the panic, here, is completely out of any sort of proportion to reality.

     

    On the OT of Drone v Drone - it ain't gonna happen.

     

    Unless you are in the same general location of the suspected intruder drone, and the intruder drone is going to hover for you to intercept it, there's no way the net or falcon "solution" would work.  By the time you can deploy the magical defense, the intruder drone's batteries have run out and the operator is packing up and going home. Just another dumb solution in search of a real problem.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>