Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Drones Vs. Drones
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: plowe
  • Date Created: 25 Jan 2016 2:06 PM Date Created
  • Views 7372 views
  • Likes 5 likes
  • Comments 59 comments
  • multi rotor
  • eagle
  • emerging_tech
  • multi-rotor
  • drone_news
  • multi rotor copter
  • drone_tech
  • drones
  • quadcopter
Related
Recommended

Drones Vs. Drones

plowe
plowe
25 Jan 2016

image

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

(Robotic falconry via Wired.Com)

 

The rise of Quadcopters and Drones has been a pretty quick one. You only have to look back to Christmas and see the numerous gadget shops that offered all sorts of cheap, off of the shelf remote controlled quadcopters to see that the technology has captured the imaginations of thousands of people around the world.

 

But what happens when that technology then needs to be kept in check? What happens, if that technology is being used for evil instead of good? (Insert your own version of 'with great power comes great responsibility' anecdote here). Well, it appears that the answer is to fight fire with fire...or more accurately Drones with Drones. Mechanical engineers from Michigan Tech University have developed an anti-drone drone that has abilities Spiderman himself would be proud of.

 

The weapon of choice is a giant net that not only fires at the offending drone, but remains attached for the attacking drone to drag its prey off to pretty much where ever it chooses. Mo Rastgaar, associate professor of mechanical engineering, said "It's like robotic falconry. What makes this unique is that the net is attached to our catcher, so you can retrieve the rogue drone or drop it in a designated, secure area."

 

Effective from up to 40 feet away, the drone catching net brings its target down upon impact and the idea of being able to carry it off means any intel that the drone has collected (as long as it's stored locally) is reclaimed and, in worse case scenarios, if the Drone is armed with explosives it can be brought down in a designated safe zone to reduce casualties and/or damage to surrounding buildings.

 

It's not the first attempt at using drones to police other drones,  in August Boeing unleashed their ground to air laser drone defense system which pretty much does what it says on the tin- spots a drone, fires laser, drone is dead...scary stuff. Others seem to be turning to more tech related methods to stop unwanted attention from the sky in the form of geo-fencing systems which prohibit a drone from flying in places by using GPS.

 

With rumors that the UK may be under threat from drones carrying explosives (Disclaimer: not sure just how true that is or how big a risk it is- please don't panic and buy anything to shoot down drones) it appears that this rise in anti-drone tech could be the start of an influx of tech based defenses to protect people from miniature aerial threats...

 

However, seeing as bears and even an eagle has been reported to have taken drones out then maybe a more natural solution could be considered- everyone is familiar with the resident Eagle at the Wimbledon Tennis Tournament which is employed to keep pigeons off of the courts; could we soon see homes and estates employing birds of prey to ward off drones?

 

Cue an epic battle in the skies that will ring throughout the ages: Drones Vs. Eagles...think I'll stay indoors for that one.

 

This video is unavailable.
You don't have permission to edit metadata of this video.

  • Sign in to reply

Top Comments

  • Dudley
    Dudley over 10 years ago in reply to gadget.iom +3
    We have a similar regulation here . It is, if anything, even more unwieldy and more legalese than the US one. I don't know about the states, but here there's a looming crisis. Air regulation relies on…
  • Problemchild
    Problemchild over 10 years ago in reply to mcb1 +3
    Hi Mark, yeah 500ft isn't that high for a drone to achieve. You've go to wonder why you want to do that though especially on some regular habitual basis as above 50 ish feet you can't hear it and at 500ft…
  • crjeder
    crjeder over 10 years ago in reply to Dudley +3
    With "Drones" which weight much less than a wild goose they are a much smaller problem for aviation than the press makes us believe. Rotors of rescue helicopters can chop small trees easily, there is no…
  • shabaz
    shabaz over 10 years ago in reply to stevemann

    For Concorde it took just 10 pounds of tyre fragment and that was sufficient to end 113 lives. If there was a drone on a runway, isn't there a reasonable risk it could cause damage?

    (Genuinely asking this question - I have no idea but the risk sounds plausible so it would be good to hear from experts). To me, some legislation on drones seems a sensible thing to do.

    Not knee-jerk legislation (no-one wants that generally) but something to reduce the risk of aircraft and objects colliding.

     

    Today other objects far smaller than some drones are banned from anywhere near an airport too, so it is not necessarily a totally new concept to have legislation concerning people's activities near airports.

     

    For example toy model rockets are banned from being launched within a 5 mile radius of airports in the UK - and they're made of paper with the bare minimum fuel. Which would be a higher risk, a drone that can be positioned with accuracy, or a paper rocket?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to mcb1

    I NEVER said they were no threat and that contact would be inconsequential. I said that a single personal drone will never bring down an airliner.

     

    There is not a single report of a personal UAS/drone in the FAA Accident and Incident database. Not one. If there is other data I should be watching, please tell me.  The reason the general public doesn't hear about most of the aircraft accidents and incidents is because they happen every day. As I said above, today in the US, 18 pilots will report a Laser Incident and 3 General Aviation airplanes will crash.

     

    If there were a verifiable collision between a manned aircraft and a personal drone, you can bet a paycheck that it will be in every newspaper and cable news channel. After all, as hyper-sensitive as the general public and the news organizations are to personal drone news, even a broken window in a florida home was national news. (http://www.miamiherald.com/news/local/community/miami-dade/hialeah/article11873771.html)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • stevemann
    stevemann over 10 years ago in reply to DAB

    In the case of the drones over the California wildfires, only one was verified, and it was many miles from the active firefighting area and not within the TFR.

    Where there are VERIFIED drones causing problems, I would agree with you. But today it is too easy to see a bird and say "I thought I saw a drone - we're all gonna die", and everyone screams for more regulations.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to stevemann

    Unfortunately for you, many of us have been around long enough to see things that would never ever happen, actually happen.

     

    I'm pleased to know that you're happy to be billed for any damage " are mostly plastic with a little metal and a battery that is mostly wet napkins. It's really no more a threat to an aircraft than a large bird."

    There is not only the cost of stripdown and inspection, but the resheduling of crew and passengers.

     

     

    It seems that there is a lot of noise being made by someone who claims to be operating legitimately.

    The last time I saw this was someone trying to sell something that didn't work as intended.

     

    There are multiple incidents within Aviation that never make the Press.

    The Authorities are aware of them, but the general public aren't, so you're basing your argument on a limited set of data.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to stevemann

    Perhaps, but the laws will still be based upon the perception.

     

    Nobody sees the 99.99% of safe flights, but 100 of Millions of people saw the drone nearly hit the skier.

     

    No matter what you say, the onus will always be on the drone users to prove they are not causing trouble.

     

    One bad publicity event and you quickly turn public opinion.  Those events always work against peoples freedoms.

     

    The one case I remember from this past summer was the announcement that fire fighters in California had to ground their helicopters and retardant dropping aircraft because  there were people flying drones in the area trying to get pictures of the range fires.  Not good press for drones when they came back and showed dozens of homes that burned because of the grounding.

     

    I agree, by themselves drones are not a problem.  Unfortunately like any tool, they can be used for bad things and those few abuses punish everyone using them.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>