Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Elderly Activity Monitoring Using Agile SmartEdge
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jarain_78
  • Date Created: 4 Sep 2019 5:34 PM Date Created
  • Views 943 views
  • Likes 3 likes
  • Comments 1 comment
Related
Recommended

Elderly Activity Monitoring Using Agile SmartEdge

jarain_78
jarain_78
4 Sep 2019
Story

 

 

In recent years there has been anincrease in applications related to Internet objects (IoT), the vast majority ofthese applications focus primarily on the control of our homes, themotorization of environmental data, intelligent cities, and so on. At the sametime, we have seen that these new devices are increasingly powerful, whichallows to incorporate automatic learning algorithms. These algorithms allow usto recognize patterns and learn autonomously using information from sensors, images, signals, etc. One of the problems observed today is the existence ofelderly people who live alone and need continuous monitoring.

 

 

Objective

 

 

The objective of this project is to be able to use the Agile SmartEdge system as an exercise monitoring system for older people and link it to an assistant robot that I did during my doctorate. The robot will be used as an activity recommendation tool and the Agile SmartEdge system will monitor whether the activity has been performed correctly. This will be done using all its sensors (3D accelerometers, a 3D gyroscope, a 3D magnetometer, a pressure sensor, a humidity and temperature sensor, a microphone, an ambient light sensor and a proximity sensor) and its motion recognizer (Brainium).

 

 

Problem to be Solved

 

 

The problem we are trying to solve is to detect and monitor the activities carried out by older people living alone. As in some cases they live alone and have no one to take care of them, stop performing the activities suggested by doctors or physiotherapists. Activities such as walking or gentle exercises that help the proper functioning of their joints and thus try to prevent possible problems in the future.

 

 

Elderly Activity Monitoring Using Agile SmartEdge

 

 

In order to do this, a robot has been developed capable of connecting to the service offered by Brainium through a raspberry pi, to make this connection is necessary to activate the gateways. These are the steps to be taken:

 

 

1. InstallBluez 5.50 to do it, connect through SSH and write the following:

 

wget https://brainium.blob.core.windows.net/public/raspberry/bluez.run sudo sh bluez.run 

 

2. Fromthe same SSH connection we receive the following:

 

wgethttps://brainium.blob.core.windows.net/public/raspberry/brainium-gateway-gtk-latest.runsudo sh ./brainium-gateway-gtk-latest.run 

 

3. Toopen the Manage GUI type the following:

 

brainium-gateway-gtk 

 

It is important to note that toperform step 3, it is necessary to have our raspberry connected to a monitor orLCD screen. Since when executing the command of step 3, we will open aninterface like the one shown in the following Figure 1.

 

 

image.png

Figure 1, Brainium Login

 

In this interface it will benecessary to authenticate ourselves with our credentials, it is assumed that wehave already linked our device to our brainium account. The only thing we willdo is change the Gateway to which our device was connected (Figure 2).

 

 

image.png

 

Figure 2, Searching Device

 


 

 

image.png

 

Figure 3, Adding Device

 


 

 

image.png

Figure 4, Selecting the Gateway

 

Once our device is linqueado andwith the correct Gateway activated in our console, the next step is to startcapturing the information (exercises). It is important to point out that theexercises to be classified are exercises in which the movement of the chest isinvolved, this is why it is necessary to use a harness. This harness willattach our sensor to the chest as shown in the Figure 5.

 

 

image.png

Figure 5, Sensor and Harness Joined

 

Once the sensor is in position, the next thing to do is to start capturing the data, for which the differentexercises were performed. Performing 5 sessions of 10 repetitions per exercise shown in the Figure 6.

 

 

image.png

 

Figure 6, Section of the 5 exercises

 


 

 

image.png

 

Figure 7, Graph of one of the exercises

 

At the end of the dataacquisition phase, the next step is to train the model. To do this, select allthe samples from each of the sessions and click on general model (Figure 8).

 

 

image.png

 

Figure 8, Model Generation

 

Once the model is generated, we will see a screen like the one shown in the following Figure 9.

 

 


 

 

3.png

 

Figure 9, Generated model

 


 

 

The next step is to apply ourmodel to our device (Figure 10).

 

 

image.png

 

Figure 10, Applying the model to the device

 


 

 

image.png

 

Figure 11, Tested the model

 


 

 

Once the configuration of thesensor and the acquisition of the data to be trained has been carried out, thenext step is to use the robot to track the activities. The robot used can be seen in thefollowing Figure 12, this robot was built using a raspberry pi 3, a 7" LCDscreen, a camera, some makebeam for the structure, a mega arduino (motorcontrol) and two DC motors. The robot responds to voice command, using the Snips system (https://snips.ai/). Using this voice recognitionsystem, the user can interact with the robot using his voice. In this way, theuser can request a recommendation for some type of physical activity. Three mqtt clients have beencreated to control the robot, one that controls voice recognition andrecommends activities. The next client controls the motors and the camera andfinally a third client acquires the information from the environmental sensors ofthe Rapid IoT device.To launch these clients, a"sh" file called "./run_snips_emir.sh" was created, whichautomatically executes the three python scripts:

 

#!/bin/bash     

python3 action_emir_v_0.0.1.py &     

python3 mqtt_iot_publish_data.py &    

python3 mqtt_robot_publish_data.py &   

wait   

 

The robot has 4 ultrasonicsensors, which are located at the front of the robot, right, left and one atthe back. These sensors are controlled through an Arduino mega and thedistances are sent through the serial port to the raspberry pi to the client mqtt_robot_publish_data.py. Once the client receives the information from the sensors, it publishes them tothe main client. At the same time, the client mqtt_robot_publish_data.py is incharge of controlling the engines, sending the different commands by voice, such as move forward, backward, left and right.

 

 

image.png

 

Figure 12, Assitant robot

 


 

 

image.png

 

Figure 13, Robot Circuit

 

Below is a description of the process that the user performs for the recommendation of an activity:

 

 

1: It asks the robot to recommend a physical activity.

 

 

2: The robot shows the 4 exercises that it has registered.

 

 

3: The robot recommends that you use the sensor and the harness.

 

 

4: The sensor recognizes the movement and sends it to the robot, which is responsible for counting them.

 

 

5: Once the exercise is finished, the robot encourages you with encouraging words so that you can continue performing the exercises.

 

Note: Since the images explaining theexercises are copyrighted, I will only give the names of the exercises. If youwant more information and see the images of the respective exercises, inreferences I leave the links.

Exercise Nº 1: Clock Reach

Exercise Nº 2: Balancing Wand

Exercise Nº 3: Wall Pushups

Exercise Nº 4: Mini Squats

 

image

 

Figure 14, The robot shows the different exercises

 


 

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image



 

 


 

 

References

 

 

https://www.lifeline.ca/en/resources/14-exercises-for-seniors-to-improve-strength-and-balance/ (exercises)

 

 

https://spa.brainium.com/apps/linux

 

 

https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fbrainium.blob.core.windows.net%2Fpublic%2Fdocs%2Fcacert.crt

 

 

https://www.element14.com/community/roadTestReviews/2982/l/brainium-smartedge-agile-review

 

  • Sign in to reply

Top Comments

  • clem57
    clem57 over 6 years ago +1
    Nicely done. I do like the robot part the best. jarain_78 this kind of reminds me of a commercial for Peleton , but for seniors instead.
  • clem57
    clem57 over 6 years ago

    Nicely done. I do like the robot part the best. jarain_78 this kind of reminds me of a commercial for Peleton, but for seniors instead.