Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Experimenting with a Cascode Switch
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jc2048
  • Date Created: 7 Jan 2021 10:26 PM Date Created
  • Views 3924 views
  • Likes 8 likes
  • Comments 8 comments
  • mosfet
  • cascode
  • arduino uno board
  • jfet
  • led
  • jc2048
Related
Recommended

Experimenting with a Cascode Switch

jc2048
jc2048
7 Jan 2021

This one came out of reading about GaN FETs in this 'essentials' blog: Semiconductors I GaNFETs for Power Conversion

 

When I had a look at the datasheet for one of the parts being advertised, I realised from the

equivalent circuit that it was a cascode combination of an Si [silicon] MOSFET and a GaN [gallium

nitride] FET (it would appear that that combination has become available because it looks like they

are growing the GaN on a Si substrate). This is how it's shown in the datasheet:

 

image

 

Although I've come across the cascode configuration as a two-stage analogue amplifier, I'm not very

familiar with how it behaves when switching, so I thought I'd experiment a bit. The actual parts in

that article are very expensive [about £10 in one-off quantities], would have the disadvantage of my

not being able to probe the junction between the Si part and the GaN part anyway, and I don't have

good test equipment for working at high currents, so I've thrown together a very low-powered version

to look at.

 

My cascode uses a BS170 mosfet for the lower switch and a BF256BBF256B n-type JFET for the upper. This will

behave quite differently to the GaN FET, so don't treat the two as in any way equivalent, but it

enables me to get an idea how the switching occurs and what the pros and cons of such a configuration

might be.

 

I'm going to set up two switches side by side, one consisting of just a BS170 part and the other

being the cascode connected BS170 and BF256BBF256B. That way I can compare the two. The input is going to

come from an IO pin of an Arduino Uno. I've previously found that that makes quite a nice pulse

generator for this kind of experiment: the output pins are fast and well behaved.

 

Here's my circuit. I used a 2N7000, instead of the BS170, for the simulation because of difficulties

with importing a model for the BS170. They're very similar, though, in the way they behave.

 

image

Because the Idss [current when Vgs is zero] of the BF256BBF256B is only about 9mA, I'm going to need to

keep the load current a good bit below that, so my load is a 10k resistor. With the rail at 20V, that

will give a current of around 2mA when the switch is on, which is well within the capability of the

JFET to deal with.

 

Here's how the two outputs behave when they're switching [blue is the single MOSFET, yellow is the

cascode]

 

image

 

Here's how it looks in the simulator:

 

image

 

Although there are some minor differences [which we'd expect, as the actual devices won't perfectly

match the typical figures used for the models], the essential features of the waveforms are all

there, so the simulator is modelling the active devices reasonably well.

 

Here are the waveforms for switching on and switching off in more detail

 

image

 

image

 

The single device is faster to switch on, but seems to be slower to switch off. Something to notice

in that second waveform is that both curves are more or less the same up to 2.5V, where they then

start to diverge. To see better what was happening, I probed the cascode, with one probe on the drain

of the MOSFET [blue] and the other on the drain of the JFET [yellow].

 

image

 

Here's the turn off in more detail

 

image

 

It's not too difficult to work out what's happening here.

 

About two divisions across, the gate voltage falls and the turning off starts. Initially, the drain

of the MOSFET goes the wrong way. That's because the load is very light and the intrinsic capacitance

from the gate of the MOSFET to the drain can couple the very fast falling gate edge across. Once

that's out of the way, we see the MOSFET turning off and the voltage at the drain rising. The two

curves track each other because the JFET is still on at this point [the small difference between them

being the drop from the JFET's 'on' resistance]. As the voltage at the source of the JFET rises, the

gate held at zero volts is going negative with respect to it and the JFET will also start to turn

off. The two curves will then steadily diverge as the resistance of the JFET increases.

 

The voltage at the drain of the MOSFET then hovers at something like the inverse of the gate

threshold of the JFET. With both devices off, that node is isolated and the voltage is held by the

intrinsic capacitance within both parts. In reality, with the oscilloscope probe attached [10M

resistance], it will be a little lower as the probe will have the effect of discharging the

capacitance, resulting in the JFET then turning on slightly to counterbalance the discharge current.

Once both devices are fully off, the rest of the curve is then simply the 10k resistor charging the

capacitance at the drain of the JFET up to the rail voltage.

 

Looking at the cascode at the point where the transistors turn on we have this

 

image

 

Here we can see that the MOSFET is quite snappy, completing in about 10ns. Again, as with the turn

off, there's feedthrough of the gate signal to the drain.

 

In contrast the JFET seems slow. But that's because, although it is on, it regulates the current and

that results in this steady downward ramp of the voltage as it discharges the intrinsic capacitance

at the drain [plus the capacitance at the probe tip, of course].

 

So some tentative observations.

 

1. We can see that the MOSFET's drain voltage excursion with the cascode is low, even where the load

is tied to a high voltage rail. The top transistor is shielding the lower one from the voltage. In my

circuit that's irrelevant because both transistors happen to have the same 60V maximum drain voltage,

but with the GaN FET it means the lower Si part can be a low voltage one and I assume that means that

it can be made with lower intrinsic capacitances and so switch faster [for a given current].

 

2. A second advantage of the cascode is that the drain voltage doesn't have to move very far, so that

too speeds the switching time of the part. Presumably, that evens things up a bit between the Si part

and the GaN part: the GaN devive will be faster, but has the burden of slewing its output over a much

greater voltage.

 

3. Once both transistors are off, the cascode arrangement may have an advantage of less capacitance

at the output, but that's very dependent on device properties. In a sense, for the cascode, the top

transistor is shielding the load from the capacitance of the bottom transistor, but whether that

makes any real difference is a 'that depends' type question.

 

The circuit I'm experimenting with here isn't particularly useful with these small-current

components. There is, though, one thing I could try with it. As the bottom transistor stays in the 0

-5V range, instead of having a separate discrete transistor I could just substitute the one that's

inside the processor driving the I/O pin. Also, since the JFET will regulate the current to about

9mA, it would make a reasonable LED driver. So something like this might work quite well, as long as

I keep an eye on the dissipation in the JFET.

 

image

 

And it does work. Some flashing LEDs, in case you've never seen them doing this before.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Here are the switching waveforms. The yellow trace is the output pin of the Arduino and the blue

trace the voltage at he bottom of the string of LEDs.

 

image

 

The pin output does indeed stay between 0V and 5V. The blue trace comes down to about 6.8V when

they're on, so that's about 1.7V for each LED. When they're off, you'll notice that the voltage only

rises to about 11V. That's because the diodes have a reverse capacitance that's only going to be

discharged by leakage currents (through the LEDs and the JFET) and the oscilloscope probe (10M to

ground). It's possible, I suppose, that I've inadvertently contrived a situation here where I've got

the leakage currents cancelling each other out because it doesn't move very far at all during the

half-second off period.

 

Here's the turning on in more detail.

 

image

 

The yellow trace is again the Arduino output. The MOSFET in the processor is nicely behaved, taking

the source of the JFET to ground without any fuss. As we saw earlier, the JFET regulates the current,

so the blue trace falls in a very measured way. The LEDs will be emitting light after about 10ns.

 

Finally, this is the turn off

 

image

 

I hope that was of some interest. Feel free to correct me if I have anything wrong. These blogs are

just me experimenting with things, they're not tutorials or lessons, and I quite often get in a

muddle trying to puzzle things out and explain them to myself, so don't assume everything I write is

necessarily accurate.

 

If you found this interesting and would like to see more blogs I've written, a list can be found

here:jc2048 Blog Index

  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 5 years ago +2
    I have a question about the last part, where the IO of an Arduino is used. How do you turn Arduino pin 12 into an open collector configuration? Or is that not needed?
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps +2
    I didn't. The upper MOSFET on the IO driver is clamping the IO pin to 5V when the output pin goes high. I would think that's why the pin waveform manages to stop so nicely when it gets up to 5V and not…
  • Andrew J
    Andrew J over 5 years ago +2
    You do a lot of great experiments Jon and I always find it interesting reading about them.
Parents
  • Jan Cumps
    Jan Cumps over 5 years ago

    I have a question about the last part, where the IO of an Arduino is used.

    How do you turn Arduino pin 12 into an open collector configuration? Or is that not needed?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps

    If I set the output pin low and then control the direction, so that only the lower MOSFET is active, I see this

     

    image

     

    This is then similar to what I had with the discrete MOSFET. That shows nicely the way that the JFET turning off shields the output from the load voltage. Bear in mind that I'm using a JFET intended for VHF work and it's [just about] keeping up with the processor's MOSFET.

     

    This is the code, in case anyone's interested.

     

    /* cascode switch test
    Repetitively sets UNO pin 12 active low for half second, then off for half second
    This is specific to UNO. 
    */
    void setup() {
      PORTB &= ~0x10;
    }
    void loop() {
      while(1) {
        DDRB |= 0x10;
        delay(500);  
        DDRB &= ~0x10;
        delay(500);  
        }
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps

    If I set the output pin low and then control the direction, so that only the lower MOSFET is active, I see this

     

    image

     

    This is then similar to what I had with the discrete MOSFET. That shows nicely the way that the JFET turning off shields the output from the load voltage. Bear in mind that I'm using a JFET intended for VHF work and it's [just about] keeping up with the processor's MOSFET.

     

    This is the code, in case anyone's interested.

     

    /* cascode switch test
    Repetitively sets UNO pin 12 active low for half second, then off for half second
    This is specific to UNO. 
    */
    void setup() {
      PORTB &= ~0x10;
    }
    void loop() {
      while(1) {
        DDRB |= 0x10;
        delay(500);  
        DDRB &= ~0x10;
        delay(500);  
        }
    }

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to jc2048

    There seem two pins on the ATMega that support open collector without having to change them to inputs: the i2c pins.

    You have to define them as i2c, then can use them as generic output pins with open collector.

    I haven't tried it, just stumbled on that while looking for "Arduino Open Collector".

    I'll check it this weekend ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 5 years ago in reply to Jan Cumps

    ...

    There seem two pins on the ATMega that support open collector without having to change them to inputs: the i2c pins.

    You have to define them as i2c, then can use them as generic output pins with open collector.

    I haven't tried it, just stumbled on that while looking for "Arduino Open Collector".

    I'll check it this weekend ...

    I could not get it to work.

    I used this setup, that should work for open collector and hard driven outputs, one on the SDA and one on the SDC pin:

    image

     

    I used this program, and commented some lines in setup to test the scenarios:

    #include <Wire.h>
    
    void setup() {
      pinMode(18, OUTPUT);
      pinMode(19, OUTPUT);
      //Wire.begin();  
      //TWCR = (1<<TWEN);
      //pinMode(18, INPUT);
      //pinMode(19, INPUT);  
    }
    
    void loop() {
      static uint8_t pinState = LOW;
      digitalWrite(18, pinState);
      digitalWrite(19, pinState);
      pinState = (pinState == LOW) ? HIGH : LOW;
      delay(500);
    }

     

    When I use pinMode(x, OUTPUT), the output swings between 0 and 5 V.

     

    When I use Wire.begin() or the TWCR register to turn the 2 pins into i2c mode, the voltage swings between 3.6 and 5 V.

    Same when I use pinMode(x, INPUT).

     

    I thought it was related to the current (13 - 15 mA). But when I replace the diode and resistor with a 10k resistor, it stays at 5 V all the time ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 5 years ago in reply to Jan Cumps

    The datasheet explains how the alternate control of the pins work. There's a diagram on page 81 and then a table on

    page 88.

     

    image

     

     

    image

     

    this is saying that the output data is forced to 0 [PVOV=0], rather than coming from the output data register, and

    the output enable control [DDOV], which is normally controlled by the pin direction register, is now controlled by

    SDO_OUT.