Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Exploring FPGAs
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: billabott
  • Date Created: 14 Aug 2013 11:42 PM Date Created
  • Views 1282 views
  • Likes 1 like
  • Comments 8 comments
  • fpga
Related
Recommended

Exploring FPGAs

billabott
billabott
14 Aug 2013

Thanks to a wonderful fellow engineer, Mr. Shabaz, I now have a KNJN.com Pluto II FPGA board with an Altera Cyclone installed to experiment with.  It seems to offer the same kind of fun exploration and experimentation as many of the microcontroller boards do.  The web site, http://www.fpga4fun.com/, is a very useful site that I am working through while testing these unknown waters.  The first project I undertook was one to blink the LED on the Pluto II: http://www.fpga4fun.com/QuartusQuickStart.html.  By following the instructions given and taking care to note which pin (PIN_10) has the clock0 signal available on this particular FPGA chip (EP1C3T100C8) and which pin (PIN_25) is connected to the LED, I managed a achieve the desired result of getting Altera's Quartus II to sucessfully compile the simple Verilog HDL file named ledblink.v.  The next step will be to actually flash the raw binary file, ledblink.rbf, into the onboard boot rom using my older Dell Lattitude D630 laptop which has the required RS-232 port available since the TXDI serial interface uses that DB-9 to communicate to and from the FPGA.  Interesting to note that the compiler creates 70+ small files all sharing the ledblink name prefix.

 

module ledblink(

          input clk,

          output LED

          );

 

reg [23:0] count;                      //  declares a 24 bit variable named 'count'


always @(posedge clk)   //  Procedure occurs only when trailing 'post' edge of clock is detected

begin

     count <= count + 24'd1;  //  the constant being added is 24 bit decimal whose value is 1

end                                           //  it will rollover and reset to zero after 2^24 clock cycles

                                          

assign LED = count [23];     //  the LED is controlled by the high order bit of the variable 'count'

                       // the LED is off for 'count' < 2^23   and is on for 'count' >= 2^23;  gives 50% duty cycle                 

                        //  AND continous evaluation of control bit and update of output register

endmodule

 

 

image

EP1C3T100C8 Datasheet: http://www.altera.com/literature/hb/cyc/cyc_c5v1.pdf

 

Post blog trivia questions:

Q1:  What single parameter can be altered to either increase or decrease the period of the LED's blinking?

Q2:  What other parameter can be altered to decrease the period of the LED's blinking?

 

Happy Trails to you!

  • Sign in to reply
Parents
  • shabaz
    shabaz over 12 years ago

    Hi William,

     

    That's great! Glad that you got through the toolchain bit. It's not easy (at least, not with Xilinx).

    I too have just tried your code on Xilinx tools, and will soon try it on a CPLD board. It's also possible to simulate it (by writing a testbench) but I'm not sure how to do that in verilog, I've only done it in VHDL.

    To alter the blinking there are a few ways for example either the input pin clock could be slowed down or sped up (but that requires a crystal change!), or the speed could be halved or doubled by changing the assign LED = count[23] line up or down, but for more flexibility, it is possible to synthesize more logic. For example, it is possible to use statements like

    assign LED = (count==24'd100)?1'b0:1'b1; which can conditionally set the LED output. By the way, I just found this link which may be useful. It seems at least as good as my textbook (which is quite basic).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 12 years ago

    Hi William,

     

    That's great! Glad that you got through the toolchain bit. It's not easy (at least, not with Xilinx).

    I too have just tried your code on Xilinx tools, and will soon try it on a CPLD board. It's also possible to simulate it (by writing a testbench) but I'm not sure how to do that in verilog, I've only done it in VHDL.

    To alter the blinking there are a few ways for example either the input pin clock could be slowed down or sped up (but that requires a crystal change!), or the speed could be halved or doubled by changing the assign LED = count[23] line up or down, but for more flexibility, it is possible to synthesize more logic. For example, it is possible to use statements like

    assign LED = (count==24'd100)?1'b0:1'b1; which can conditionally set the LED output. By the way, I just found this link which may be useful. It seems at least as good as my textbook (which is quite basic).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • billabott
    billabott over 12 years ago in reply to shabaz

    That China link is not available at this time.  maybe later.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to billabott

    Oh, that's interesting.  I still have a copy, I'll find a way to forward it (I originally found it via just a google search, so I don't think there is a copyright issue).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • billabott
    billabott over 12 years ago in reply to shabaz

    Yes, I would like to have Verilog Gold pdf.  If you have time to provide a workable link.  Thanks.