Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs Getting up and running with Arm Design Start
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: adamtaylorcengfiet
  • Date Created: 19 Nov 2018 10:50 AM Date Created
  • Views 7271 views
  • Likes 9 likes
  • Comments 7 comments
  • xilinx_explore
  • arm m3
  • fpga
  • arty
  • arty s7
  • design start fpga
  • arm m1
Related
Recommended

Getting up and running with Arm Design Start

adamtaylorcengfiet
adamtaylorcengfiet
19 Nov 2018

One of the big announcements at the recent Xilinx Developer Forum (XDF) in San Jose was the Arm design start programme. This opens to FPGA developers license free both the cortex M1 and M3 for our Xilinx FPGA designs.

In our design, we use the Cortex M cores for tasks such as System Management, IO and Sensor Controllers.

So, what do you need to get up and running with the Arm FPGA Design Start?

  • Arty A35T or Arty S50
  • Vivado 2018.2
  • Arm M1 or M3 Design Start pack depending upon core choice

In the remainder of this blog we are going to look at how we can get the initial design example up and running on the Arty hardware. We will follow this up with another blog which examines how we can create our own software applications for the design.

The first step in creating this example is to download the relevant Cortex core from the Arm Design Start page.

 

To download the design, you will need to register and agree to the license terms.

image

Both M1 and M3 packages are downloaded as compressed files, unzip these files until you see the following file structure.

image

The directories are self-evident

  • Docs – Contains the design documentation
  • Hardware – Contains the design example projects and bit files in Vivado
  • Software – Contains the SW application for the demo application
  • Vivado – Contains Vivado IP and SDK SW repositories required to create a new design from scratch

For this example, we are going to open the existing projects, these are under the hardware directory.

For the M1 example you will see two choices projects and bit files for either the Arty A7 or S7, while for the M3 you will see the project for the Arty A7.

image

Before we can open any of these projects, we need to also set the default IP location, such that when the project is opened it knows where to look for the Arm cores.

We can do this in Vivado before we open a project, click on Tools -> Setting and select IP Defaults and add the path to the Vivado folder we just extracted with the download.

image

Once we have added the default IP search path, we can open the project of our choosing. For this blog I am going to open the M3 Arty design.

The project may take a few minutes to open depending upon the speed of your machine, however once it is opened. We can explore the block diagram of the design

image

The next stage is to program the provided bit file into the Arty.

On the left hand of the screen in Vivado select hardware manager, this will configure Vivado to be able to connect to and download bit files.

image

When the hardware manager is open you will see a green bar across the top and the words Open Target in blue. Ensure your Arty board is connected and left click on Open Target and select Auto Connect.

This will connect to the Arty using the USB JTAG, allowing us to download the bit file.

Before we can download the bit file, we should open a terminal program and connect to the serial port. For this I used PuTTY the serial rate is 115200 with 1 stop and start and no parity.

image

Once we have the terminal program connected the next step is to download the bit file

image

 

Right click on the device under Hardware and select program device, this will open a dialog window which will include the bit file. Select this bit file and click program.

image

Once the application has programmed in the terminal, we should be able to see the hello world message from the running Cortex M3

image

We can now use the DIP and push button switches to change the states of the LEDs as below.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Now we know the basics of how to get the example design up and running we will look next time at how we can write software for our chosen Cortex M core.

In the mean time explore the block diagram and read the documentation to gain further understanding of not only the example design but also the reference documentation.

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +2
    A very useful guide. Thanks.
  • Fred27
    Fred27 over 7 years ago in reply to 14rhb +2
    I think only the Cortex-M1 is supported on the Arty S7.
  • DAB
    DAB over 7 years ago +1
    It looks like Xilinx is getting serious about bringing FPGA devices to the maker world. DAB
Parents
  • 14rhb
    14rhb over 7 years ago

    Hi Adam,

     

    This is interesting stuff to know, I've got a Digilent Arty S7 and from the ARM link you provide I can see they also support that. Hopefully I'll have some time over the holiday period to try it out. That said, I didn't get on too well experimenting with the Vivado Microblaze IP core (a lack of knowledge, low spec computer etc) but I did still learn a lot and would aim to do the same placing my own Cortex-M3 on the FPGA.

     

    Thanks,

     

    Rod

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to 14rhb

    I think only the Cortex-M1 is supported on the Arty S7.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to Fred27

    I think the example design for the Cortex-M1 is provided on the Arty S& you can of course target it to anything you would like

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to adamtaylorcengfiet

    What I mean is that you can't do the Cortex-M3 on the Arty-S7.

     

    By the way, you made it onto Hackaday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to Fred27

    I just tried synthesizing the M3 design to my Spartan board and it did OK. I need to change the pinout but I think it will implement OK too

     

    I saw that is really cool

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • adamtaylorcengfiet
    adamtaylorcengfiet over 7 years ago in reply to Fred27

    I just tried synthesizing the M3 design to my Spartan board and it did OK. I need to change the pinout but I think it will implement OK too

     

    I saw that is really cool