Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs High Voltage GaN FETs - Part 3: Probing the LMG3410 Half-Bridge
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 24 Aug 2016 4:14 PM Date Created
  • Views 3144 views
  • Likes 7 likes
  • Comments 14 comments
  • switching_supplies
  • lmg3410
  • half_bridge
  • texas_instruments
  • gan
  • power_electronics
Related
Recommended

High Voltage GaN FETs - Part 3: Probing the LMG3410 Half-Bridge

Jan Cumps
Jan Cumps
24 Aug 2016

The series will use high-voltage FETs in half-bridge configuration.

This time I look at the bridge's output signal.

image

I'm particularly interested in the overshoot, because controlling that is one of the claimed advantages of GaN technology.

 

The high and low side of the bridge are controlled by an opposite signal. Both signals have a dead time inserted when one signal goes low and the other switches high.

GaN semiconductors don't need a lot of dead time. The setup here is configured for a 50 ns band.

 

image

*1: I was sloppy when capturing this scope window. The falling edge of the input signal should be where the orange line is. Check comments below for more info.

Thank you jc2048 for spotting this.

 

 

The scope capture above shows the input (low-power) signals.

The white line is the input signal, with 22% duty cycle and a frequency of 200 kHz.

The yellow line is the driver signal for the high side FET, the blue signal for the low side one. Check the schematic below to get an idea of where the 3 signals occur.

(excuses for the mismatch in scope horizontal scale setting between yellow and blue. I only saw this after I disconnected my setup. They have the same amplitude.)

 

image

 

I'm going to probe the switcher's output signal. I'll zoom in on the overshoot positions, so you can see that the signal is behaving decently in the dead time.

 

image

This trace is a full high part of the output at 200 kHz, 22% duty cycle.

It gives an impression of the switching artifacts just before the edges.

 

A detailed capture of the rising edge overshoot looks like this:

image

The input signal is 60 V. The overshoot is approximately -8 V:

image

 

On the falling edge, there's less switching residue:

image

(the time scale is extended to the limits of what I can show on my scope screen. Check the full signal above to get an idea of how steep (50 ns) this ramp-down and overshoot is.)

 

image

 

The evaluation board that I'm using has reasonable filtering at the output. Let's check how the DC signal after that flter looks like.

image

The load I'm using is approx. 12 W (12 V, 1 A). The capture below shows only the AC (noise) component of the output.

I get close to 650 mV of ripple peak-to-peak.

image

 

Not surprisingly, the largest artifacts appear at the edges of the PWM driver signals. This is a reasonable DC signal.

Further filtering will smoothen it more - the board I'm using is to show how the GaN FETs perform, so it doesn't focus on output filtering.

 

image

 

 

 

 

Part 1: Several 100 Volts
Part 2: Test Setup with LMG3410 Half-Bridge
Part 3: Probing the LMG3410 Half-Bridge
  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Great update. I did have one thought, I wonder if the overshoot measurement was limited by your scopes bandwidth. Granted 50 nano seconds is not much, but I have seen femtosecond pulses destroy circuits…
  • jc2048
    jc2048 over 10 years ago +1
    Good stuff, Jan. Thanks for posting this. The high side FET anticipates the input signal and turns off 50nS before it arrives? Something tells me that might not be right. Line drawn in wrong place? I take…
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to jc2048 +1
    I expect that if I would re-take the capture, and not exaggerate the saved input signal, the white signal would look like the (drawn by me in Paint ) red signal here:
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to jc2048

    That white line is not a drawn one, it's an in-memory saved input signal.

    Your comment is spot on though, that falling edge of the white signal should be frilliseconds before the falling edge of the yellow signal.

     

    The reason why that line doesn't appear on the right place can be:

    • either the drift of my signal generator causes this, and the duty-cycle of the signal dropped a little between when the signal was stored, and the scope screen capture (there was approx half an hour between the two actions, where I didn't touch generator settings, but this is a lowly home use generator)
    • I exaggerated the amplitude of that stored signal so hard it shows as a straight line, but in reality it's a dirty square wave that drops off earlier than the position it shows on the scope.
      I'll check if I still have it stored so hat I can show what it really looks like.
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 10 years ago

    Good stuff, Jan. Thanks for posting this.

     

    The high side FET anticipates the input signal and turns off 50nS before it arrives? Something tells me that might not be right. Line drawn in wrong place?

     

    I take it the waveforms are with the filter on the output. Are they with a load of 1A?

     

    What does the falling edge look like at a load current of 0.5A?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 10 years ago in reply to DAB

    Yes, that's possible.

    With analog scopes, even if something was beyond the bandwidth, you typically saw some attenuated artifact on screen.

    With the sampling ones, like mine, these may just not get sampled at all.

     

    The manual for the evaluation board says about the scope requirements to measure this circuit:

    Oscilloscope: Capable of at least 200 MHz operation. A 1 GHz or greater oscilloscope and probes with

    short ground springs are recommended for accurate measurements.

    I don't have such a scope image. I do have the (self-made) ground springs though.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Great update.

     

    I did have one thought, I wonder if the overshoot measurement was limited by your scopes bandwidth.

    Granted 50 nano seconds is not much, but I have seen femtosecond pulses destroy circuits.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<