Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs How Many Tools Does it Take To ....... Remove a screw from the wall
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: dubbie
  • Date Created: 29 Aug 2020 12:11 PM Date Created
  • Views 2983 views
  • Likes 7 likes
  • Comments 20 comments
  • tools
Related
Recommended

How Many Tools Does it Take To ....... Remove a screw from the wall

dubbie
dubbie
29 Aug 2020

I've always known that it takes many more tools than you think to do even the simplest of jobs and today I was able to confirm that. One of my bedrooms is being redecorated and this involved removing some box shelve units, which in itself was very straight forward, but it did leave the screws still fixed into the wall. I think the shelves were put up some 20 years ago so have had plenty of time to fuse into place. Additionally, they were also unusual screws as they were much longer than expected, being 5 cm long. Fortunately they were crosshead and I managed to remove 3 of the four using basically brute strength. How I put them in I cannot imagine - I must have been much stronger 20 years ago.

 

For the last screw every cross head screwdriver I used wasn't good enough and I ended up stripping the screw head. So, I used a junior hacksaw to cut a slot, then a standard hacksaw to make the slot wide enough for a flat blade screwdriver and eventually managed to remove the screw. The tools I used are shown below - and I used them all (except the hammer)! Plus a step ladder.

 

image

 

 

So from top to bottom:

 

1) Junior hacksaw.

2) Large pliers (a gift from Element14 - thanks very much) Tried to use these to rotate the screw - they didn't work.

3) Small pliers (for trying to remove the wall plug - didn't work)

4) Small wooden handles flat blade screwdriver (Not big enough)

5) Ratchet screwdriver flat blade (Not big enough)

6) Large wooden handled screwdriver flat blade (Finally did the job once a slot was cut into the screw head)

7) Rubber handled flat blade screwdriver (a gift from Element14 - thanks very much) Just not big enough.

8) Ratchet screwdriver cross head. (Worked for three of the screws just not for the last one)

9) Standard hacksaw.

10 Drill bits for drilling out the wall plug.

11) Set of screwdriver bits (Used with tool 8.)

12) Hammer (Actually I don't think I did use this)

13) Cordless drill (Used to remove the wall plug - mostly)

14) Step ladder (Not shown.)

 

So I had to use 13 tools (I haven't counted the hammer) to remove one screw from the wall, along with it's accompanying wall plug.

 

Below is the hole I ended up with. Parts of the wall plug are still inside this hole but I thought this hole is big enough as it is so I stopped.

 

image

 

I was surprised at how many tools I did need for this seemingly simple task.

 

Dubbie

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 6 years ago +5
    I like jobs like this they present a challenge. I also like to buy new and special tools so a tough job often gives me a pretext to add a new member to my arsenal of tools. I have often used a vise-grip…
  • Andrew J
    Andrew J over 6 years ago +5
    This would be a lot more believable if there was a can of WD-40 on the table
  • beacon_dave
    beacon_dave over 6 years ago +5
    I don't see the 48" stilson pipe wrench or the hydraulic ram though ? Must be a small job...
Parents
  • Fred27
    Fred27 over 6 years ago

    I've also been doing some decorating today. There were loads of rawlplugs to remove because the previous owner thought it was OK to just wallpaper over them! I found that this hook and claw hammer do the best job for removing rawlplugs. Just screw in the hook (with a slightly undersized screw thread) and use a claw hammer to pull the plug out. I like the pliers for stubborn screws too. Note the grooves at the tip of the jaws which are aligned to make grabbing a screw head and twisting easy.

    image

    When it come to filling, this is by far the best filler I've found. You can fill even large deep holes or cracks and it doesn't shrink. I has a nice grainy texture and it sands and paints easily.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago in reply to Fred27

    Fred,

     

    I thought of using a claw hammer to rip the screw out but I thought that would probably make more dents where the hammer had rested on the plaster so I never tried it.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dubbie
    dubbie over 6 years ago in reply to Fred27

    Fred,

     

    I thought of using a claw hammer to rip the screw out but I thought that would probably make more dents where the hammer had rested on the plaster so I never tried it.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down