Personal Blogs
  • Community Hub
  • More
Personal Blogs
Legacy Personal Blogs I've got a problem to solve!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sasquatch84
  • Date Created: 7 Sep 2017 2:00 AM Date Created
  • Views 2190 views
  • Likes 6 likes
  • Comments 15 comments
Related
Recommended

I've got a problem to solve!

sasquatch84
sasquatch84
7 Sep 2017

I believe it was John Adams that once said, "every problem is an opportunity in disguise."  This, as it turns out, is great advice for those wanting to come up with a new Arduino project.  When I first started to look for project ideas, I was just trying to make use of what I have and create something that looked cool.  But now that I am looking for problems to solve, well, the possibilities are endless!  Take my job for starters.  I am a logger.  If there is one industry that has completely lacked technological advancement for the last 50 years* and deals with some of the greatest problems any of us will ever face on a daily basis, it's the logging industry.  Cable logging to be more precise. 

The first problem I would like to solve is one of safety:

A grapple yarder (if you're already lost watch https://www.google.ca/url?sa=t&rct=j&q=&esrc=s&source=web&cd=3&cad=rja&uact=8&ved=0ahUKEwiKlZWB-pHWAhVH1WMKHahkDIkQtwIIL… ) is held in place by cables called "guylines".  These guylines are most often anchored on stumps that are called "tailholds".  A grapple yarder puts these stumps under major stress and sometimes the stumps are pulled right out of the ground.  This is never supposed to happen, because it can cause major damage to machinery as well as death.  But it happens.

So my solution would be to have a unit that is placed on the tailhold that alerts the grapple yarder operator if the stump is starting to move. 

My idea:

So I think I might be stepping a little too far out of my range of expertise, but I would like to try to use an accelerometer on the stump connected to an Arduino.  then the Arduino puts out an rf signal to another Arduino in the grapple yarder.  This second Arduino will then display on an LCD display or a row of LEDs how much the stump is moving.  I have never used the rf module although I have one.  Also, never even tried my accelerometer.

Any suggestions?

 

*In the last 5 years there has FINALLY been a slow trend of new technology in the bush, but by and large, we are still stuck in the 1960's.  Seriously.

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 8 years ago +5
    Hi Clinton, If the stump is pulled out slowly the acceleration may be too low to sense. Also once the stump is moving it would have no acceleration. Finally if a root snaps the acceleration would certainly…
  • DAB
    DAB over 8 years ago +4
    Hi Clinton, I would look at adding a strain gage to the cables. The Arduino could monitor the cable stress and could quickly detect if there was a slackening in the cable due to stump movement. It would…
  • ntewinkel
    ntewinkel over 8 years ago +4
    Hi Clinton, I would assume that during regular use there would be a fair bit of vibration, so it would be hard to detect "bad" movement amongst the regular movement. The big question is at what point is…
Parents
  • ntewinkel
    ntewinkel over 8 years ago

    Hi Clinton,

     

    I would assume that during regular use there would be a fair bit of vibration, so it would be hard to detect "bad" movement amongst the regular movement.

     

    The big question is at what point is it too late? What are the pre-failure warning signs we can use to determine when to sound the alarm?

    Can a tilt sensor be used on the stump so that if it starts leaning over too far it sounds the alarm? Or is that already too late? - ie, by the time it tilts any amount the stump is already flying out of the ground?

     

    Interesting question image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 8 years ago

    Hi Clinton,

     

    I would assume that during regular use there would be a fair bit of vibration, so it would be hard to detect "bad" movement amongst the regular movement.

     

    The big question is at what point is it too late? What are the pre-failure warning signs we can use to determine when to sound the alarm?

    Can a tilt sensor be used on the stump so that if it starts leaning over too far it sounds the alarm? Or is that already too late? - ie, by the time it tilts any amount the stump is already flying out of the ground?

     

    Interesting question image

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • sasquatch84
    sasquatch84 over 8 years ago in reply to ntewinkel

    I'm already showing my inexperience.  I thought that's what an accelerometer could do; detect a change in angle.  That is what I want to measure.  The suggestions of attaching a line is just very difficult if you know about logging.  Detecting angle changing would be perfectly sufficient.  A stump can't move more than maybe an inch without being compromised.  Also, having a reel of some kind would definitely be more vulnerable to damage.  If anyone here has ever seen logging equipment, they would see how rough a life our stuff has.  I want to have a completely contained unit that can be shoved into my pocket (I need two hands to do the rock scaling/hill climbing that is normal life out here) and then attached to a stump and take wind, rain, snow etc.  in stride.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sasquatch84
    sasquatch84 over 8 years ago in reply to sasquatch84

    Then again, sometimes, because of the angle of the pull, the stumps pull straight sideways and never really tilt at all.  This makes me think that something that detected distance wirelessly would be best.  maybe use an ultrasonic distance sensor.  I can aim it at the hill behind it or a tree, whatever, and hit the "on" button.  Then it will measure that distance and look for any change.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to sasquatch84

    An accelerometer can be used to measure the angle change, it's just that a tilt sensor does it more simply as on/off after a threshold. I think I have a few that have a little metal ball that rolls over to close a circuit.

    Of course, some boards (like the Arduino 101) have the accelerometer already there, in which case you may as well use that image

     

    Stumps going straight sideways make for an interesting and challenging problem! And in that case I think you're right about it being a distance thing. And Maybe the simplest is what Douglas suggested - just use a string pinned into the next stump that pulls a pin if it moves more than half an inch.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to sasquatch84

    Thinking about the options then....

    Could you place something that has two level detectors in it.

    These would need to be set when you attach it, but could trigger a wireless warning system.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to sasquatch84

    Does the line holding the pulley block always go around two stumps ?

     

    If so, than perhaps some sort of stump-to-stump detection system could be used.